aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorBin Meng2018-10-11 00:06:57 -0500
committerSimon Glass2018-11-14 11:16:27 -0600
commite601ab1bb69901420ba2c55d2f2d194a38739182 (patch)
tree7516a87dfe7fcb1bbb1b283bb61107274f44a5a9 /include
parent6fe8abcce740a67e81fb6115f54dba380bd2ff4d (diff)
downloadu-boot-e601ab1bb69901420ba2c55d2f2d194a38739182.tar.gz
u-boot-e601ab1bb69901420ba2c55d2f2d194a38739182.tar.xz
u-boot-e601ab1bb69901420ba2c55d2f2d194a38739182.zip
dm: util: Add a livetree equivalent API of dm_fdt_pre_reloc()
This adds a new API dm_ofnode_pre_reloc(), a livetree equivalent API of dm_fdt_pre_reloc(). Signed-off-by: Bin Meng <bmeng.cn@gmail.com> Reviewed-by: Simon Glass <sjg@chromium.org>
Diffstat (limited to 'include')
-rw-r--r--include/dm/util.h27
1 files changed, 26 insertions, 1 deletions
diff --git a/include/dm/util.h b/include/dm/util.h
index 898822e445..9ff6531d1b 100644
--- a/include/dm/util.h
+++ b/include/dm/util.h
@@ -55,7 +55,7 @@ static inline void dm_dump_devres(void)
55 * There are 3 settings currently in use 55 * There are 3 settings currently in use
56 * - 56 * -
57 * - u-boot,dm-pre-reloc: legacy and indicates any of TPL or SPL 57 * - u-boot,dm-pre-reloc: legacy and indicates any of TPL or SPL
58 * Existing platforms only use it to indicate nodes needee in 58 * Existing platforms only use it to indicate nodes needed in
59 * SPL. Should probably be replaced by u-boot,dm-spl for 59 * SPL. Should probably be replaced by u-boot,dm-spl for
60 * existing platforms. 60 * existing platforms.
61 * @blob: devicetree 61 * @blob: devicetree
@@ -65,4 +65,29 @@ static inline void dm_dump_devres(void)
65 */ 65 */
66bool dm_fdt_pre_reloc(const void *blob, int offset); 66bool dm_fdt_pre_reloc(const void *blob, int offset);
67 67
68/**
69 * Check if an of node should be or was bound before relocation.
70 *
71 * Devicetree nodes can be marked as needed to be bound
72 * in the loader stages via special devicetree properties.
73 *
74 * Before relocation this function can be used to check if nodes
75 * are required in either SPL or TPL stages.
76 *
77 * After relocation and jumping into the real U-Boot binary
78 * it is possible to determine if a node was bound in one of
79 * SPL/TPL stages.
80 *
81 * There are 3 settings currently in use
82 * -
83 * - u-boot,dm-pre-reloc: legacy and indicates any of TPL or SPL
84 * Existing platforms only use it to indicate nodes needed in
85 * SPL. Should probably be replaced by u-boot,dm-spl for
86 * existing platforms.
87 * @node: of node
88 *
89 * Returns true if node is needed in SPL/TL, false otherwise.
90 */
91bool dm_ofnode_pre_reloc(ofnode node);
92
68#endif 93#endif