diff options
author | Joe Hershberger | 2018-04-13 15:26:32 -0500 |
---|---|---|
committer | Joe Hershberger | 2018-04-13 15:48:05 -0500 |
commit | 92fa44d58f4e5433eeb5fe6a56f2b6faf5e84c20 (patch) | |
tree | 9d6b283898b9a97eef13006750a65fb183429fc1 /net | |
parent | ba6288557d8a1bd845b841b9287b9752a470faa9 (diff) | |
download | u-boot-92fa44d58f4e5433eeb5fe6a56f2b6faf5e84c20.tar.gz u-boot-92fa44d58f4e5433eeb5fe6a56f2b6faf5e84c20.tar.xz u-boot-92fa44d58f4e5433eeb5fe6a56f2b6faf5e84c20.zip |
net: Move net command options to the cmd menu
Options that controlled the tftp and bootp commands depended on their
commands, but lived in the net menu.
Move them so they are in a consistent location.
Signed-off-by: Joe Hershberger <joe.hershberger@ni.com>
Reviewed-by: Chris Packham <judge.packham@gmail.com>
Diffstat (limited to 'net')
-rw-r--r-- | net/Kconfig | 50 |
1 files changed, 0 insertions, 50 deletions
diff --git a/net/Kconfig b/net/Kconfig index d421a34d97..f2363e5256 100644 --- a/net/Kconfig +++ b/net/Kconfig | |||
@@ -22,54 +22,4 @@ config NETCONSOLE | |||
22 | Support the 'nc' input/output device for networked console. | 22 | Support the 'nc' input/output device for networked console. |
23 | See README.NetConsole for details. | 23 | See README.NetConsole for details. |
24 | 24 | ||
25 | config NET_TFTP_VARS | ||
26 | bool "Control TFTP timeout and count through environment" | ||
27 | depends on CMD_TFTPBOOT | ||
28 | default y | ||
29 | help | ||
30 | If set, allows controlling the TFTP timeout through the | ||
31 | environment variable tftptimeout, and the TFTP maximum | ||
32 | timeout count through the variable tftptimeoutcountmax. | ||
33 | If unset, timeout and maximum are hard-defined as 1 second | ||
34 | and 10 timouts per TFTP transfer. | ||
35 | |||
36 | config BOOTP_BOOTPATH | ||
37 | bool "Enable BOOTP BOOTPATH" | ||
38 | depends on CMD_BOOTP | ||
39 | |||
40 | config BOOTP_DNS | ||
41 | bool "Enable bootp DNS" | ||
42 | depends on CMD_BOOTP | ||
43 | |||
44 | config BOOTP_GATEWAY | ||
45 | bool "Enable BOOTP gateway" | ||
46 | depends on CMD_BOOTP | ||
47 | |||
48 | config BOOTP_HOSTNAME | ||
49 | bool "Enable BOOTP hostname" | ||
50 | depends on CMD_BOOTP | ||
51 | |||
52 | config BOOTP_PXE | ||
53 | bool "Enable BOOTP PXE" | ||
54 | depends on CMD_BOOTP | ||
55 | |||
56 | config BOOTP_SUBNETMASK | ||
57 | bool "Enable BOOTP subnetmask" | ||
58 | depends on CMD_BOOTP | ||
59 | |||
60 | config BOOTP_PXE_CLIENTARCH | ||
61 | hex | ||
62 | depends on CMD_BOOTP | ||
63 | default 0x16 if ARM64 | ||
64 | default 0x15 if ARM | ||
65 | default 0 if X86 | ||
66 | |||
67 | config BOOTP_VCI_STRING | ||
68 | string | ||
69 | depends on CMD_BOOTP | ||
70 | default "U-Boot.armv7" if CPU_V7 || CPU_V7M | ||
71 | default "U-Boot.armv8" if ARM64 | ||
72 | default "U-Boot.arm" if ARM | ||
73 | default "U-Boot" | ||
74 | |||
75 | endif # if NET | 25 | endif # if NET |