aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* Revert "Add Android.bp to build U-Boot's mkimage."Ian Zerny2018-08-2824-26/+0
| | | | | | | | This reverts commit 0a8baca502643f8d3250711b8a7a792c8c8100db. Reason for revert: causes failure on git_pi-dev-plus-aosp build_test Change-Id: I942a07070770f92babc2d9ae46096d61fad60497
* Add Android.bp to build U-Boot's mkimage.Alistair Strachan2018-08-2224-0/+26
This tool is needed to build FIT images for the Beagleboard-X15 platform. As it is not a required host build dependency, we must build it from sources. This change introduces a build of the mkimage tool from 2018.07, however the image signing feature is disabled because it depends on an openssl API which was removed from boringssl. This would need further changes upstream to resolve. A directory containing a large number of symlinks to existing headers is also provided, as the GNU Make build system was using the "-idirafter" feature to stop copies of standard C headers like stdint.h, stdlib.h from being selected from the U-Boot 'include' directory, which is an unsupported feature in the Android build system. Bug: 74437007 Change-Id: Idadda650232749d198320b4556a7ba5379a441d0 Signed-off-by: Alistair Strachan <astrachan@google.com>