CONFIG_MIPS=y CONFIG_SYS_TEXT_BASE=0x80010000 CONFIG_ARCH_BMIPS=y CONFIG_SOC_BMIPS_BCM6368=y # CONFIG_MIPS_BOOT_CMDLINE_LEGACY is not set # CONFIG_MIPS_BOOT_ENV_LEGACY is not set CONFIG_MIPS_BOOT_FDT=y CONFIG_NR_DRAM_BANKS=1 # CONFIG_SYS_MALLOC_CLEAR_ON_INIT is not set CONFIG_OF_STDOUT_VIA_ALIAS=y CONFIG_DISPLAY_CPUINFO=y CONFIG_HUSH_PARSER=y CONFIG_SYS_PROMPT="WAP-5813n # " CONFIG_CMD_CPU=y CONFIG_CMD_LICENSE=y # CONFIG_CMD_BOOTD is not set # CONFIG_CMD_ELF is not set # CONFIG_CMD_XIMG is not set # CONFIG_CMD_EXPORTENV is not set # CONFIG_CMD_IMPORTENV is not set # CONFIG_CMD_EDITENV is not set # CONFIG_CMD_SAVEENV is not set # CONFIG_CMD_ENV_EXISTS is not set # CONFIG_CMD_CRC32 is not set CONFIG_CMD_MEMINFO=y # CONFIG_CMD_LOADS is not set CONFIG_CMD_USB=y # CONFIG_CMD_MISC is not set CONFIG_OF_EMBED=y CONFIG_DEFAULT_DEVICE_TREE="comtrend,wap-5813n" # CONFIG_NET is not set # CONFIG_DM_DEVICE_REMOVE is not set CONFIG_DM_GPIO=y CONFIG_BCM6345_GPIO=y CONFIG_LED=y CONFIG_LED_GPIO=y CONFIG_MTD=y CONFIG_MTD_NOR_FLASH=y CONFIG_FLASH_CFI_DRIVER=y CONFIG_CFI_FLASH=y CONFIG_SYS_FLASH_PROTECTION=y CONFIG_SYS_FLASH_CFI=y CONFIG_PHY=y CONFIG_BCM6368_USBH_PHY=y CONFIG_DM_RESET=y CONFIG_RESET_BCM6345=y # CONFIG_SPL_SERIAL_PRESENT is not set CONFIG_DM_SERIAL=y CONFIG_BCM6345_SERIAL=y CONFIG_USB=y CONFIG_DM_USB=y CONFIG_USB_EHCI_HCD=y CONFIG_USB_EHCI_GENERIC=y CONFIG_USB_OHCI_HCD=y CONFIG_USB_OHCI_GENERIC=y