Notes on the the generic USB-OHCI driver ======================================== This driver (drivers/usb/usb_ohci.[ch]) is the result of the merge of various existing OHCI drivers that were basically identical beside cpu/board dependant initalization. This initalization has been moved into cpu/board directories and are called via the hooks below. Configuration options ---------------------- CONFIG_USB_OHCI_NEW: enable the new OHCI driver CONFIG_SYS_USB_OHCI_BOARD_INIT: call the board dependant hooks: - extern int usb_board_init(void); - extern int usb_board_stop(void); - extern int usb_cpu_init_fail(void); CONFIG_SYS_USB_OHCI_CPU_INIT: call the cpu dependant hooks: - extern int usb_cpu_init(void); - extern int usb_cpu_stop(void); - extern int usb_cpu_init_fail(void); CONFIG_SYS_USB_OHCI_REGS_BASE: defines the base address of the OHCI registers CONFIG_SYS_USB_OHCI_SLOT_NAME: slot name CONFIG_SYS_USB_OHCI_MAX_ROOT_PORTS: maximal number of ports of the root hub. Endianness issues ------------------ The USB bus operates in little endian, but unfortunately there are OHCI controllers that operate in big endian such as ppc4xx. For these the config option CONFIG_SYS_OHCI_BE_CONTROLLER needs to be defined. PCI Controllers ---------------- You'll need to define CONFIG_PCI_OHCI If you have several USB PCI controllers, define CONFIG_PCI_OHCI_DEVNO: number of the OHCI device in PCI list If undefined, the first instance found in PCI space will be used. PCI Controllers need to do byte swapping on register accesses, so they should to define: CONFIG_SYS_OHCI_SWAP_REG_ACCESS