// SPDX-License-Identifier: GPL-2.0+ /* * (C) Copyright 2000-2010 * Wolfgang Denk, DENX Software Engineering, wd@denx.de. * * (C) Copyright 2008 * Stuart Wood, Lab X Technologies * * (C) Copyright 2004 * Jian Zhang, Texas Instruments, jzhang@ti.com. * * (C) Copyright 2001 Sysgo Real-Time Solutions, GmbH * Andreas Heppel */ #include #include #include #include #include #include #include #include #include #if defined(CONFIG_CMD_SAVEENV) && defined(CONFIG_CMD_NAND) && \ !defined(CONFIG_SPL_BUILD) #define CMD_SAVEENV #elif defined(CONFIG_ENV_OFFSET_REDUND) #error CONFIG_ENV_OFFSET_REDUND must have CONFIG_CMD_SAVEENV & CONFIG_CMD_NAND #endif #if defined(CONFIG_ENV_SIZE_REDUND) && \ (CONFIG_ENV_SIZE_REDUND != CONFIG_ENV_SIZE) #error CONFIG_ENV_SIZE_REDUND should be the same as CONFIG_ENV_SIZE #endif #ifndef CONFIG_ENV_RANGE #define CONFIG_ENV_RANGE CONFIG_ENV_SIZE #endif #if defined(ENV_IS_EMBEDDED) env_t *env_ptr = &environment; #elif defined(CONFIG_NAND_ENV_DST) env_t *env_ptr = (env_t *)CONFIG_NAND_ENV_DST; #else /* ! ENV_IS_EMBEDDED */ env_t *env_ptr; #endif /* ENV_IS_EMBEDDED */ DECLARE_GLOBAL_DATA_PTR; /* * This is called before nand_init() so we can't read NAND to * validate env data. * * Mark it OK for now. env_relocate() in env_common.c will call our * relocate function which does the real validation. * * When using a NAND boot image (like sequoia_nand), the environment * can be embedded or attached to the U-Boot image in NAND flash. * This way the SPL loads not only the U-Boot image from NAND but * also the environment. */ static int env_nand_init(void) { #if defined(ENV_IS_EMBEDDED) || defined(CONFIG_NAND_ENV_DST) int crc1_ok = 0, crc2_ok = 0; env_t *tmp_env1; #ifdef CONFIG_ENV_OFFSET_REDUND env_t *tmp_env2; tmp_env2 = (env_t *)((ulong)env_ptr + CONFIG_ENV_SIZE); crc2_ok = crc32(0, tmp_env2->data, ENV_SIZE) == tmp_env2->crc; #endif tmp_env1 = env_ptr; crc1_ok = crc32(0, tmp_env1->data, ENV_SIZE) == tmp_env1->crc; if (!crc1_ok && !crc2_ok) { gd->env_addr = 0; gd->env_valid = ENV_INVALID; return 0; } else if (crc1_ok && !crc2_ok) { gd->env_valid = ENV_VALID; } #ifdef CONFIG_ENV_OFFSET_REDUND else if (!crc1_ok && crc2_ok) { gd->env_valid = ENV_REDUND; } else { /* both ok - check serial */ if (tmp_env1->flags == 255 && tmp_env2->flags == 0) gd->env_valid = ENV_REDUND; else if (tmp_env2->flags == 255 && tmp_env1->flags == 0) gd->env_valid = ENV_VALID; else if (tmp_env1->flags > tmp_env2->flags) gd->env_valid = ENV_VALID; else if (tmp_env2->flags > tmp_env1->flags) gd->env_valid = ENV_REDUND; else /* flags are equal - almost impossible */ gd->env_valid = ENV_VALID; } if (gd->env_valid == ENV_REDUND) env_ptr = tmp_env2; else #endif if (gd->env_valid == ENV_VALID) env_ptr = tmp_env1; gd->env_addr = (ulong)env_ptr->data; #else /* ENV_IS_EMBEDDED || CONFIG_NAND_ENV_DST */ gd->env_addr = (ulong)&default_environment[0]; gd->env_valid = ENV_VALID; #endif /* ENV_IS_EMBEDDED || CONFIG_NAND_ENV_DST */ return 0; } #ifdef CMD_SAVEENV /* * The legacy NAND code saved the environment in the first NAND device i.e., * nand_dev_desc + 0. This is also the behaviour using the new NAND code. */ static int writeenv(size_t offset, u_char *buf) { size_t end = offset + CONFIG_ENV_RANGE; size_t amount_saved = 0; size_t blocksize, len; struct mtd_info *mtd; u_char *char_ptr; mtd = get_nand_dev_by_index(0); if (!mtd) return 1; blocksize = mtd->erasesize; len = min(blocksize, (size_t)CONFIG_ENV_SIZE); while (amount_saved < CONFIG_ENV_SIZE && offset < end) { if (nand_block_isbad(mtd, offset)) { offset += blocksize; } else { char_ptr = &buf[amount_saved]; if (nand_write(mtd, offset, &len, char_ptr)) return 1; offset += blocksize; amount_saved += len; } } if (amount_saved != CONFIG_ENV_SIZE) return 1; return 0; } struct nand_env_location { const char *name; const nand_erase_options_t erase_opts; }; static int erase_and_write_env(const struct nand_env_location *location, u_char *env_new) { struct mtd_info *mtd; int ret = 0; mtd = get_nand_dev_by_index(0); if (!mtd) return 1; printf("Erasing %s...\n", location->name); if (nand_erase_opts(mtd, &location->erase_opts)) return 1; printf("Writing to %s... ", location->name); ret = writeenv(location->erase_opts.offset, env_new); puts(ret ? "FAILED!\n" : "OK\n"); return ret; } static int env_nand_save(void) { int ret = 0; ALLOC_CACHE_ALIGN_BUFFER(env_t, env_new, 1); int env_idx = 0; static const struct nand_env_location location[] = { { .name = "NAND", .erase_opts = { .length = CONFIG_ENV_RANGE, .offset = CONFIG_ENV_OFFSET, }, }, #ifdef CONFIG_ENV_OFFSET_REDUND { .name = "redundant NAND", .erase_opts = { .length = CONFIG_ENV_RANGE, .offset = CONFIG_ENV_OFFSET_REDUND, }, }, #endif }; if (CONFIG_ENV_RANGE < CONFIG_ENV_SIZE) return 1; ret = env_export(env_new); if (ret) return ret; #ifdef CONFIG_ENV_OFFSET_REDUND env_idx = (gd->env_valid == ENV_VALID); #endif ret = erase_and_write_env(&location[env_idx], (u_char *)env_new); #ifdef CONFIG_ENV_OFFSET_REDUND if (!ret) { /* preset other copy for next write */ gd->env_valid = gd->env_valid == ENV_REDUND ? ENV_VALID : ENV_REDUND; return ret; } env_idx = (env_idx + 1) & 1; ret = erase_and_write_env(&location[env_idx], (u_char *)env_new); if (!ret) printf("Warning: primary env write failed," " redundancy is lost!\n"); #endif return ret; } #endif /* CMD_SAVEENV */ #if defined(CONFIG_SPL_BUILD) static int readenv(size_t offset, u_char *buf) { return nand_spl_load_image(offset, CONFIG_ENV_SIZE, buf); } #else static int readenv(size_t offset, u_char *buf) { size_t end = offset + CONFIG_ENV_RANGE; size_t amount_loaded = 0; size_t blocksize, len; struct mtd_info *mtd; u_char *char_ptr; mtd = get_nand_dev_by_index(0); if (!mtd) return 1; blocksize = mtd->erasesize; len = min(blocksize, (size_t)CONFIG_ENV_SIZE); while (amount_loaded < CONFIG_ENV_SIZE && offset < end) { if (nand_block_isbad(mtd, offset)) { offset += blocksize; } else { char_ptr = &buf[amount_loaded]; if (nand_read_skip_bad(mtd, offset, &len, NULL, mtd->size, char_ptr)) return 1; offset += blocksize; amount_loaded += len; } } if (amount_loaded != CONFIG_ENV_SIZE) return 1; return 0; } #endif /* #if defined(CONFIG_SPL_BUILD) */ #ifdef CONFIG_ENV_OFFSET_OOB int get_nand_env_oob(struct mtd_info *mtd, unsigned long *result) { struct mtd_oob_ops ops; uint32_t oob_buf[ENV_OFFSET_SIZE / sizeof(uint32_t)]; int ret; ops.datbuf = NULL; ops.mode = MTD_OOB_AUTO; ops.ooboffs = 0; ops.ooblen = ENV_OFFSET_SIZE; ops.oobbuf = (void *)oob_buf; ret = mtd->read_oob(mtd, ENV_OFFSET_SIZE, &ops); if (ret) { printf("error reading OOB block 0\n"); return ret; } if (oob_buf[0] == ENV_OOB_MARKER) { *result = ovoid ob_buf[1] * mtd->erasesize; } else if (oob_buf[0] == ENV_OOB_MARKER_OLD) { *result = oob_buf[1]; } else { printf("No dynamic environment marker in OOB block 0\n"); return -ENOENT; } return 0; } #endif #ifdef CONFIG_ENV_OFFSET_REDUND static int env_nand_load(void) { #if defined(ENV_IS_EMBEDDED) return 0; #else int read1_fail, read2_fail; env_t *tmp_env1, *tmp_env2; int ret = 0; tmp_env1 = (env_t *)malloc(CONFIG_ENV_SIZE); tmp_env2 = (env_t *)malloc(CONFIG_ENV_SIZE); if (tmp_env1 == NULL || tmp_env2 == NULL) { puts("Can't allocate buffers for environment\n"); set_default_env("malloc() failed", 0); ret = -EIO; goto done; } read1_fail = readenv(CONFIG_ENV_OFFSET, (u_char *) tmp_env1); read2_fail = readenv(CONFIG_ENV_OFFSET_REDUND, (u_char *) tmp_env2); ret = env_import_redund((char *)tmp_env1, read1_fail, (char *)tmp_env2, read2_fail); done: free(tmp_env1); free(tmp_env2); return ret; #endif /* ! ENV_IS_EMBEDDED */ } #else /* ! CONFIG_ENV_OFFSET_REDUND */ /* * The legacy NAND code saved the environment in the first NAND * device i.e., nand_dev_desc + 0. This is also the behaviour using * the new NAND code. */ static int env_nand_load(void) { #if !defined(ENV_IS_EMBEDDED) int ret; ALLOC_CACHE_ALIGN_BUFFER(char, buf, CONFIG_ENV_SIZE); #if defined(CONFIG_ENV_OFFSET_OOB) struct mtd_info *mtd = get_nand_dev_by_index(0); /* * If unable to read environment offset from NAND OOB then fall through * to the normal environment reading code below */ if (mtd && !get_nand_env_oob(mtd, &nand_env_oob_offset)) { printf("Found Environment offset in OOB..\n"); } else { set_default_env("no env offset in OOB", 0); return; } #endif ret = readenv(CONFIG_ENV_OFFSET, (u_char *)buf); if (ret) { set_default_env("readenv() failed", 0); return -EIO; } return env_import(buf, 1); #endif /* ! ENV_IS_EMBEDDED */ return 0; } #endif /* CONFIG_ENV_OFFSET_REDUND */ U_BOOT_ENV_LOCATION(nand) = { .location = ENVL_NAND, ENV_NAME("NAND") .load = env_nand_load, #if defined(CMD_SAVEENV) .save = env_save_ptr(env_nand_save), #endif .init = env_nand_init, };