/* SPDX-License-Identifier: GPL-2.0+ */ /* * (C) Copyright 2000-2004 * Wolfgang Denk, DENX Software Engineering, wd@denx.de. */ #ifndef _PCMCIA_H #define _PCMCIA_H #include #include /* * Allow configuration to select PCMCIA slot, * or try to generate a useful default */ #if defined(CONFIG_CMD_PCMCIA) #if !defined(CONFIG_PCMCIA_SLOT_A) && !defined(CONFIG_PCMCIA_SLOT_B) # error "PCMCIA Slot not configured" #endif /* !defined(CONFIG_PCMCIA_SLOT_A) && !defined(CONFIG_PCMCIA_SLOT_B) */ /* Make sure exactly one slot is defined - we support only one for now */ #if !defined(CONFIG_PCMCIA_SLOT_A) && !defined(CONFIG_PCMCIA_SLOT_B) #error Neither CONFIG_PCMCIA_SLOT_A nor CONFIG_PCMCIA_SLOT_B configured #endif #if defined(CONFIG_PCMCIA_SLOT_A) && defined(CONFIG_PCMCIA_SLOT_B) #error Both CONFIG_PCMCIA_SLOT_A and CONFIG_PCMCIA_SLOT_B configured #endif #ifndef PCMCIA_SOCKETS_NO #define PCMCIA_SOCKETS_NO 1 #endif #ifndef PCMCIA_MEM_WIN_NO #define PCMCIA_MEM_WIN_NO 4 #endif #define PCMCIA_IO_WIN_NO 2 /* define _slot_ to be able to optimize macros */ #ifdef CONFIG_PCMCIA_SLOT_A # define _slot_ 0 # define PCMCIA_SLOT_MSG "slot A" # define PCMCIA_SLOT_x PCMCIA_PSLOT_A #else # define _slot_ 1 # define PCMCIA_SLOT_MSG "slot B" # define PCMCIA_SLOT_x PCMCIA_PSLOT_B #endif /* * This structure is used to address each window in the PCMCIA controller. * * Keep in mind that we assume that pcmcia_win_t[n+1] is mapped directly * after pcmcia_win_t[n]... */ typedef struct { ulong br; ulong or; } pcmcia_win_t; /**********************************************************************/ /* * CIS Tupel codes */ #define CISTPL_NULL 0x00 #define CISTPL_DEVICE 0x01 #define CISTPL_LONGLINK_CB 0x02 #define CISTPL_INDIRECT 0x03 #define CISTPL_CONFIG_CB 0x04 #define CISTPL_CFTABLE_ENTRY_CB 0x05 #define CISTPL_LONGLINK_MFC 0x06 #define CISTPL_BAR 0x07 #define CISTPL_PWR_MGMNT 0x08 #define CISTPL_EXTDEVICE 0x09 #define CISTPL_CHECKSUM 0x10 #define CISTPL_LONGLINK_A 0x11 #define CISTPL_LONGLINK_C 0x12 #define CISTPL_LINKTARGET 0x13 #define CISTPL_NO_LINK 0x14 #define CISTPL_VERS_1 0x15 #define CISTPL_ALTSTR 0x16 #define CISTPL_DEVICE_A 0x17 #define CISTPL_JEDEC_C 0x18 #define CISTPL_JEDEC_A 0x19 #define CISTPL_CONFIG 0x1a #define CISTPL_CFTABLE_ENTRY 0x1b #define CISTPL_DEVICE_OC 0x1c #define CISTPL_DEVICE_OA 0x1d #define CISTPL_DEVICE_GEO 0x1e #define CISTPL_DEVICE_GEO_A 0x1f #define CISTPL_MANFID 0x20 #define CISTPL_FUNCID 0x21 #define CISTPL_FUNCE 0x22 #define CISTPL_SWIL 0x23 #define CISTPL_END 0xff /* * CIS Function ID codes */ #define CISTPL_FUNCID_MULTI 0x00 #define CISTPL_FUNCID_MEMORY 0x01 #define CISTPL_FUNCID_SERIAL 0x02 #define CISTPL_FUNCID_PARALLEL 0x03 #define CISTPL_FUNCID_FIXED 0x04 #define CISTPL_FUNCID_VIDEO 0x05 #define CISTPL_FUNCID_NETWORK 0x06 #define CISTPL_FUNCID_AIMS 0x07 #define CISTPL_FUNCID_SCSI 0x08 /* * Fixed Disk FUNCE codes */ #define CISTPL_IDE_INTERFACE 0x01 #define CISTPL_FUNCE_IDE_IFACE 0x01 #define CISTPL_FUNCE_IDE_MASTER 0x02 #define CISTPL_FUNCE_IDE_SLAVE 0x03 /* First feature byte */ #define CISTPL_IDE_SILICON 0x04 #define CISTPL_IDE_UNIQUE 0x08 #define CISTPL_IDE_DUAL 0x10 /* Second feature byte */ #define CISTPL_IDE_HAS_SLEEP 0x01 #define CISTPL_IDE_HAS_STANDBY 0x02 #define CISTPL_IDE_HAS_IDLE 0x04 #define CISTPL_IDE_LOW_POWER 0x08 #define CISTPL_IDE_REG_INHIBIT 0x10 #define CISTPL_IDE_HAS_INDEX 0x20 #define CISTPL_IDE_IOIS16 0x40 #endif #endif /* _PCMCIA_H */