aboutsummaryrefslogtreecommitdiffstats
blob: 1a9a23b51b92443e076da9468831ed3352f2b0cf (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
!!! WARNING !!!

This guide describes to the old way of doing things. No new Ethernet drivers
should be implemented this way. All new drivers should be written against the
U-Boot core driver model. See doc/driver-model/README.txt

-----------------------
 Ethernet Driver Guide
-----------------------

The networking stack in Das U-Boot is designed for multiple network devices
to be easily added and controlled at runtime.  This guide is meant for people
who wish to review the net driver stack with an eye towards implementing your
own ethernet device driver.  Here we will describe a new pseudo 'APE' driver.

------------------
 Driver Functions
------------------

All functions you will be implementing in this document have the return value
meaning of 0 for success and non-zero for failure.

 ----------
  Register
 ----------

When U-Boot initializes, it will call the common function eth_initialize().
This will in turn call the board-specific board_eth_init() (or if that fails,
the cpu-specific cpu_eth_init()).  These board-specific functions can do random
system handling, but ultimately they will call the driver-specific register
function which in turn takes care of initializing that particular instance.

Keep in mind that you should code the driver to avoid storing state in global
data as someone might want to hook up two of the same devices to one board.
Any such information that is specific to an interface should be stored in a
private, driver-defined data structure and pointed to by eth->priv (see below).

So the call graph at this stage would look something like:
board_init()
	eth_initialize()
		board_eth_init() / cpu_eth_init()
			driver_register()
				initialize eth_device
				eth_register()

At this point in time, the only thing you need to worry about is the driver's
register function.  The pseudo code would look something like:
int ape_register(bd_t *bis, int iobase)
{
	struct ape_priv *priv;
	struct eth_device *dev;
	struct mii_dev *bus;

	priv = malloc(sizeof(*priv));
	if (priv == NULL)
		return -ENOMEM;

	dev = malloc(sizeof(*dev));
	if (dev == NULL) {
		free(priv);
		return -ENOMEM;
	}

	/* setup whatever private state you need */

	memset(dev, 0, sizeof(*dev));
	sprintf(dev->name, "APE");

	/*
	 * if your device has dedicated hardware storage for the
	 * MAC, read it and initialize dev->enetaddr with it
	 */
	ape_mac_read(dev->enetaddr);

	dev->iobase = iobase;
	dev->priv = priv;
	dev->init = ape_init;
	dev->halt = ape_halt;
	dev->send = ape_send;
	dev->recv = ape_recv;
	dev->write_hwaddr = ape_write_hwaddr;

	eth_register(dev);

#ifdef CONFIG_PHYLIB
	bus = mdio_alloc();
	if (!bus) {
		free(priv);
		free(dev);
		return -ENOMEM;
	}

	bus->read = ape_mii_read;
	bus->write = ape_mii_write;
	mdio_register(bus);
#endif

	return 1;
}

The exact arguments needed to initialize your device are up to you.  If you
need to pass more/less arguments, that's fine.  You should also add the
prototype for your new register function to include/netdev.h.

The return value for this function should be as follows:
< 0 - failure (hardware failure, not probe failure)
>=0 - number of interfaces detected

You might notice that many drivers seem to use xxx_initialize() rather than
xxx_register().  This is the old naming convention and should be avoided as it
causes confusion with the driver-specific init function.

Other than locating the MAC address in dedicated hardware storage, you should
not touch the hardware in anyway.  That step is handled in the driver-specific
init function.  Remember that we are only registering the device here, we are
not checking its state or doing random probing.

 -----------
  Callbacks
 -----------

Now that we've registered with the ethernet layer, we can start getting some
real work done.  You will need five functions:
	int ape_init(struct eth_device *dev, bd_t *bis);
	int ape_send(struct eth_device *dev, volatile void *packet, int length);
	int ape_recv(struct eth_device *dev);
	int ape_halt(struct eth_device *dev);
	int ape_write_hwaddr(struct eth_device *dev);

The init function checks the hardware (probing/identifying) and gets it ready
for send/recv operations.  You often do things here such as resetting the MAC
and/or PHY, and waiting for the link to autonegotiate.  You should also take
the opportunity to program the device's MAC address with the dev->enetaddr
member.  This allows the rest of U-Boot to dynamically change the MAC address
and have the new settings be respected.

The send function does what you think -- transmit the specified packet whose
size is specified by length (in bytes).  You should not return until the
transmission is complete, and you should leave the state such that the send
function can be called multiple times in a row.

The recv function should process packets as long as the hardware has them
readily available before returning.  i.e. you should drain the hardware fifo.
For each packet you receive, you should call the net_process_received_packet() function on it
along with the packet length.  The common code sets up packet buffers for you
already in the .bss (net_rx_packets), so there should be no need to allocate your
own.  This doesn't mean you must use the net_rx_packets array however; you're
free to call the net_process_received_packet() function with any buffer you wish.  So the pseudo
code here would look something like:
int ape_recv(struct eth_device *dev)
{
	int length, i = 0;
	...
	while (packets_are_available()) {
		...
		length = ape_get_packet(&net_rx_packets[i]);
		...
		net_process_received_packet(&net_rx_packets[i], length);
		...
		if (++i >= PKTBUFSRX)
			i = 0;
		...
	}
	...
	return 0;
}

The halt function should turn off / disable the hardware and place it back in
its reset state.  It can be called at any time (before any call to the related
init function), so make sure it can handle this sort of thing.

The write_hwaddr function should program the MAC address stored in dev->enetaddr
into the Ethernet controller.

So the call graph at this stage would look something like:
some net operation (ping / tftp / whatever...)
	eth_init()
		dev->init()
	eth_send()
		dev->send()
	eth_rx()
		dev->recv()
	eth_halt()
		dev->halt()

--------------------------------
 CONFIG_PHYLIB / CONFIG_CMD_MII
--------------------------------

If your device supports banging arbitrary values on the MII bus (pretty much
every device does), you should add support for the mii command.  Doing so is
fairly trivial and makes debugging mii issues a lot easier at runtime.

After you have called eth_register() in your driver's register function, add
a call to mdio_alloc() and mdio_register() like so:
	bus = mdio_alloc();
	if (!bus) {
		free(priv);
		free(dev);
		return -ENOMEM;
	}

	bus->read = ape_mii_read;
	bus->write = ape_mii_write;
	mdio_register(bus);

And then define the mii_read and mii_write functions if you haven't already.
Their syntax is straightforward:
	int mii_read(struct mii_dev *bus, int addr, int devad, int reg);
	int mii_write(struct mii_dev *bus, int addr, int devad, int reg,
		      u16 val);

The read function should read the register 'reg' from the phy at address 'addr'
and return the result to its caller.  The implementation for the write function
should logically follow.