aboutsummaryrefslogtreecommitdiffstats
blob: 9011109b47b781f30220f1c8b8296ac3d32de2f8 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
menu "Environment"

config ENV_IS_NOWHERE
	bool "Environment is not stored"
	depends on !ENV_IS_IN_EEPROM
	depends on !ENV_IS_IN_EXT4
	depends on !ENV_IS_IN_FAT
	depends on !ENV_IS_IN_FLASH
	depends on !ENV_IS_IN_MMC
	depends on !ENV_IS_IN_NAND
	depends on !ENV_IS_IN_NVRAM
	depends on !ENV_IS_IN_ONENAND
	depends on !ENV_IS_IN_REMOTE
	depends on !ENV_IS_IN_SPI_FLASH
	depends on !ENV_IS_IN_UBI
	default y
	help
	  Define this if you don't want to or can't have an environment stored
	  on a storage medium. In this case the environment will still exist
	  while U-Boot is running, but once U-Boot exits it will not be
	  stored. U-Boot will therefore always start up with a default
	  environment.

config ENV_IS_IN_EEPROM
	bool "Environment in EEPROM"
	depends on !CHAIN_OF_TRUST
	help
	  Use this if you have an EEPROM or similar serial access
	  device and a driver for it.

	  - CONFIG_ENV_OFFSET:
	  - CONFIG_ENV_SIZE:

	  These two #defines specify the offset and size of the
	  environment area within the total memory of your EEPROM.

	  Note that we consider the length of the address field to
	  still be one byte because the extra address bits are hidden
	  in the chip address.

	  - CONFIG_ENV_EEPROM_IS_ON_I2C
	  define this, if you have I2C and SPI activated, and your
	  EEPROM, which holds the environment, is on the I2C bus.

	  - CONFIG_I2C_ENV_EEPROM_BUS
	  if you have an Environment on an EEPROM reached over
	  I2C muxes, you can define here, how to reach this
	  EEPROM. For example:

	  #define CONFIG_I2C_ENV_EEPROM_BUS	  1

	  EEPROM which holds the environment, is reached over
	  a pca9547 i2c mux with address 0x70, channel 3.

config ENV_IS_IN_FAT
	bool "Environment is in a FAT filesystem"
	depends on !CHAIN_OF_TRUST
	default y if ARCH_BCM283X
	default y if ARCH_SUNXI && MMC
	default y if MMC_OMAP_HS && TI_COMMON_CMD_OPTIONS
	select FS_FAT
	select FAT_WRITE
	help
	  Define this if you want to use the FAT file system for the environment.

config ENV_IS_IN_EXT4
	bool "Environment is in a EXT4 filesystem"
	depends on !CHAIN_OF_TRUST
	select EXT4_WRITE
	help
	  Define this if you want to use the EXT4 file system for the environment.

config ENV_IS_IN_FLASH
	bool "Environment in flash memory"
	depends on !CHAIN_OF_TRUST
	default y if ARCH_CINTEGRATOR
	default y if ARCH_INTEGRATOR_CP
	default y if M548x || M547x || M5282 || MCF547x_8x
	default y if MCF532x || MCF52x2
	default y if MPC86xx || MPC83xx
	default y if ARCH_MPC8572 || ARCH_MPC8548 || ARCH_MPC8641
	default y if SH && !CPU_SH4
	help
	  Define this if you have a flash device which you want to use for the
	  environment.

	  a) The environment occupies one whole flash sector, which is
	   "embedded" in the text segment with the U-Boot code. This
	   happens usually with "bottom boot sector" or "top boot
	   sector" type flash chips, which have several smaller
	   sectors at the start or the end. For instance, such a
	   layout can have sector sizes of 8, 2x4, 16, Nx32 kB. In
	   such a case you would place the environment in one of the
	   4 kB sectors - with U-Boot code before and after it. With
	   "top boot sector" type flash chips, you would put the
	   environment in one of the last sectors, leaving a gap
	   between U-Boot and the environment.

	  CONFIG_ENV_OFFSET:

	   Offset of environment data (variable area) to the
	   beginning of flash memory; for instance, with bottom boot
	   type flash chips the second sector can be used: the offset
	   for this sector is given here.

	   CONFIG_ENV_OFFSET is used relative to CONFIG_SYS_FLASH_BASE.

	  CONFIG_ENV_ADDR:

	   This is just another way to specify the start address of
	   the flash sector containing the environment (instead of
	   CONFIG_ENV_OFFSET).

	  CONFIG_ENV_SECT_SIZE:

	   Size of the sector containing the environment.


	  b) Sometimes flash chips have few, equal sized, BIG sectors.
	   In such a case you don't want to spend a whole sector for
	   the environment.

	  CONFIG_ENV_SIZE:

	   If you use this in combination with CONFIG_ENV_IS_IN_FLASH
	   and CONFIG_ENV_SECT_SIZE, you can specify to use only a part
	   of this flash sector for the environment. This saves
	   memory for the RAM copy of the environment.

	   It may also save flash memory if you decide to use this
	   when your environment is "embedded" within U-Boot code,
	   since then the remainder of the flash sector could be used
	   for U-Boot code. It should be pointed out that this is
	   STRONGLY DISCOURAGED from a robustness point of view:
	   updating the environment in flash makes it always
	   necessary to erase the WHOLE sector. If something goes
	   wrong before the contents has been restored from a copy in
	   RAM, your target system will be dead.

	  CONFIG_ENV_ADDR_REDUND
	  CONFIG_ENV_SIZE_REDUND

	   These settings describe a second storage area used to hold
	   a redundant copy of the environment data, so that there is
	   a valid backup copy in case there is a power failure during
	   a "saveenv" operation.

	  BE CAREFUL! Any changes to the flash layout, and some changes to the
	  source code will make it necessary to adapt <board>/u-boot.lds*
	  accordingly!

config ENV_IS_IN_MMC
	bool "Environment in an MMC device"
	depends on !CHAIN_OF_TRUST
	depends on MMC
	default y if ARCH_EXYNOS4
	default y if MX6SX || MX7D
	default y if TEGRA30 || TEGRA124
	default y if TEGRA_ARMV8_COMMON
	help
	  Define this if you have an MMC device which you want to use for the
	  environment.

	  CONFIG_SYS_MMC_ENV_DEV:

	  Specifies which MMC device the environment is stored in.

	  CONFIG_SYS_MMC_ENV_PART (optional):

	  Specifies which MMC partition the environment is stored in. If not
	  set, defaults to partition 0, the user area. Common values might be
	  1 (first MMC boot partition), 2 (second MMC boot partition).

	  CONFIG_ENV_OFFSET:
	  CONFIG_ENV_SIZE:

	  These two #defines specify the offset and size of the environment
	  area within the specified MMC device.

	  If offset is positive (the usual case), it is treated as relative to
	  the start of the MMC partition. If offset is negative, it is treated
	  as relative to the end of the MMC partition. This can be useful if
	  your board may be fitted with different MMC devices, which have
	  different sizes for the MMC partitions, and you always want the
	  environment placed at the very end of the partition, to leave the
	  maximum possible space before it, to store other data.

	  These two values are in units of bytes, but must be aligned to an
	  MMC sector boundary.

	  CONFIG_ENV_OFFSET_REDUND (optional):

	  Specifies a second storage area, of CONFIG_ENV_SIZE size, used to
	  hold a redundant copy of the environment data. This provides a
	  valid backup copy in case the other copy is corrupted, e.g. due
	  to a power failure during a "saveenv" operation.

	  This value may also be positive or negative; this is handled in the
	  same way as CONFIG_ENV_OFFSET.

	  This value is also in units of bytes, but must also be aligned to
	  an MMC sector boundary.

	  CONFIG_ENV_SIZE_REDUND (optional):

	  This value need not be set, even when CONFIG_ENV_OFFSET_REDUND is
	  set. If this value is set, it must be set to the same value as
	  CONFIG_ENV_SIZE.

config ENV_IS_IN_NAND
	bool "Environment in a NAND device"
	depends on !CHAIN_OF_TRUST
	help
	  Define this if you have a NAND device which you want to use for the
	  environment.

	  - CONFIG_ENV_OFFSET:
	  - CONFIG_ENV_SIZE:

	  These two #defines specify the offset and size of the environment
	  area within the first NAND device.  CONFIG_ENV_OFFSET must be
	  aligned to an erase block boundary.

	  - CONFIG_ENV_OFFSET_REDUND (optional):

	  This setting describes a second storage area of CONFIG_ENV_SIZE
	  size used to hold a redundant copy of the environment data, so
	  that there is a valid backup copy in case there is a power failure
	  during a "saveenv" operation.	 CONFIG_ENV_OFFSET_REDUND must be
	  aligned to an erase block boundary.

	  - CONFIG_ENV_RANGE (optional):

	  Specifies the length of the region in which the environment
	  can be written.  This should be a multiple of the NAND device's
	  block size.  Specifying a range with more erase blocks than
	  are needed to hold CONFIG_ENV_SIZE allows bad blocks within
	  the range to be avoided.

	  - CONFIG_ENV_OFFSET_OOB (optional):

	  Enables support for dynamically retrieving the offset of the
	  environment from block zero's out-of-band data.  The
	  "nand env.oob" command can be used to record this offset.
	  Currently, CONFIG_ENV_OFFSET_REDUND is not supported when
	  using CONFIG_ENV_OFFSET_OOB.

config ENV_IS_IN_NVRAM
	bool "Environment in a non-volatile RAM"
	depends on !CHAIN_OF_TRUST
	help
	  Define this if you have some non-volatile memory device
	  (NVRAM, battery buffered SRAM) which you want to use for the
	  environment.

	  - CONFIG_ENV_ADDR:
	  - CONFIG_ENV_SIZE:

	  These two #defines are used to determine the memory area you
	  want to use for environment. It is assumed that this memory
	  can just be read and written to, without any special
	  provision.

config ENV_IS_IN_ONENAND
	bool "Environment is in OneNAND"
	depends on !CHAIN_OF_TRUST
	help
	  Define this if you want to put your local device's environment in
	  OneNAND.

	  - CONFIG_ENV_ADDR:
	  - CONFIG_ENV_SIZE:

	  These two #defines are used to determine the device range you
	  want to use for environment. It is assumed that this memory
	  can just be read and written to, without any special
	  provision.

config ENV_IS_IN_REMOTE
	bool "Environment is in remote memory space"
	depends on !CHAIN_OF_TRUST
	help
	  Define this if you have a remote memory space which you
	  want to use for the local device's environment.

	  - CONFIG_ENV_ADDR:
	  - CONFIG_ENV_SIZE:

	  These two #defines specify the address and size of the
	  environment area within the remote memory space. The
	  local device can get the environment from remote memory
	  space by SRIO or PCIE links.

config ENV_IS_IN_SPI_FLASH
	bool "Environment is in SPI flash"
	depends on !CHAIN_OF_TRUST
	default y if ARMADA_XP
	default y if INTEL_BAYTRAIL
	default y if INTEL_BRASWELL
	default y if INTEL_BROADWELL
	default y if NORTHBRIDGE_INTEL_IVYBRIDGE
	default y if INTEL_QUARK
	default y if INTEL_QUEENSBAY
	help
	  Define this if you have a SPI Flash memory device which you
	  want to use for the environment.

	  - CONFIG_ENV_OFFSET:
	  - CONFIG_ENV_SIZE:

	  These two #defines specify the offset and size of the
	  environment area within the SPI Flash. CONFIG_ENV_OFFSET must be
	  aligned to an erase sector boundary.

	  - CONFIG_ENV_SECT_SIZE:

	  Define the SPI flash's sector size.

	  - CONFIG_ENV_OFFSET_REDUND (optional):

	  This setting describes a second storage area of CONFIG_ENV_SIZE
	  size used to hold a redundant copy of the environment data, so
	  that there is a valid backup copy in case there is a power failure
	  during a "saveenv" operation. CONFIG_ENV_OFFSET_REDUND must be
	  aligned to an erase sector boundary.

	  - CONFIG_ENV_SPI_BUS (optional):
	  - CONFIG_ENV_SPI_CS (optional):

	  Define the SPI bus and chip select. If not defined they will be 0.

	  - CONFIG_ENV_SPI_MAX_HZ (optional):

	  Define the SPI max work clock. If not defined then use 1MHz.

	  - CONFIG_ENV_SPI_MODE (optional):

	  Define the SPI work mode. If not defined then use SPI_MODE_3.

config ENV_IS_IN_UBI
	bool "Environment in a UBI volume"
	depends on !CHAIN_OF_TRUST
	help
	  Define this if you have an UBI volume that you want to use for the
	  environment.  This has the benefit of wear-leveling the environment
	  accesses, which is important on NAND.

	  - CONFIG_ENV_UBI_PART:

	  Define this to a string that is the mtd partition containing the UBI.

	  - CONFIG_ENV_UBI_VOLUME:

	  Define this to the name of the volume that you want to store the
	  environment in.

	  - CONFIG_ENV_UBI_VOLUME_REDUND:

	  Define this to the name of another volume to store a second copy of
	  the environment in.  This will enable redundant environments in UBI.
	  It is assumed that both volumes are in the same MTD partition.

config ENV_FAT_INTERFACE
	string "Name of the block device for the environment"
	depends on ENV_IS_IN_FAT
	default "mmc" if ARCH_SUNXI
	default "mmc" if TI_COMMON_CMD_OPTIONS || ARCH_ZYNQMP || ARCH_AT91
	help
	  Define this to a string that is the name of the block device.

config ENV_FAT_DEVICE_AND_PART
	string "Device and partition for where to store the environemt in FAT"
	depends on ENV_IS_IN_FAT
	default "0:1" if TI_COMMON_CMD_OPTIONS
	default "0:auto" if ARCH_ZYNQMP
	default "0:auto" if ARCH_SUNXI && MMC_SUNXI_SLOT_EXTRA = -1
	default "1:auto" if ARCH_SUNXI && MMC_SUNXI_SLOT_EXTRA != -1
	default "0" if ARCH_AT91
	help
	  Define this to a string to specify the partition of the device. It can
	  be as following:

	    "D:P", "D:0", "D", "D:" or "D:auto" (D, P are integers. And P >= 1)
	       - "D:P": device D partition P. Error occurs if device D has no
	                partition table.
	       - "D:0": device D.
	       - "D" or "D:": device D partition 1 if device D has partition
	                      table, or the whole device D if has no partition
	                      table.
	       - "D:auto": first partition in device D with bootable flag set.
	                   If none, first valid partition in device D. If no
	                   partition table then means device D.

config ENV_FAT_FILE
	string "Name of the FAT file to use for the environment"
	depends on ENV_IS_IN_FAT
	default "uboot.env"
	help
	  It's a string of the FAT file name. This file use to store the
	  environment.

config ENV_EXT4_INTERFACE
	string "Name of the block device for the environment"
	depends on ENV_IS_IN_EXT4
	help
	  Define this to a string that is the name of the block device.

config ENV_EXT4_DEVICE_AND_PART
	string "Device and partition for where to store the environemt in EXT4"
	depends on ENV_IS_IN_EXT4
	help
	  Define this to a string to specify the partition of the device. It can
	  be as following:

	    "D:P", "D:0", "D", "D:" or "D:auto" (D, P are integers. And P >= 1)
	       - "D:P": device D partition P. Error occurs if device D has no
	                partition table.
	       - "D:0": device D.
	       - "D" or "D:": device D partition 1 if device D has partition
	                      table, or the whole device D if has no partition
	                      table.
	       - "D:auto": first partition in device D with bootable flag set.
	                   If none, first valid partition in device D. If no
	                   partition table then means device D.

config ENV_EXT4_FILE
	string "Name of the EXT4 file to use for the environment"
	depends on ENV_IS_IN_EXT4
	default "uboot.env"
	help
	  It's a string of the EXT4 file name. This file use to store the
	  environment (explicit path to the file)

if ARCH_ROCKCHIP || ARCH_SUNXI || ARCH_ZYNQ || ARCH_ZYNQMP || ARCH_VERSAL

config ENV_OFFSET
	hex "Environment Offset"
	depends on !ENV_IS_IN_UBI
	depends on !ENV_IS_NOWHERE
	default 0x3f8000 if ARCH_ROCKCHIP
	default 0x88000 if ARCH_SUNXI
	default 0xE0000 if ARCH_ZYNQ
	default 0x1E00000 if ARCH_ZYNQMP
	help
	  Offset from the start of the device (or partition)

config ENV_SIZE
	hex "Environment Size"
	default 0x40000 if ENV_IS_IN_SPI_FLASH && ARCH_ZYNQMP
	default 0x20000 if ARCH_SUNXI || ARCH_ZYNQ
	default 0x8000 if ARCH_ROCKCHIP || ARCH_ZYNQMP || ARCH_VERSAL
	help
	  Size of the environment storage area

config ENV_SECT_SIZE
	hex "Environment Sector-Size"
	depends on !ENV_IS_NOWHERE && (ARCH_ZYNQ || ARCH_ZYNQMP)
	default 0x40000 if ARCH_ZYNQMP
	default 0x20000 if ARCH_ZYNQ
	help
	  Size of the sector containing the environment.

config ENV_UBI_PART
	string "UBI partition name"
	depends on ENV_IS_IN_UBI
	help
	  MTD partition containing the UBI device

config ENV_UBI_VOLUME
	string "UBI volume name"
	depends on ENV_IS_IN_UBI
	help
	  Name of the volume that you want to store the environment in.

endif

config USE_DEFAULT_ENV_FILE
	bool "Create default environment from file"
	help
	  Normally, the default environment is automatically generated
	  based on the settings of various CONFIG_* options, as well
	  as the CONFIG_EXTRA_ENV_SETTINGS. By selecting this option,
	  you can instead define the entire default environment in an
	  external file.

config DEFAULT_ENV_FILE
	string "Path to default environment file"
	depends on USE_DEFAULT_ENV_FILE
	help
	  The path containing the default environment. The format is
	  the same as accepted by the mkenvimage tool: lines
	  containing key=value pairs, blank lines and lines beginning
	  with # are ignored.

config ENV_VARS_UBOOT_RUNTIME_CONFIG
	bool "Add run-time information to the environment"
	help
	  Enable this in order to add variables describing certain
	  run-time determined information about the hardware to the
	  environment.  These will be named board_name, board_rev.

if SPL_ENV_SUPPORT
config SPL_ENV_IS_NOWHERE
	bool "SPL Environment is not stored"
	default y if ENV_IS_NOWHERE
	help
	  Similar to ENV_IS_NOWHERE, used for SPL environment.

config SPL_ENV_IS_IN_MMC
	bool "SPL Environment in an MMC device"
	depends on !SPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_MMC
	default y
	help
	  Similar to ENV_IS_IN_MMC, used for SPL environment.

config SPL_ENV_IS_IN_FAT
	bool "SPL Environment is in a FAT filesystem"
	depends on !SPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_FAT
	default y
	help
	  Similar to ENV_IS_IN_FAT, used for SPL environment.

config SPL_ENV_IS_IN_EXT4
	bool "SPL Environment is in a EXT4 filesystem"
	depends on !SPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_EXT4
	default y
	help
	  Similar to ENV_IS_IN_EXT4, used for SPL environment.

config SPL_ENV_IS_IN_NAND
	bool "SPL Environment in a NAND device"
	depends on !SPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_NAND
	default y
	help
	  Similar to ENV_IS_IN_NAND, used for SPL environment.

config SPL_ENV_IS_IN_SPI_FLASH
	bool "SPL Environment is in SPI flash"
	depends on !SPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_SPI_FLASH
	default y
	help
	  Similar to ENV_IS_IN_SPI_FLASH, used for SPL environment.

config SPL_ENV_IS_IN_FLASH
	bool "SPL Environment in flash memory"
	depends on !SPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_FLASH
	default y
	help
	  Similar to ENV_IS_IN_FLASH, used for SPL environment.

endif

if TPL_ENV_SUPPORT

config TPL_ENV_IS_NOWHERE
	bool "TPL Environment is not stored"
	default y if ENV_IS_NOWHERE
	help
	  Similar to ENV_IS_NOWHERE, used for TPL environment.

config TPL_ENV_IS_IN_MMC
	bool "TPL Environment in an MMC device"
	depends on !TPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_MMC
	default y
	help
	  Similar to ENV_IS_IN_MMC, used for TPL environment.

config TPL_ENV_IS_IN_FAT
	bool "TPL Environment is in a FAT filesystem"
	depends on !TPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_FAT
	default y
	help
	  Similar to ENV_IS_IN_FAT, used for TPL environment.

config TPL_ENV_IS_IN_EXT4
	bool "TPL Environment is in a EXT4 filesystem"
	depends on !TPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_EXT4
	default y
	help
	  Similar to ENV_IS_IN_EXT4, used for TPL environment.

config TPL_ENV_IS_IN_NAND
	bool "TPL Environment in a NAND device"
	depends on !TPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_NAND
	default y
	help
	  Similar to ENV_IS_IN_NAND, used for TPL environment.

config TPL_ENV_IS_IN_SPI_FLASH
	bool "TPL Environment is in SPI flash"
	depends on !TPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_SPI_FLASH
	default y
	help
	  Similar to ENV_IS_IN_SPI_FLASH, used for TPL environment.

config TPL_ENV_IS_IN_FLASH
	bool "TPL Environment in flash memory"
	depends on !TPL_ENV_IS_NOWHERE
	depends on ENV_IS_IN_FLASH
	default y
	help
	  Similar to ENV_IS_IN_FLASH, used for TPL environment.

endif

endmenu