aboutsummaryrefslogtreecommitdiffstats
blob: 72d8b96f54140c535276040890d5dfc2d05997cd (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
// SPDX-License-Identifier: GPL-2.0+
/*
 * Copyright (C) 2014 Charles Manning <cdhmanning@gmail.com>
 *
 * Reference documents:
 *   Cyclone V SoC: https://www.altera.com/content/dam/altera-www/global/en_US/pdfs/literature/hb/cyclone-v/cv_5400a.pdf
 *   Arria V SoC:   https://www.altera.com/content/dam/altera-www/global/en_US/pdfs/literature/hb/arria-v/av_5400a.pdf
 *   Arria 10 SoC:  https://www.altera.com/content/dam/altera-www/global/en_US/pdfs/literature/hb/arria-10/a10_5400a.pdf
 *
 * Bootable SoCFPGA image requires a structure of the following format
 * positioned at offset 0x40 of the bootable image. Endian is LSB.
 *
 * There are two versions of the SoCFPGA header format, v0 and v1.
 * The version 0 is used by Cyclone V SoC and Arria V SoC, while
 * the version 1 is used by the Arria 10 SoC.
 *
 * Version 0:
 * Offset   Length   Usage
 * -----------------------
 *   0x40        4   Validation word (0x31305341)
 *   0x44        1   Version (0x0)
 *   0x45        1   Flags (unused, zero is fine)
 *   0x46        2   Length (in units of u32, including the end checksum).
 *   0x48        2   Zero (0x0)
 *   0x4A        2   Checksum over the header. NB Not CRC32
 *
 * Version 1:
 * Offset   Length   Usage
 * -----------------------
 *   0x40        4   Validation word (0x31305341)
 *   0x44        1   Version (0x1)
 *   0x45        1   Flags (unused, zero is fine)
 *   0x46        2   Header length (in units of u8).
 *   0x48        4   Length (in units of u8).
 *   0x4C        4   Image entry offset from standard of header
 *   0x50        2   Zero (0x0)
 *   0x52        2   Checksum over the header. NB Not CRC32
 *
 * At the end of the code we have a 32-bit CRC checksum over whole binary
 * excluding the CRC.
 *
 * Note that the CRC used here is **not** the zlib/Adler crc32. It is the
 * CRC-32 used in bzip2, ethernet and elsewhere.
 *
 * The Image entry offset in version 1 image is relative the the start of
 * the header, 0x40, and must not be a negative number. Therefore, it is
 * only possible to make the SoCFPGA jump forward. The U-Boot bootloader
 * places a trampoline instruction at offset 0x5c, 0x14 bytes from the
 * start of the SoCFPGA header, which jumps to the reset vector.
 *
 * The image is padded out to 64k, because that is what is
 * typically used to write the image to the boot medium.
 */

#include "pbl_crc32.h"
#include "imagetool.h"
#include "mkimage.h"

#include <image.h>

#define HEADER_OFFSET	0x40
#define VALIDATION_WORD	0x31305341

static uint8_t buffer_v0[0x10000];
static uint8_t buffer_v1[0x40000];

struct socfpga_header_v0 {
	uint32_t	validation;
	uint8_t		version;
	uint8_t		flags;
	uint16_t	length_u32;
	uint16_t	zero;
	uint16_t	checksum;
};

struct socfpga_header_v1 {
	uint32_t	validation;
	uint8_t		version;
	uint8_t		flags;
	uint16_t	header_u8;
	uint32_t	length_u8;
	uint32_t	entry_offset;
	uint16_t	zero;
	uint16_t	checksum;
};

static unsigned int sfp_hdr_size(uint8_t ver)
{
	if (ver == 0)
		return sizeof(struct socfpga_header_v0);
	if (ver == 1)
		return sizeof(struct socfpga_header_v1);
	return 0;
}

static unsigned int sfp_pad_size(uint8_t ver)
{
	if (ver == 0)
		return sizeof(buffer_v0);
	if (ver == 1)
		return sizeof(buffer_v1);
	return 0;
}

/*
 * The header checksum is just a very simple checksum over
 * the header area.
 * There is still a crc32 over the whole lot.
 */
static uint16_t sfp_hdr_checksum(uint8_t *buf, unsigned char ver)
{
	uint16_t ret = 0;
	int len = sfp_hdr_size(ver) - sizeof(ret);

	while (--len)
		ret += *buf++;

	return ret;
}

static void sfp_build_header(uint8_t *buf, uint8_t ver, uint8_t flags,
			     uint32_t length_bytes)
{
	struct socfpga_header_v0 header_v0 = {
		.validation	= cpu_to_le32(VALIDATION_WORD),
		.version	= 0,
		.flags		= flags,
		.length_u32	= cpu_to_le16(length_bytes / 4),
		.zero		= 0,
	};

	struct socfpga_header_v1 header_v1 = {
		.validation	= cpu_to_le32(VALIDATION_WORD),
		.version	= 1,
		.flags		= flags,
		.header_u8	= cpu_to_le16(sizeof(header_v1)),
		.length_u8	= cpu_to_le32(length_bytes),
		.entry_offset	= cpu_to_le32(0x14),	/* Trampoline offset */
		.zero		= 0,
	};

	uint16_t csum;

	if (ver == 0) {
		csum = sfp_hdr_checksum((uint8_t *)&header_v0, 0);
		header_v0.checksum = cpu_to_le16(csum);
		memcpy(buf, &header_v0, sizeof(header_v0));
	} else {
		csum = sfp_hdr_checksum((uint8_t *)&header_v1, 1);
		header_v1.checksum = cpu_to_le16(csum);
		memcpy(buf, &header_v1, sizeof(header_v1));
	}
}

/*
 * Perform a rudimentary verification of header and return
 * size of image.
 */
static int sfp_verify_header(const uint8_t *buf, uint8_t *ver)
{
	struct socfpga_header_v0 header_v0;
	struct socfpga_header_v1 header_v1;
	uint16_t hdr_csum, sfp_csum;
	uint32_t img_len;

	/*
	 * Header v0 is always smaller than Header v1 and the validation
	 * word and version field is at the same place, so use Header v0
	 * to check for version during verifiction and upgrade to Header
	 * v1 if needed.
	 */
	memcpy(&header_v0, buf, sizeof(header_v0));

	if (le32_to_cpu(header_v0.validation) != VALIDATION_WORD)
		return -1;

	if (header_v0.version == 0) {
		hdr_csum = le16_to_cpu(header_v0.checksum);
		sfp_csum = sfp_hdr_checksum((uint8_t *)&header_v0, 0);
		img_len = le16_to_cpu(header_v0.length_u32) * 4;
	} else if (header_v0.version == 1) {
		memcpy(&header_v1, buf, sizeof(header_v1));
		hdr_csum = le16_to_cpu(header_v1.checksum);
		sfp_csum = sfp_hdr_checksum((uint8_t *)&header_v1, 1);
		img_len = le32_to_cpu(header_v1.length_u8);
	} else {	/* Invalid version */
		return -EINVAL;
	}

	/* Verify checksum */
	if (hdr_csum != sfp_csum)
		return -EINVAL;

	*ver = header_v0.version;
	return img_len;
}

/* Sign the buffer and return the signed buffer size */
static int sfp_sign_buffer(uint8_t *buf, uint8_t ver, uint8_t flags,
			   int len, int pad_64k)
{
	uint32_t calc_crc;

	/* Align the length up */
	len = (len + 3) & ~3;

	/* Build header, adding 4 bytes to length to hold the CRC32. */
	sfp_build_header(buf + HEADER_OFFSET, ver, flags, len + 4);

	/* Calculate and apply the CRC */
	calc_crc = ~pbl_crc32(0, (char *)buf, len);

	*((uint32_t *)(buf + len)) = cpu_to_le32(calc_crc);

	if (!pad_64k)
		return len + 4;

	return sfp_pad_size(ver);
}

/* Verify that the buffer looks sane */
static int sfp_verify_buffer(const uint8_t *buf)
{
	int len; /* Including 32bit CRC */
	uint32_t calc_crc;
	uint32_t buf_crc;
	uint8_t ver = 0;

	len = sfp_verify_header(buf + HEADER_OFFSET, &ver);
	if (len < 0) {
		debug("Invalid header\n");
		return -1;
	}

	if (len < HEADER_OFFSET || len > sfp_pad_size(ver)) {
		debug("Invalid header length (%i)\n", len);
		return -1;
	}

	/*
	 * Adjust length to the base of the CRC.
	 * Check the CRC.
	*/
	len -= 4;

	calc_crc = ~pbl_crc32(0, (const char *)buf, len);

	buf_crc = le32_to_cpu(*((uint32_t *)(buf + len)));

	if (buf_crc != calc_crc) {
		fprintf(stderr, "CRC32 does not match (%08x != %08x)\n",
			buf_crc, calc_crc);
		return -1;
	}

	return 0;
}

/* mkimage glue functions */
static int socfpgaimage_verify_header(unsigned char *ptr, int image_size,
				      struct image_tool_params *params)
{
	if (image_size < 0x80)
		return -1;

	return sfp_verify_buffer(ptr);
}

static void socfpgaimage_print_header(const void *ptr)
{
	if (sfp_verify_buffer(ptr) == 0)
		printf("Looks like a sane SOCFPGA preloader\n");
	else
		printf("Not a sane SOCFPGA preloader\n");
}

static int socfpgaimage_check_params(struct image_tool_params *params)
{
	/* Not sure if we should be accepting fflags */
	return	(params->dflag && (params->fflag || params->lflag)) ||
		(params->fflag && (params->dflag || params->lflag)) ||
		(params->lflag && (params->dflag || params->fflag));
}

static int socfpgaimage_check_image_types_v0(uint8_t type)
{
	if (type == IH_TYPE_SOCFPGAIMAGE)
		return EXIT_SUCCESS;
	return EXIT_FAILURE;
}

static int socfpgaimage_check_image_types_v1(uint8_t type)
{
	if (type == IH_TYPE_SOCFPGAIMAGE_V1)
		return EXIT_SUCCESS;
	return EXIT_FAILURE;
}

/*
 * To work in with the mkimage framework, we do some ugly stuff...
 *
 * First, socfpgaimage_vrec_header() is called.
 * We prepend a fake header big enough to make the file sfp_pad_size().
 * This gives us enough space to do what we want later.
 *
 * Next, socfpgaimage_set_header() is called.
 * We fix up the buffer by moving the image to the start of the buffer.
 * We now have some room to do what we need (add CRC and padding).
 */

static int data_size;

static int sfp_fake_header_size(unsigned int size, uint8_t ver)
{
	return sfp_pad_size(ver) - size;
}

static int sfp_vrec_header(struct image_tool_params *params,
			   struct image_type_params *tparams, uint8_t ver)
{
	struct stat sbuf;

	if (params->datafile &&
	    stat(params->datafile, &sbuf) == 0 &&
	    sbuf.st_size <= (sfp_pad_size(ver) - sizeof(uint32_t))) {
		data_size = sbuf.st_size;
		tparams->header_size = sfp_fake_header_size(data_size, ver);
	}
	return 0;

}

static int socfpgaimage_vrec_header_v0(struct image_tool_params *params,
				       struct image_type_params *tparams)
{
	return sfp_vrec_header(params, tparams, 0);
}

static int socfpgaimage_vrec_header_v1(struct image_tool_params *params,
				       struct image_type_params *tparams)
{
	return sfp_vrec_header(params, tparams, 1);
}

static void sfp_set_header(void *ptr, unsigned char ver)
{
	uint8_t *buf = (uint8_t *)ptr;

	/*
	 * This function is called after vrec_header() has been called.
	 * At this stage we have the sfp_fake_header_size() dummy bytes
	 * followed by data_size image bytes. Total = sfp_pad_size().
	 * We need to fix the buffer by moving the image bytes back to
	 * the beginning of the buffer, then actually do the signing stuff...
	 */
	memmove(buf, buf + sfp_fake_header_size(data_size, ver), data_size);
	memset(buf + data_size, 0, sfp_fake_header_size(data_size, ver));

	sfp_sign_buffer(buf, ver, 0, data_size, 0);
}

static void socfpgaimage_set_header_v0(void *ptr, struct stat *sbuf, int ifd,
				       struct image_tool_params *params)
{
	sfp_set_header(ptr, 0);
}

static void socfpgaimage_set_header_v1(void *ptr, struct stat *sbuf, int ifd,
				       struct image_tool_params *params)
{
	sfp_set_header(ptr, 1);
}

U_BOOT_IMAGE_TYPE(
	socfpgaimage,
	"Altera SoCFPGA Cyclone V / Arria V image support",
	0, /* This will be modified by vrec_header() */
	(void *)buffer_v0,
	socfpgaimage_check_params,
	socfpgaimage_verify_header,
	socfpgaimage_print_header,
	socfpgaimage_set_header_v0,
	NULL,
	socfpgaimage_check_image_types_v0,
	NULL,
	socfpgaimage_vrec_header_v0
);

U_BOOT_IMAGE_TYPE(
	socfpgaimage_v1,
	"Altera SoCFPGA Arria10 image support",
	0, /* This will be modified by vrec_header() */
	(void *)buffer_v1,
	socfpgaimage_check_params,
	socfpgaimage_verify_header,
	socfpgaimage_print_header,
	socfpgaimage_set_header_v1,
	NULL,
	socfpgaimage_check_image_types_v1,
	NULL,
	socfpgaimage_vrec_header_v1
);