summaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* ARM_User_Space_App: resize the terminal to print out all linesHEADmasterHongmei Gou2019-04-171-0/+3
| | | | | | | | * This is required when running the user space application with processor sdk filesystem on NFS, which has screen size of 24 rows, and cannot print out the last several lines for Delay/Compensation, Estimated Frequency, and etc. Signed-off-by: Hongmei Gou <a0271529@ti.com>
* ARM_User_Space_App: Makefile: remove ARM_CCT and use CCHongmei Gou2018-09-061-18/+1
| | | | | | * CC is defined from Processor SDK Linux Signed-off-by: Hongmei Gou <a0271529@ti.com>
* Updating the run.sh script to include the output enable GPIOJason Reeder2018-08-021-0/+10
| | | | Signed-off-by: Jason Reeder <jreeder@ti.com>
* Updating the dts file to include the output enable GPIOJason Reeder2018-08-021-0/+1
| | | | Signed-off-by: Jason Reeder <jreeder@ti.com>
* Change the frequency estimation channel index to be 1 basedJason Reeder2018-08-021-6/+6
| | | | Signed-off-by: Jason Reeder <jreeder@ti.com>
* Change the out of box frequency estimation deviceJason Reeder2018-08-021-1/+1
| | | | Signed-off-by: Jason Reeder <jreeder@ti.com>
* More description user space app display outputJason Reeder2018-08-021-2/+2
| | | | Signed-off-by: Jason Reeder <jreeder@ti.com>
* Fixed a bug that could cause a lockup to occurJason Reeder2018-08-021-1/+2
| | | | | | | | | | | | | | | There was one handshake that did not use a temporary variable before checking the value in the while loop. Without the temporary variable the XIN instruction may place the value to be checked into a different core register than the one being checked. This commit adds a temporary variable in order to force the compiler to copy the value to the variable being checked by the while loop. All other while loops involving the XIN instruction already used this method. Signed-off-by: Jason Reeder <jreeder@ti.com>
* Ignoring/removing temporary vim filesJason Reeder2018-02-012-0/+2
| | | | Signed-off-by: Jason Reeder <jreeder@ti.com>
* Fix channel configuration commentJason Reeder2018-02-011-1/+1
| | | | Signed-off-by: Jason Reeder <jreeder@ti.com>
* Adding .gitignore to ignore generated filesJason Reeder2018-02-011-0/+1
| | | | Signed-off-by: Jason Reeder <jreeder@ti.com>
* Removing generated filesJason Reeder2018-02-019-4393/+0
| | | | Signed-off-by: Jason Reeder <jreeder@ti.com>
* Initial commitJason Reeder2017-12-2023-0/+6463
Signed-off-by: Jason Reeder <jreeder@ti.com>