summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'sample-files/denzil/local-arago-linaro.conf.sample')
-rw-r--r--sample-files/denzil/local-arago-linaro.conf.sample3
1 files changed, 0 insertions, 3 deletions
diff --git a/sample-files/denzil/local-arago-linaro.conf.sample b/sample-files/denzil/local-arago-linaro.conf.sample
index 0bfcc03..ba542c9 100644
--- a/sample-files/denzil/local-arago-linaro.conf.sample
+++ b/sample-files/denzil/local-arago-linaro.conf.sample
@@ -119,9 +119,6 @@ USER_CLASSES ?= "buildstats image-mklibs image-prelink"
119# By default disable interactive patch resolution (tasks will just fail instead): 119# By default disable interactive patch resolution (tasks will just fail instead):
120PATCHRESOLVE = "noop" 120PATCHRESOLVE = "noop"
121 121
122# Qemu 0.12.x is giving too much problems recently (2010.05), so disable it for users
123ENABLE_BINARY_LOCALE_GENERATION = "0"
124
125# By default the machine configuration file sets the IMAGE_FSTYPES. But if you 122# By default the machine configuration file sets the IMAGE_FSTYPES. But if you
126# would like to add additional file system types you can uncomment the 123# would like to add additional file system types you can uncomment the
127# following line and add the additional IMAGE_FSTYPES you want created 124# following line and add the additional IMAGE_FSTYPES you want created