diff options
Diffstat (limited to 'sample-files/local-arago64.conf.sample')
-rw-r--r-- | sample-files/local-arago64.conf.sample | 3 |
1 files changed, 0 insertions, 3 deletions
diff --git a/sample-files/local-arago64.conf.sample b/sample-files/local-arago64.conf.sample index 6d7af90..6b77547 100644 --- a/sample-files/local-arago64.conf.sample +++ b/sample-files/local-arago64.conf.sample | |||
@@ -122,9 +122,6 @@ USER_CLASSES ?= "buildstats image-mklibs image-prelink" | |||
122 | # By default disable interactive patch resolution (tasks will just fail instead): | 122 | # By default disable interactive patch resolution (tasks will just fail instead): |
123 | PATCHRESOLVE = "noop" | 123 | PATCHRESOLVE = "noop" |
124 | 124 | ||
125 | # Qemu 0.12.x is giving too much problems recently (2010.05), so disable it for users | ||
126 | ENABLE_BINARY_LOCALE_GENERATION = "0" | ||
127 | |||
128 | # By default the machine configuration file sets the IMAGE_FSTYPES. But if you | 125 | # By default the machine configuration file sets the IMAGE_FSTYPES. But if you |
129 | # would like to add additional file system types you can uncomment the | 126 | # would like to add additional file system types you can uncomment the |
130 | # following line and add the additional IMAGE_FSTYPES you want created | 127 | # following line and add the additional IMAGE_FSTYPES you want created |