aboutsummaryrefslogtreecommitdiffstats
blob: f997b46783bf2ee76dcbbd190d05a709bad21ccc (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
/*
 * Copyright (c) 2017-2020, ARM Limited and Contributors. All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

#include <arch.h>
#include <asm_macros.S>
#include <cortex_a72.h>
#include <cpu_macros.S>
#include <platform_def.h>

#define K3_BOOT_REASON_COLD_RESET 0x1

	/* ------------------------------------------------------------------
	 *  uintptr_t plat_get_my_entrypoint(void)
	 * ------------------------------------------------------------------
	 *
	 * This function is called with the called with the MMU and caches
	 * disabled (SCTLR_EL3.M = 0 and SCTLR_EL3.C = 0). The function is
	 * responsible for distinguishing between a warm and cold reset for the
	 * current CPU using platform-specific means. If it's a warm reset,
	 * then it returns the warm reset entrypoint point provided to
	 * plat_setup_psci_ops() during BL31 initialization. If it's a cold
	 * reset then this function must return zero.
	 *
	 * This function does not follow the Procedure Call Standard used by
	 * the Application Binary Interface for the ARM 64-bit architecture.
	 * The caller should not assume that callee saved registers are
	 * preserved across a call to this function.
	 */
	.globl	plat_get_my_entrypoint
func plat_get_my_entrypoint
	ldr x0, k3_boot_reason_data_store
	cmp  x0, #K3_BOOT_REASON_COLD_RESET

	/* We ONLY support cold boot at this point */
	bne plat_unsupported_boot
	mov	x0, #0
	ret

	/*
	 * We self manage our boot reason.
	 * At load time, we have just a default reason - which is cold reset
	 */
k3_boot_reason_data_store:
	.word	K3_BOOT_REASON_COLD_RESET

plat_unsupported_boot:
	b plat_unsupported_boot

endfunc plat_get_my_entrypoint

	/* ------------------------------------------------------------------
	 * unsigned int plat_my_core_pos(void)
	 * ------------------------------------------------------------------
	 *
	 * This function returns the index of the calling CPU which is used as a
	 * CPU-specific linear index into blocks of memory (for example while
	 * allocating per-CPU stacks). This function will be invoked very early
	 * in the initialization sequence which mandates that this function
	 * should be implemented in assembly and should not rely on the
	 * avalability of a C runtime environment. This function can clobber x0
	 * - x8 and must preserve x9 - x29.
	 *
	 * This function plays a crucial role in the power domain topology
	 * framework in PSCI and details of this can be found in Power Domain
	 * Topology Design.
	 */
	.globl plat_my_core_pos
func plat_my_core_pos
	mrs	x0, MPIDR_EL1

	and	x1, x0, #MPIDR_CLUSTER_MASK
	lsr	x1, x1, #MPIDR_AFF1_SHIFT
	and	x0, x0, #MPIDR_CPU_MASK

	cmp	x1, 0
	b.eq out
	add	x0, x0, #K3_CLUSTER0_CORE_COUNT

	cmp	x1, 1
	b.eq out
	add	x0, x0, #K3_CLUSTER1_CORE_COUNT

	cmp	x1, 2
	b.eq out
	add	x0, x0, #K3_CLUSTER2_CORE_COUNT

out:
	ret
endfunc plat_my_core_pos

	/* --------------------------------------------------------------------
	 * This handler does the following:
	 * - Set the L2 Data RAM latency to 2 (i.e. 3 cycles) for Cortex-A72
	 * --------------------------------------------------------------------
	 */
	.globl plat_reset_handler
func plat_reset_handler
	/* Only on Cortex-A72 */
	jump_if_cpu_midr CORTEX_A72_MIDR, a72
	ret

	/* Cortex-A72 specific settings */
a72:
	mrs x0, CORTEX_A72_L2CTLR_EL1
#if K3_DATA_RAM_4_LATENCY
	/* Set L2 cache data RAM latency to 4 cycles */
	orr x0, x0, #(CORTEX_A72_L2_DATA_RAM_LATENCY_4_CYCLES << \
			CORTEX_A72_L2CTLR_DATA_RAM_LATENCY_SHIFT)
#else
	/* Set L2 cache data RAM latency to 3 cycles */
	orr x0, x0, #(CORTEX_A72_L2_DATA_RAM_LATENCY_3_CYCLES << \
			CORTEX_A72_L2CTLR_DATA_RAM_LATENCY_SHIFT)
#endif
	/* Enable L2 ECC and parity with inline data */
	orr x0, x0, #CORTEX_A72_L2CTLR_EL1_ECC_AND_PARITY_ENABLE
	orr x0, x0, #CORTEX_A72_L2CTLR_EL1_DATA_INLINE_ECC_ENABLE
	msr CORTEX_A72_L2CTLR_EL1, x0

	mrs x0, CORTEX_A72_L2ACTLR_EL1
	/* Enable L2 UniqueClean evictions with data */
	orr x0, x0, #CORTEX_A72_L2ACTLR_ENABLE_UNIQUE_CLEAN
	msr CORTEX_A72_L2ACTLR_EL1, x0

#if K3_EXCLUSIVE_SNOOP_DELAY
	mrs	x0, CORTEX_A72_CPUACTLR_EL1
	/* Set Snoop-delayed exclusive handling */
	orr	x0, x0, #CORTEX_A72_CPUACTLR_EL1_DELAY_EXCLUSIVE_SNOOP
	msr	CORTEX_A72_CPUACTLR_EL1, x0
#endif

	isb
	ret
endfunc plat_reset_handler

	/* ---------------------------------------------
	 * int plat_crash_console_init(void)
	 * Function to initialize the crash console
	 * without a C Runtime to print crash report.
	 * Clobber list : x0 - x4
	 * ---------------------------------------------
	 */
	.globl plat_crash_console_init
func plat_crash_console_init
	mov_imm	x0, CRASH_CONSOLE_BASE
	mov_imm	x1, CRASH_CONSOLE_CLK
	mov_imm	x2, CRASH_CONSOLE_BAUD_RATE
	mov w3, #0x0
	b	console_16550_core_init
endfunc plat_crash_console_init

	/* ---------------------------------------------
	 * int plat_crash_console_putc(void)
	 * Function to print a character on the crash
	 * console without a C Runtime.
	 * Clobber list : x1, x2
	 * ---------------------------------------------
	 */
	.globl plat_crash_console_putc
func plat_crash_console_putc
	mov_imm	x1, CRASH_CONSOLE_BASE
	b	console_16550_core_putc
endfunc plat_crash_console_putc

	/* ---------------------------------------------
	 * void plat_crash_console_flush()
	 * Function to force a write of all buffered
	 * data that hasn't been output.
	 * Out : void.
	 * Clobber list : x0, x1
	 * ---------------------------------------------
	 */
	.globl plat_crash_console_flush
func plat_crash_console_flush
	mov_imm	x0, CRASH_CONSOLE_BASE
	b	console_16550_core_flush
endfunc plat_crash_console_flush