summaryrefslogtreecommitdiffstats
path: root/src
Commit message (Collapse)AuthorAgeFilesLines
* get_rproc_info: Introduce new API to query remoteproc1.00.00.08Karthik Ramanan2016-06-201-2/+46
| | | | | | | | | | | | | | | | | | | | This is the initial implementation of an extensible API that allows the user to query various remote core parameters. Currently, there are three query parameters that are supported: 1. CPU Load 2. Total configured heap size 3. Available heap size The intent of this API is to programmatically call the API and feed it in various other tools that can be developed on top of this (for example: soc performance visualization etc.) NOTE: This would require a corresponding change in the libdce as well. Signed-off-by: Karthik Ramanan <a0393906@ti.com>
* dce: package.xdc: Remove requiring CE and FC componentsJacob Stiffler2015-12-021-5/+0
| | | | | | | | | | * These "requires" lines cause the build procedure to rebuild components in CE and FC. * Rebuilding these CE and FC components can break when building in a parallel framework such as yocto. Signed-off-by: Jacob Stiffler <j-stiffler@ti.com> Signed-off-by: Karthik Ramanan <a0393906@ti.com>
* update MemHeader to hold the flagsPradeep Venkatasubbarao2014-03-211-0/+1
| | | | | | | | | | | | | | | The MemHeader structure is updated to hold the memory attribute flags. This change is triggered by the need to hold the coreid in the flags from the libdce perpective. In future flags can be used to hold more attributes. The least significant 4 bits is assumed to hold the coreid. This information is noted needed by the remoteproc. Its only for book keeping and the structure sizes on MPU and remote procs must match. dependent MPU Patch: http://review.omapzoom.org/#/c/34863 Signed-off-by: Pradeep Venkatasubbarao <pradeepv@ti.com>
* Modified Memory Map in Resource table.1.00.00.00Pradeep Venkatasubbarao2013-12-031-55/+100
| | | | | | Now DSP can allocate upto 64MB. Signed-off-by: Pradeep Venkatasubbarao <pradeepv@ti.com>
* [DCE] Add initial code for DSPPradeep Venkatasubbarao2013-11-177-0/+1261
This is the first draft of the DCE code on DSP. It contains a sample Universal Copy codec below the VIDEC2 interface. Signed-off-by: Pradeep Venkatasubbarao <pradeepv@ti.com>