aboutsummaryrefslogtreecommitdiffstats
Commit message (Expand)AuthorAgeFilesLines
* autogen: wingo signed commentLuis de Bethencourt2011-03-221-1/+1
* Bump automake requirement to 1.10 and autoconf to 2.60Tim-Philipp Müller2010-06-281-5/+4
* autogen.sh: Use printf instead of 'echo -n'. Check for automake-1.1[01]Jan Schmidt2009-06-261-2/+2
* autotools: move -Wno-portability for automake to configure.acTim-Philipp Müller2009-05-221-1/+1
* Run libtoolize before aclocalMarc-Andre Lureau2009-05-101-1/+1
* autogen.sh: actually setting up a symbolic link for the pre-commit hookEdward Hervey2009-02-211-2/+2
* Use a symbolic link for the pre-commit client-side hookEdward Hervey2009-01-301-1/+1
* Install and use pre-commit indentation hook from commonEdward Hervey2009-01-211-0/+7
* autogen.sh : Use git submoduleEdward Hervey2009-01-201-8/+5
* Require gettext 0.17 because older versions don't mix with libtool 2.2. At bu...Sebastian Dröge2008-11-291-1/+1
* fix package nameChristian Schaller2008-06-031-1/+1
* autogen.sh: Add -Wno-portability to the automake parameters to stop warnings ...Sebastian Dröge2008-01-101-1/+1
* autogen.sh: Require automake 1.7Thomas Vander Stichele2007-04-291-1/+1
* autogen.sh: libtoolize on Darwin/MacOSX is called glibtoolizeEdward Hervey2006-05-081-1/+1
* autogen.sh: Don't check for file that only exists in CVS but isn't disted (#3...Mikhail Zabaluev2006-03-131-1/+1
* autogen.sh: Allow automake 1.9Michael Smith2006-02-241-1/+1
* Enable documentation.Julien Moutte2005-11-061-1/+1
* releasing 0.9.1Thomas Vander Stichele2005-09-061-8/+8
* Make autogen work again.Jan Schmidt2005-08-301-1/+1
* gst/avi/Makefile.am (libgstavi_la_CFLAGS): No gettext hacks, the defines come...Andy Wingo2005-07-081-6/+6
* updates to make this closer to compileChristian Schaller2005-05-051-1/+1
* make this module a bit more 0.9 friendlyChristian Schaller2005-05-051-6/+6
* whoops, checked in too muchBenjamin Otte2004-05-161-1/+1
* compute offsets correctly for internal buffers so timestamps are set correctl...David Moore2004-05-161-1/+1
* update for plugin changes to export symbolsThomas Vander Stichele2004-02-291-2/+2
* autogen.sh: replace test -e with test -x for mkinstalldirs to be more portable.Benjamin Otte2004-02-221-1/+1
* up gettext versionThomas Vander Stichele2004-02-131-1/+1
* force autopointThomas Vander Stichele2004-02-121-1/+1
* run only onceThomas Vander Stichele2004-02-121-11/+0
* putting i18n in place for pluginsThomas Vander Stichele2004-01-191-0/+24
* fixing bug #126985, gst core requires 1.6 anywayLeif Johnson2003-11-261-1/+1
* get last fix correct.David Schleef2003-08-301-1/+1
* Handle libtoolize with alternate namesDavid Schleef2003-08-171-2/+2
* I'm too lazy to comment thisThomas Vander Stichele2003-05-281-1/+1
* fix Makefiles for C++ libraries. They should now work with Forte. This needs ...Benjamin Otte2003-05-221-1/+1
* Updated autogen.sh/configure.ac and various Makefiles to make the configure s...Brian Cameron2003-05-211-1/+1
* fixes 107967Thomas Vander Stichele2003-05-121-3/+4
* remove bashismsDavid Schleef2003-05-091-2/+2
* Change autoconf_2.52d_check to 2_52 to make bash happyDavid Schleef2003-04-131-1/+1
* oopsThomas Vander Stichele2002-12-301-1/+1
* slurp in ffmpeg a) please test b) please help me figure out how to portably l...Thomas Vander Stichele2002-12-261-0/+3
* run libtoolize, remove generated file ltmain.sh add some newer versions for t...David I. Lehn2002-11-011-7/+3
* list preferred autotoolsThomas Vander Stichele2002-09-301-4/+8
* same changesThomas Vander Stichele2002-05-271-2/+4
* small fixThomas Vander Stichele2002-05-181-0/+4
* same fix for pluginsThomas Vander Stichele2002-04-181-1/+2
* let's not update here, it's not necessary; ie, if you run cvs update in gst-p...Andy Wingo2002-03-021-3/+0
* fix a typoAndy Wingo2002-03-021-1/+1
* more changesThomas Vander Stichele2002-03-021-0/+3
* adapt to use new stuffThomas Vander Stichele2002-03-021-6/+6