aboutsummaryrefslogtreecommitdiffstats
path: root/gst
Commit message (Expand)AuthorAgeFilesLines
* jpegparse: change caps/prio to be picked by decodebin2Harinarayan Bhatta2014-04-082-3/+3
* h264parse: disable passthrough when we might see B framesVincent Penquerc'h2013-05-151-4/+11
* omxcamerabinsrc: use the modes we know are workingVincent Penquerc'h2013-05-151-6/+4
* h264parse: fix AU chunking for interlaced streamsVincent Penquerc'h2013-05-151-4/+7
* h264parse: simulate passthrough mode when it is scheduledVincent Penquerc'h2013-05-151-1/+30
* h264parse: use num-reorder-frames from caps if not found in streamVincent Penquerc'h2013-05-152-0/+7
* h264parse: add num-reorder-frames to the caps, if presentVincent Penquerc'h2013-05-151-0/+4
* h264parse: attach picture order count to buffersVincent Penquerc'h2013-05-152-2/+13
* h264parse: do not send PPS and SPS alone in byte-stream modeVincent Penquerc'h2013-05-152-7/+14
* h264parse: do not use VUI values if they were not found in the streamVincent Penquerc'h2013-05-151-1/+2
* h264parse: add num-ref-frames in capsVincent Penquerc'h2013-05-152-0/+12
* h264parse: delay setting passthrough mode when waiting to known resolutionVincent Penquerc'h2013-05-152-1/+9
* h264parse: do not use a buffer after it was unreffedVincent Penquerc'h2013-05-151-1/+2
* h264parse: split interlaced fields in separate packetsVincent Penquerc'h2013-05-152-1/+11
* Revert "h264parse: disable some optimizations with AVC input"Vincent Penquerc'h2013-05-151-6/+0
* h264parse: wait to get resolution before pushing buffersVincent Penquerc'h2013-05-152-1/+35
* h264parse: disable some optimizations with AVC inputAlessandro Decina2013-05-151-0/+6
* camerabin2: record audio with video by defaultLuciana Fujii Pontello2013-05-151-0/+10
* vc1parse: disable BDU parsing until it's more matureAlessandro Decina2013-05-151-0/+7
* h264parse: flag B framesAlessandro Decina2013-05-152-0/+6
* vc1parse: set duration on output buffersAlessandro Decina2013-05-152-1/+10
* vc1parse: flag bframesAlessandro Decina2013-05-151-0/+10
* vc1parse: workaround for simple/main codec_data being 5 bytes longAlessandro Decina2013-05-151-1/+2
* vc1parse: remove stub stream conversion codeAlessandro Decina2013-05-151-127/+4
* vc1parse: add some more debugging to _renegotiateAlessandro Decina2013-05-151-1/+3
* vc1parse: Add VC1 parser pluginAlessandro Decina2013-05-154-2/+1759
* camerabin2: change profile to h264Luciana Fujii Pontello2013-05-151-5/+3
* mpegvideoparse: Fix rebase of interlaced fieldLuciana Fujii Pontello2013-05-151-4/+3
* camerabin2: Change viewfinderbin to accept yuvLuciana Fujii Pontello2013-05-151-1/+1
* omxcamerabinsrc: Request yuv from omx_camera src padLuciana Fujii Pontello2013-05-151-16/+5
* mpegpsdemux: limit the amount of scanning done on duration queriesAlessandro Decina2013-05-151-13/+27
* h264parse: consider input as packetized only if format=avc is explicitly set ...Alessandro Decina2013-05-151-1/+2
* mpegvideoparse: set interlaced field in capsAlessandro Decina2013-05-151-1/+2
* dvdspu: add interlaced supportRob Clark2013-05-153-75/+116
* dvdspu: cleanup debug codeRob Clark2013-05-151-44/+26
* dvdspu: use refcnting instead of explicit copyRob Clark2013-05-151-2/+2
* dvdspu: some optimizationsRob Clark2013-05-153-17/+30
* dvdspu: add NV12 supportRob Clark2013-05-155-26/+35
* h264parse: avoid pushing SPS/PPS at start only if both are found in streamAlessandro Decina2013-05-152-4/+26
* omxcamerabinsrc: Add property "camera-device"Luciana Fujii Pontello2013-05-152-1/+53
* camerabin2: Add a timer to measure shot-to-save delay.George Kiagiadakis2013-05-152-0/+13
* omxcamerabinsrc: make recordings start at running_time=0Alessandro Decina2013-05-151-0/+8
* camerabin2: fix _unref(NULL) assertionAlessandro Decina2013-05-151-2/+1
* camerabin2: swap image-filter and image-capture-capsAlessandro Decina2013-05-151-2/+2
* omxcamerabinsrc: add allocate-buffers and source-filter propertiesAlessandro Decina2013-05-152-4/+76
* omxcamerabinsrc: get viewfinder and video buffers from omx_camera:srcAlessandro Decina2013-05-152-10/+17
* freeze: Add timeout property.Daniel Díaz2013-05-151-0/+6
* camerabin2: cleanup omxcamerabinsrc a bitAlessandro Decina2013-05-152-306/+54
* omxcamerabinsrc: forward the zoom property to omx_cameraAlessandro Decina2013-05-151-1/+6
* camerabin2: rename GstBaseCameraSrc to GstBaseCameraBinSrcAlessandro Decina2013-05-154-28/+28