1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
|
/*
* Copyright (c) 2011-2018, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/*
* ======== Resource.xdc ========
*/
/*!
* ======== Resource ========
* Resource Module
*/
@Template("./Resource.xdt")
@ModuleStartup
module Resource {
/*!
* @def Resource_loadAddr
* @brief Default load address for the Resource table
*/
metaonly config UInt loadAddr = 0x3000;
/*!
* @def Resource_loadSegment
* @brief If loadSegment is defined, loadAddr is overridden with the base
* address of the loadSegment
*/
metaonly config String loadSegment;
/*!
* @def Resource_loadSymbol
* @brief If loadSymbol is defined, loadAddr is overridden with the
* loadSymbol as external pointer
*/
metaonly config String loadSymbol;
/*!
* @def Resource_traceOnly
* @brief Set traceOnly to true in order to get an image with trace
* resources only, and without VRINGs.
* Implemented only for the Keystone II (TCI6638) platform.
*/
metaonly config Bool traceOnly = false;
/*!
* Flag to indicate the user will provide a custom resource table
*
* If false (the default), a default resource table will be
* created during configuration.
*
* If true, the user must supply their own resource table.
* Fundamentally, this amounts to providing a well-formed
* resource_table structure named 'ti_ipc_remoteproc_ResourceTable'.
*/
metaonly config Bool customTable = false;
/*!
* @def Resource_S_SUCCESS
* @brief Operation is successful.
*/
const Int S_SUCCESS = 0;
/*!
* @def Resource_E_NOTFOUND
* @brief Element was not found in table
*/
const Int E_NOTFOUND = -1;
/*!
* @def Resource_RscTable
*
* @brief An open-ended type-length-value based resource table
*/
struct RscTable {
UInt32 ver;
UInt32 num;
UInt32 reserved[2];
UInt32 offset[1];
};
/*!
* @def Resource_MemEntry
*
* @brief A Resource Table memory type record
*/
struct MemEntry {
UInt32 type;
UInt32 da; /* Device Virtual Address */
UInt32 pa; /* Physical Address */
UInt32 len;
UInt32 flags;
UInt32 reserved;
Char name[32];
};
/*!
* @brief Virtual to Physical address translation function
*
* @sa Resource_physToVirt
*/
@DirectCall
Int virtToPhys(UInt32 da, UInt32 *pa);
/*!
* @brief Physical to Virtual address translation function
*
* @sa Resource_virtToPhys
*/
@DirectCall
Int physToVirt(UInt32 pa, UInt32 *da);
/*!
* @brief Get the Trace Buffer address from resource table.
*
* @return Pointer to trace buffer, or NULL if not found.
*/
@DirectCall
Ptr getTraceBufPtr();
/*!
* @brief Get the Trace Buffer Size from resource table.
*
* @return Size of trace buffer, or NULL if not found.
*/
@DirectCall
SizeT getTraceBufSize();
/*!
* @brief Get the status field of the VDEV, given the fw_rsc_vdev id.
*
* @return status value which is set by Virtio device on HLOS.
*/
@DirectCall
Char getVdevStatus(UInt32 id);
/*!
* @brief Get the nth (vqId) vring address from the VDEV struct.
*
* @return NULL if no VDEV found, or vqId is not found.
*/
@DirectCall
Ptr getVringDA(UInt32 vqId);
internal: /* not for client use */
/*!
* @brief Use resource and resourceLen so table could be properly
* allocated
*
*/
Void init();
/*!
* @brief Return the i-th entry in the resource table if the entry
* is of type CARVEOUT or DEVMEM, or NULL otherwise.
*
*/
MemEntry *getMemEntry(UInt index);
struct Module_State {
RscTable *pTable; /* Resource Resource Table pointer */
};
}
|