diff options
author | Manu Mathew | 2020-06-19 08:47:16 -0500 |
---|---|---|
committer | Manu Mathew | 2020-06-19 09:13:11 -0500 |
commit | 252247115ec2d4eb54dba496cfa94ffce94023ad (patch) | |
tree | 1ba4c6feac20fc2c116693c4f2df3c1281f081cb /scripts/test_dist.py | |
parent | 9d0b3422cc0915028dd92b4d07377b3b8f45534f (diff) | |
download | pytorch-mmdetection-252247115ec2d4eb54dba496cfa94ffce94023ad.tar.gz pytorch-mmdetection-252247115ec2d4eb54dba496cfa94ffce94023ad.tar.xz pytorch-mmdetection-252247115ec2d4eb54dba496cfa94ffce94023ad.zip |
documentation added
Diffstat (limited to 'scripts/test_dist.py')
-rwxr-xr-x | scripts/test_dist.py | 18 |
1 files changed, 9 insertions, 9 deletions
diff --git a/scripts/test_dist.py b/scripts/test_dist.py index cb4879ad..4fc7ddfa 100755 --- a/scripts/test_dist.py +++ b/scripts/test_dist.py | |||
@@ -11,21 +11,21 @@ from torch.distributed import launch as distributed_launch | |||
11 | Usage: | 11 | Usage: |
12 | (1) Use one of the following config files. | 12 | (1) Use one of the following config files. |
13 | (2) Inside the config file, make sure that the dataset that needs to be trained on is uncommented. | 13 | (2) Inside the config file, make sure that the dataset that needs to be trained on is uncommented. |
14 | (3) Use the appropriate input resolution int the config file (input_size). | 14 | (3) Use the appropriate input resolution in the config file (input_size). |
15 | (4) Recommend to run the first training with voc0712 dataset as it is widely used and reasonably small. | 15 | (4) Recommend to run the first training with voc0712 dataset as it is widely used and reasonably small. |
16 | (5) To convert cityscapes to coco format, run the script: tools/convert_datasets/cityscapes.py | 16 | (5) To convert cityscapes to coco format, run the script: tools/convert_datasets/cityscapes.py |
17 | 17 | ||
18 | config='./configs/jacinto_ai/ssd_mobilenet.py' | 18 | config='./configs/ssd/ssd_mobilenet.py' |
19 | config='./configs/jacinto_ai/ssd_mobilenet_fpn.py' | 19 | config='./configs/ssd/ssd_mobilenet_fpn.py' |
20 | config='./configs/jacinto_ai/ssd_resnet_fpn.py' | 20 | config='./configs/ssd/ssd_resnet_fpn.py' |
21 | config='./configs/jacinto_ai/ssd_regnet_fpn_bgr.py' | 21 | config='./configs/ssd/ssd_regnet_fpn_bgr.py' |
22 | 22 | ||
23 | config='./configs/jacinto_ai/retinanet_regnet_fpn_bgr.py' | 23 | config='./configs/retinanet/retinanet_regnet_fpn_bgr.py' |
24 | config='./configs/jacinto_ai/retinanet_resnet_fpn.py' | 24 | config='./configs/retinanet/retinanet_resnet_fpn.py' |
25 | config='./configs/jacinto_ai/fcos_regnet_fpn_bgr.py' | 25 | config='./configs/retinanet/fcos_regnet_fpn_bgr.py' |
26 | ''' | 26 | ''' |
27 | 27 | ||
28 | config='./configs/jacinto_ai/retinanet_resnet_fpn.py' | 28 | config='./configs/retinanet/retinanet_regnet_fpn_bgr.py' |
29 | 29 | ||
30 | ######################################################################## | 30 | ######################################################################## |
31 | # other settings | 31 | # other settings |