1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
|
JAILHOUSE
=========
Introduction
------------
Jailhouse is a partitioning Hypervisor based on Linux. It is able to run
bare-metal applications or (adapted) operating systems besides Linux. For this
purpose, it configures CPU and device virtualization features of the hardware
platform in a way that none of these domains, called "cells" here, can
interfere with each other in an unacceptable way.
Jailhouse is optimized for simplicity rather than feature richness. Unlike
full-featured Linux-based hypervisors like KVM or Xen, Jailhouse does not
support overcommitment of resources like CPUs, RAM or devices. It performs no
scheduling and only virtualizes those resources in software, that are essential
for a platform and cannot be partitioned in hardware.
Once Jailhouse is activated, it runs bare-metal, i.e. it takes full control
over the hardware and needs no external support. However, in contrast to other
bare-metal hypervisors, it is loaded and configured by a normal Linux system.
Its management interface is based on Linux infrastructure. So you boot Linux
first, then you enable Jailhouse and finally you split off parts of the
system's resources and assign them to additional cells.
Community Resources
-------------------
Project home:
- https://github.com/siemens/jailhouse
Source code:
- https://github.com/siemens/jailhouse.git
- git@github.com:siemens/jailhouse.git
Demo and testing images:
- https://github.com/siemens/jailhouse-images
Frequently Asked Questions (FAQ):
- See [FAQ file](FAQ.md)
IRC channel:
- Freenode, irc.freenode.net, #jailhouse
- [![Webchat](https://img.shields.io/badge/irc-freenode-blue.svg "IRC Freenode")](https://webchat.freenode.net/?channels=jailhouse)
Mailing list:
- jailhouse-dev@googlegroups.com
- Subscription:
- jailhouse-dev+subscribe@googlegroups.com
- https://groups.google.com/forum/#!forum/jailhouse-dev/join
- Archives
- https://groups.google.com/forum/#!forum/jailhouse-dev
- https://www.mail-archive.com/jailhouse-dev@googlegroups.com
Continuous integration:
- https://github.com/siemens/jailhouse/actions
- Status:
- ![](https://github.com/siemens/jailhouse/actions/workflows/main.yaml/badge.svg?branch=master) on master
- ![](https://github.com/siemens/jailhouse/actions/workflows/main.yaml/badge.svg?branch=next) on next
Static code analysis:
- https://scan.coverity.com/projects/siemens-jailhouse
- Status:
- ![](https://scan.coverity.com/projects/siemens-jailhouse/badge.svg) on coverity_scan
See the [contribution documentation](CONTRIBUTING.md) for details
on how to write Jailhouse patches and propose them for upstream integration.
Hardware requirements (preliminary)
-----------------------------------
#### x86 architecture:
- Intel system:
- support for 64-bit and VMX, more precisely
- EPT (extended page tables)
- unrestricted guest mode
- preemption timer
- Intel IOMMU (VT-d) with interrupt remapping support
(except when running inside QEMU)
- or AMD system:
- support for 64-bit and SVM (AMD-V), and also
- NPT (nested page tables); required
- Decode Assists; recommended
- AMD IOMMU (AMD-Vi) is unsupported now but will be required in future
- At least 2 logical CPUs
#### ARM architecture:
- ARMv7 with virtualization extensions or ARMv8
- At least 2 logical CPUs
- Supported ARM boards:
- Banana Pi ([see more](Documentation/setup-on-banana-pi-arm-board.md))
- Orange Pi Zero (256 MB version)
- NVIDIA Jetson TK1
- ARM Versatile Express with Cortex-A15 or A7 cores
(includes ARM Fast Model)
- emtrion emCON-RZ/G1x series based on Renesas RZ/G ([see more](Documentation/setup-on-emtrion-emcon-rz-boards.md))
- Supported ARM64 boards:
- AMD Seattle / SoftIron Overdrive 3000
- LeMaker HiKey
- NVIDIA Jetson TX1 and TX2
- Xilinx ZCU102 (ZynqMP evaluation board)
- NXP MCIMX8M-EVK
Software requirements
---------------------
#### x86 architecture:
- x86-64 Linux kernel (tested against 3.14+)
- VT-d IOMMU usage (DMAR) has to be disabled in the Linux kernel, e.g. via
the command line parameter:
intel_iommu=off
- To exploit the faster x2APIC, interrupt remapping needs to be on in the
kernel (check for CONFIG_IRQ_REMAP)
- The hypervisor requires a contiguous piece of RAM for itself and each
additional cell. This currently has to be pre-allocated during boot-up.
On x86 this is typically done by adding
memmap=82M$0x3a000000
as parameter to the command line of the virtual machine's kernel. Note that
if you plan to put this parameter in GRUB2 variables in /etc/default/grub,
then you will need three escape characters before the dollar
(e.g. ```GRUB_CMDLINE_LINUX_DEFAULT="memmap=82M\\\$0x3a000000"```).
#### ARM architecture:
- Linux kernel:
- 3.19+ for ARM
- 4.7+ for ARM64
- Appropriate boot loader support (typically U-Boot)
- Linux is started in HYP mode
- PSCI support for CPU offlining
- The hypervisor requires a contiguous piece of RAM for itself and each
additional cell. This currently has to be pre-allocated during boot-up.
On ARM this can be obtained by reducing the amount of memory seen by the
kernel (through the `mem=` kernel boot parameter) or by modifying the
Device Tree (i.e. the `reserved-memory` node).
Build & Installation
--------------------
Simply run `make`, optionally specifying the target kernel directory:
make [KDIR=/path/to/kernel/objects]
#### Installation
It is recommended to install all of Jailhouse on your target machine. That will
take care of a kernel module, the firmware, tools etc. Just call
make install
from the top-level directory.
The traditional Linux cross-compilation (i.e. `ARCH=` and `CROSS_COMPILE=`) and
installation (i.e. `DESTDIR=`) flags are supported as well.
#### Running without Installation
Except for the hypervisor image `jailhouse*.bin`, that has to be available in
the firmware search path, you can run Jailhouse from the build directory.
If you cannot or do not want to use `make install`, you can either install just
the firmware using `make firmware_install` or customize the firmware search
path:
echo -n /path/to/jailhouse/hypervisor/ \
> /sys/module/firmware_class/parameters/path
Configuration
-------------
Jailhouse requires one configuration file for the complete system and one for
each additional cell besides the primary Linux. These .cell files have to be
passed to the jailhouse command line tool for enabling the hypervisor or
creating new cells.
On x86, the required hardware capabilities can be validated by running
jailhouse hardware check
A system configuration can be created on an x86 target system by running the
following command:
jailhouse config create sysconfig.c
In order to translate this into the required binary form, place this file in
the configs/x86/ directory. The build system will pick up every .c file from
there and generate a corresponding .cell file.
Currently, there is no config generator for the ARM architecture; therefore the
config file must be manually written by starting from the reference examples
and checking hardware-specific datasheets, DTS and /proc entries.
Depending on the target system, the C structures may require some adjustments to
make Jailhouse work properly or to reduce the desired access rights of the Linux
root cell.
Configurations for additional (non-root) cells currently require manual
creation. To study the structures, use one of the demo cell configurations files
as reference, e.g. configs/x86/apic-demo.c or configs/x86/e1000-demo.c.
x86 Demonstration in QEMU/KVM
-----------------------------
**NOTE**: You can also build and execute the following demo steps with the
help of the jailhouse-images side project at
https://github.com/siemens/jailhouse-images.
The included system configuration qemu-x86.c can be used to run Jailhouse in
QEMU/KVM virtual machine on x86 hosts (Intel and AMD are supported). Currently
it requires Linux 4.4 or newer on the host side. QEMU version 2.8 or newer is
required.
You also need a Linux guest image with a recent kernel (tested with >= 3.9) and
the ability to build a module for this kernel. Further steps depend on the type
of CPU you have on your system.
For Intel CPUs: Make sure the kvm-intel module was loaded with nested=1 to
enable nested VMX support. Start the virtual machine as follows:
qemu-system-x86_64 -machine q35,kernel_irqchip=split -m 1G -enable-kvm \
-smp 4 -device intel-iommu,intremap=on,x-buggy-eim=on \
-cpu host,-kvm-pv-eoi,-kvm-pv-ipi,-kvm-asyncpf,-kvm-steal-time,-kvmclock \
-drive file=LinuxInstallation.img,format=raw|qcow2|...,id=disk,if=none \
-device ide-hd,drive=disk -serial stdio -serial vc \
-netdev user,id=net -device e1000e,addr=2.0,netdev=net \
-device intel-hda,addr=1b.0 -device hda-duplex -device pcie-pci-bridge
For AMD CPUs: Make sure the kvm-amd module was loaded with nested=1 to enable
nested SVM support. Start the virtual machine as follows:
qemu-system-x86_64 -machine q35 -m 1G -enable-kvm -smp 4 \
-cpu host,-kvm-pv-eoi,-kvm-pv-ipi,-kvm-asyncpf,-kvm-steal-time,-kvmclock \
-drive file=LinuxInstallation.img,format=raw|qcow2|...,id=disk,if=none \
-device ide-hd,drive=disk -serial stdio -serial vc \
-netdev user,id=net -device e1000e,addr=2.0,netdev=net \
-device intel-hda,addr=1b.0 -device hda-duplex -device pcie-pci-bridge
Inside the VM, make sure that `jailhouse-*.bin`, generated by the build process,
are available for firmware loading (typically /lib/firmware), see above for
installation steps.
The Jailhouse QEMU cell config will block use of the serial port by the guest
OS, so make sure that the guest kernel command line does NOT have its console
set to log to the serial port (ie remove any 'console=ttyS0' arguments from the
grub config). Reboot the guest and load jailhouse.ko. Then enable Jailhouse
like this:
jailhouse enable /path/to/qemu-x86.cell
Next you can create a cell with a demonstration application as follows:
jailhouse cell create /path/to/apic-demo.cell
jailhouse cell load apic-demo /path/to/apic-demo.bin
jailhouse cell start apic-demo
apic-demo.bin is left by the built process in the inmates/demos/x86 directory.
This application will program the APIC timer interrupt to fire at 10 Hz,
measuring the jitter against the PM timer and displaying the result on the
console. Given that this demonstration runs in a virtual machine, obviously
no decent latencies should be expected.
After creation, cells are addressed via the command line tool by providing
their names or their runtime-assigned IDs. You can obtain information about
active cells this way:
jailhouse cell list
Cell destruction is performed by specifying the configuration file of the
desired cell. This command will destroy the apic-demo:
jailhouse cell destroy apic-demo
Note that the first destruction or shutdown request on the apic-demo cell will
fail. The reason is that this cell contains logic to demonstrate an ordered
shutdown as well as the ability of a cell to reject shutdown requests.
The apic-demo cell has another special property for demonstration purposes: As
long as it is running, no cell reconfigurations can be performed - the
apic-demo locks the hypervisor in this regard. In order to destroy another cell
or create an additional one, shut down the apic-demo first.
jailhouse cell shutdown apic-demo # call again if error is returned
To demonstrate the execution of a second, non-Linux cell, issue the following
commands:
jailhouse cell create /path/to/pci-demo.cell
jailhouse cell load pci-demo /path/to/pci-demo.bin \
-s "con-base=0x2f8" -a 0x1000
jailhouse cell start pci-demo
The pci-demo will use the second serial port provided by QEMU. You will find
its output in a virtual console of the QEMU window. The purpose of this demo is
to show basic PCI device configuration and MSI handling.
While cell configurations are locked, it is still possible, though, to reload
the content of existing cell (provided they accept their shutdown first). To
reload and restart the tiny-demo, issue the following commands:
jailhouse cell start apic-demo
jailhouse cell load pci-demo /path/to/pci-demo.bin \
-s "con-base=0x2f8" -a 0x1000
jailhouse cell start pci-demo
Finally, Jailhouse is can be stopped completely again:
jailhouse disable # call again on error due to running apic-demo
All non-Linux cells running at that point will be destroyed, and resources
will be returned to Linux.
ARM64 Demonstration in QEMU
---------------------------
Similarly like x86, Jailhouse can be tried out in a completely emulated ARM64
(aarch64) environment under QEMU. QEMU version 3.0 or later is required.
Start the QEMU machine like this:
qemu-system-aarch64 -cpu cortex-a57 -smp 16 -m 1G \
-machine virt,gic-version=3,virtualization=on,its=off -nographic \
-netdev user,id=net -device virtio-net-device,netdev=net \
-drive file=LinuxInstallation.img,format=raw|qcow2|...,id=disk,if=none \
-device virtio-blk-device,drive=disk \
-kernel /path/to/kernel-image -append "root=/dev/vda1 mem=768M"
Jailhouse can be started after loading its kernel module. Run:
jailhouse enable /path/to/qemu-arm64.cell
The corresponding test to apic-demo on x86 is the gic-demo:
jailhouse cell create /path/to/qemu-arm64-inmate-demo.cell
jailhouse cell load inmate-demo /path/to/gic-demo.bin
jailhouse cell start inmate-demo
|