| Commit message (Collapse) | Author | Age | Files | Lines |
|
|
|
|
|
|
|
|
| |
Do not duplicate this in SoC specific Makefiles, it is more clear which
types of images work with which SoCs if it is one location. AM65x and
J721e cannot do combined, AM62x cannot do split, others can do both.
Signed-off-by: Andrew Davis <afd@ti.com>
Signed-off-by: Vignesh Raghavendra <vigneshr@ti.com>
|
|
|
|
|
|
|
|
|
| |
When building a combined image, do not generate a standalone sysfw.itb.
Vice-versa for split image and tiboot3.bin. There is no need to
generate the other image and for HS it will be non-functional.
Signed-off-by: Andrew Davis <afd@ti.com>
Signed-off-by: Vignesh Raghavendra <vigneshr@ti.com>
|
|
|
|
|
|
|
|
|
|
|
| |
Fix below build warnings due to change in defintion of
boardcfg_sa2ul_cfg struct
./soc/j721s2/evm/sec-cfg.c:92:18: warning: excess elements in array initializer
92 | .rsvd = {0, 0, 0, 0},
| ^
Signed-off-by: Vignesh Raghavendra <vigneshr@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
R5 SPL on AM65x still uses MCU R5_1 as host ID for requesting DMA
resources. Therefore mark resources b/w MCU R5_0 as shared with MCU
R5_1.
In order to keep number of entries under 260, drop Ring_monitors
allocation fro A53_3
Without this OSPI boot cannot use DMA in R5 SPL stage
Signed-off-by: Vignesh Raghavendra <vigneshr@ti.com>
|
|
|
|
|
|
|
|
|
| |
Update rm-cfg to ensure DMA resources are shared consistently across
RTOS and Linux SDKs. This mainly reduces DMA channels, Rings and GPIO
interrupts available for A53 host, but should be sufficient to meet
Linux requirements.
Signed-off-by: Vignesh Raghavendra <vigneshr@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
| |
The System Firmware functionality on K3 J721E and J7200 SoCs has been
reduced to only cater to the foundational security pieces starting from
SYSFW 2020.08, and the binaries have been renamed accordingly.
Introduce a Makefile variable SCIFS to account for these changes.
Signed-off-by: Suman Anna <s-anna@ti.com>
Acked-by: Praneeth Bajjuri <praneeth@ti.com>
Signed-off-by: Dan Murphy <dmurphy@ti.com>
|
|
|
|
|
|
|
|
|
|
|
| |
Update the common.h headers to add new defines from
SYSFW 2020.08.
Starting from SYSFW v2020.08, a secure_handover_config section
is mandatory in the security config. Otherwise the boot fails
on all SoCs.
Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
|
|
|
|
|
|
|
|
|
| |
Each SOC has its own Makefile and some SOCs may have a need for a
different load address, so define the LOADADDR variable in the SOC
specific Makefile.
Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
Reviewed-by: Suman Anna <s-anna@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Update the common.h headers to add new defines from
SYSFW 2020.07-rc1.
Starting from SYSFW v2020.07-rc1, a secure_debug_config section
is mandatory in the security config. Otherwise the boot fails
on all SoCs.
Fix this by adding a section for secure_debug_config with
appropriate parameters configured on all on AM65x, AM65x SR2.0,
J721E and J7200 SoCs.
Signed-off-by: Suman Anna <s-anna@ti.com>
|
|
|
|
|
|
|
|
|
|
|
| |
Now that SoCs have different boot image targets, introduce SOC specific
Makefiles to represent boot targets. Below are boot targets:
- AM65x: sysfw.itb
- AM65x SR2: sysfw.itb
- J721E: sysfw.itb
- J7200: tiboot3.bin, sysfw.itb
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
|
|
|
|
|
|
|
|
|
|
| |
The number of Main NavSS rings reserved by DMSC for High capacity Rx
channels is off by one. Update the board configuration validation
script and fix the RM cfg resource entries for the same on both AM65x
and AM65x SR2.0 SoCs.
Signed-off-by: Suman Anna <s-anna@ti.com>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Each of the MCU R5F cores are represented by different HOST_IDs, and
the ABI 3.0 RM changes have reassigned all the MAIN2MCU interrupt router
outputs back to only the MCU R5F Core0. This breaks the IPC use-cases
when the MCU R5FSS cluster is configured for Split-mode.
Partition both the MAIN2MCU_LVL and MAIN2MCU_PLS Interrupt Router
outputs equally between the non-secure contexts of both the MCU
R5F cores.
Signed-off-by: Suman Anna <s-anna@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
The Main NavSS IR on AM65x SoCs has a total of 152 output interrupt
lines, out of which the first 16 are reserved for System Firmware.
The ABI 3.0 resource updates have assigned all the remaining IR
output lines to the A53 host context HOST_ID_A53_2, which is wrong.
The Main NavSS IR also supports some interrupt lines for the MCU
R5F cores (connected through MAIN2MCU LVL IR) and for each of the
3 ICSSG subsystems.
Fix up the Main NavSS IR outputs properly by adding resources for
each of the processor subsystems. The output lines [120:127] are
split equally for each of the MCU R5F cores (to support Split-mode),
leaving only 104 usable interrupts for the A53 core. The output
lines [128:151] are associated with the ICSSG subsystems.
Signed-off-by: Suman Anna <s-anna@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
| |
Update the common.h headers to add new defines from SYSFW 2020.04.
Starting from SYSFW v2020.04, an sa2ul_config section is mandatory in
the security config. Otherwise the boot fails.
Fix this by adding a section for sa2ul_config with all parameters
configured to 0.
Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Update the common.h headers to add new defines from SYSFW 2020.03.
Starting from SYSFW v2020.03, a dkek_config section is mandatory in
the security config. Otherwise the boot fails.
Fix this by adding a section for dkek_config with HOST_ID_ALL in
allowed_hosts and allow_dkek_export_tisci set.
Signed-off-by: Dave Gerlach <d-gerlach@ti.com>
Tested-by: Suman Anna <s-anna@ti.com>
|
|
|
|
|
|
|
| |
Update the AM65x RM board configuration to use ABI 3.0 resource type
definitions.
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
| |
Update the common.h headers to add new defines from SYSFW 2019.12.
Starting from SYSFW v2019.12, an otp_config section is mandatory in
the security config. Otherwise the boot fails.
Fix this by adding a section for opt_config with no other host
having permission to OTP array.
Signed-off-by: Nikhil Devshatwar <nikhil.nd@ti.com>
|
|
|
|
|
|
|
|
|
| |
HOST_ID_R5_1 is to be used only with secure context.
HOST_ID_R5_2 is the right Host Id to use for R5F core 1
Fixes: 54933d505c4d ("rm-cfg: Partition interrupt resources between R5F contexts")
Signed-off-by: Sam Nelson <sam.nelson@ti.com>
Acked-by: Suman Anna <s-anna@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Sysfw provides a provision for enabling sysfw traces while booting.
This has to be enabled in board-cfg. In order to ease debug, enable
the sysfw trace support with the help of a build option. Use the
option to enable it:
$ make ENABLE_TRACE=1
Reported-by: Sekhar Nori <nsekhar@ti.com>
Signed-off-by: Lokesh Vutla <lokeshvutla@ti.com>
Signed-off-by: Andreas Dannenberg <dannenberg@ti.com>
|
|
|
|
|
|
|
|
|
|
| |
ROM boots up MCU R5 in secure context and R5 SPL continues to run in the
same context. In order for R5 SPL to use DMA (e.g: with OSPI) add MCU
NAVSS resources with MCU R5 secure host ID that is used by R5 SPL.
Resources allocated are same as those allocated for A53.
Signed-off-by: Vignesh Raghavendra <vigneshr@ti.com>
|
|
Allow for multiple SoCs to be built and object file names per SoC.
Signed-off-by: Nishanth Menon <nm@ti.com>
Signed-off-by: Andreas Dannenberg <dannenberg@ti.com>
Reviewed-by: Suman Anna <s-anna@ti.com>
|