summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorHao Zhang2011-04-21 16:47:53 -0500
committerHao Zhang2011-04-21 16:47:53 -0500
commitac56ca1b9cedc3918227cddaac5acb886b81902e (patch)
tree89340730e6d865f017c6ee7ce4f0d0800a521765
parent076ca095c68f326e39ed57b661a1e3ea948e4dc9 (diff)
downloadmcsdk-tools-ac56ca1b9cedc3918227cddaac5acb886b81902e.tar.gz
mcsdk-tools-ac56ca1b9cedc3918227cddaac5acb886b81902e.tar.xz
mcsdk-tools-ac56ca1b9cedc3918227cddaac5acb886b81902e.zip
MCSDK 2.0.0.7 Eng2 ReleaseDEV.BIOS.MCSDK.02.00.00.07.Eng2
-rw-r--r--boot_loader/IBL_README.txt6
-rw-r--r--boot_loader/examples/i2c/emac/docs/README.txt4
2 files changed, 6 insertions, 4 deletions
diff --git a/boot_loader/IBL_README.txt b/boot_loader/IBL_README.txt
index 433ceb1..9d9aa25 100644
--- a/boot_loader/IBL_README.txt
+++ b/boot_loader/IBL_README.txt
@@ -36,8 +36,10 @@ Steps to program IBL:
36 window and select "Load GEL" 36 window and select "Load GEL"
37 37
38 e. Run the GEL script EVMC66xx IBL->setConfig_c66xx_main, this will by default set the boot parameters for NOR boot over 38 e. Run the GEL script EVMC66xx IBL->setConfig_c66xx_main, this will by default set the boot parameters for NOR boot over
39 I2C. If the user wants to configure NAND boot or EMAC boot over I2C, he/she should run EVMC66xx IBL->setConfig_c66xx_main 39 I2C. Wait for 10 seconds to ensure that the script configuration is completed.
40
41 f. If the user wants to configure NAND boot or EMAC boot over I2C, he/she should run EVMC66xx IBL->setConfig_c66xx_main
40 followed by EVMC66xx IBL->setConfig_c66xx_nand or EVMC66xx IBL->setConfig_c66xx_emac. 42 followed by EVMC66xx IBL->setConfig_c66xx_nand or EVMC66xx IBL->setConfig_c66xx_emac.
41 43
42 f. Press "Enter" in the CCS console window, and the program will write the boot configuration table to the EEPROM 44 g. Press "Enter" in the CCS console window, and the program will write the boot configuration table to the EEPROM
43 45
diff --git a/boot_loader/examples/i2c/emac/docs/README.txt b/boot_loader/examples/i2c/emac/docs/README.txt
index f5fe3d9..5043281 100644
--- a/boot_loader/examples/i2c/emac/docs/README.txt
+++ b/boot_loader/examples/i2c/emac/docs/README.txt
@@ -41,8 +41,8 @@ Steps to program i2cemacboot to EMAC:
415. Start a TFTP server (you can download a free, open source application from http://tftpd32.jounin.net) and copy 415. Start a TFTP server (you can download a free, open source application from http://tftpd32.jounin.net) and copy
42 app.dat to the TFTP base directory. 42 app.dat to the TFTP base directory.
43 43
446. Set the IP address of the PC that is running the TFTP server to 192.168.1.101, since by default IBL will set the EVM IP 446. Set the IP address of the PC that is running the TFTP server to 192.168.2.101, since by default IBL will set the EVM IP
45 address to 192.168.1.100 and the TFTP server IP address to 192.168.1.101. 45 address to 192.168.2.100 and the TFTP server IP address to 192.168.2.101.
46 46
477. Be sure the EVM and the PC are connected in the same subnet of a local network, after POR, the EVM will download the 477. Be sure the EVM and the PC are connected in the same subnet of a local network, after POR, the EVM will download the
48 boot image from TFTP server and boot from it. 48 boot image from TFTP server and boot from it.