summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorCasey Smith2013-03-26 09:28:16 -0500
committerCasey Smith2013-03-26 09:28:16 -0500
commit29504368f409d2d8c78a3f9352868925f4839838 (patch)
treefbcae318735f1dae1eb11d1628f5a997d40bdaa5 /program_evm/gel
parentec241985a4f8e4ae4b518acaa9316b31fce6671e (diff)
downloadmcsdk-tools-29504368f409d2d8c78a3f9352868925f4839838.tar.gz
mcsdk-tools-29504368f409d2d8c78a3f9352868925f4839838.tar.xz
mcsdk-tools-29504368f409d2d8c78a3f9352868925f4839838.zip
Diffstat (limited to 'program_evm/gel')
-rw-r--r--program_evm/gel/README.txt10
1 files changed, 5 insertions, 5 deletions
diff --git a/program_evm/gel/README.txt b/program_evm/gel/README.txt
index 43ecad4..decdcb0 100644
--- a/program_evm/gel/README.txt
+++ b/program_evm/gel/README.txt
@@ -1,15 +1,15 @@
1Steps to update GELs for C66x EVMs 1Steps to update GELs for C66x EVMs
2---------------------------------- 2----------------------------------
3 3
41: There are two GEL files provided in this directory evmc6670l.gel and evmc6678l.gel 41: There are one or more GEL files provided in this directory
5 5
62: These GEL files needs to be copied to CCS installation 62: These GEL files needs to be copied to CCS installation
7 7
83: The following steps will assume the CCS is installed in <CCS_INSTALL_DIR> (which is typically C:\Program Files\Texas Instruments\ccsv5 for Windows XP and ~/ti/ccsv5) 83: The following steps will assume the CCS is installed in <CCS_INSTALL_DIR> (which is typically C:\Program Files\Texas Instruments\ccsv5 for Windows XP and ~/ti/ccsv5 for Linux)
9 9
104: Close the CCS if open 104: Close CCS if open
11 11
125: Replace the GEL file present in the <CCS_INSTALL_DIR>/ccs_base/emulation/boards/evmc6670l/gel directory with the evmc6670l.gel file present in this directory 125: Replace the GEL file present in the <CCS_INSTALL_DIR>/ccs_base/emulation/boards/<BOARD_NAME>/gel directory with the <BOARD_NAME>.gel file present in this directory
13 13
146: Replace the GEL file present in the <CCS_INSTALL_DIR>/ccs_base/emulation/boards/evmc6678l/gel directory with the evmc6678l.gel file present in this directory 146: Repeat step 5 for all gel files present in this directory
15 15