summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
-rw-r--r--boot_loader/IBL_README.txt6
-rw-r--r--boot_loader/examples/i2c/emac/docs/README.txt4
2 files changed, 6 insertions, 4 deletions
diff --git a/boot_loader/IBL_README.txt b/boot_loader/IBL_README.txt
index 433ceb1..9d9aa25 100644
--- a/boot_loader/IBL_README.txt
+++ b/boot_loader/IBL_README.txt
@@ -36,8 +36,10 @@ Steps to program IBL:
36 window and select "Load GEL" 36 window and select "Load GEL"
37 37
38 e. Run the GEL script EVMC66xx IBL->setConfig_c66xx_main, this will by default set the boot parameters for NOR boot over 38 e. Run the GEL script EVMC66xx IBL->setConfig_c66xx_main, this will by default set the boot parameters for NOR boot over
39 I2C. If the user wants to configure NAND boot or EMAC boot over I2C, he/she should run EVMC66xx IBL->setConfig_c66xx_main 39 I2C. Wait for 10 seconds to ensure that the script configuration is completed.
40
41 f. If the user wants to configure NAND boot or EMAC boot over I2C, he/she should run EVMC66xx IBL->setConfig_c66xx_main
40 followed by EVMC66xx IBL->setConfig_c66xx_nand or EVMC66xx IBL->setConfig_c66xx_emac. 42 followed by EVMC66xx IBL->setConfig_c66xx_nand or EVMC66xx IBL->setConfig_c66xx_emac.
41 43
42 f. Press "Enter" in the CCS console window, and the program will write the boot configuration table to the EEPROM 44 g. Press "Enter" in the CCS console window, and the program will write the boot configuration table to the EEPROM
43 45
diff --git a/boot_loader/examples/i2c/emac/docs/README.txt b/boot_loader/examples/i2c/emac/docs/README.txt
index f5fe3d9..5043281 100644
--- a/boot_loader/examples/i2c/emac/docs/README.txt
+++ b/boot_loader/examples/i2c/emac/docs/README.txt
@@ -41,8 +41,8 @@ Steps to program i2cemacboot to EMAC:
415. Start a TFTP server (you can download a free, open source application from http://tftpd32.jounin.net) and copy 415. Start a TFTP server (you can download a free, open source application from http://tftpd32.jounin.net) and copy
42 app.dat to the TFTP base directory. 42 app.dat to the TFTP base directory.
43 43
446. Set the IP address of the PC that is running the TFTP server to 192.168.1.101, since by default IBL will set the EVM IP 446. Set the IP address of the PC that is running the TFTP server to 192.168.2.101, since by default IBL will set the EVM IP
45 address to 192.168.1.100 and the TFTP server IP address to 192.168.1.101. 45 address to 192.168.2.100 and the TFTP server IP address to 192.168.2.101.
46 46
477. Be sure the EVM and the PC are connected in the same subnet of a local network, after POR, the EVM will download the 477. Be sure the EVM and the PC are connected in the same subnet of a local network, after POR, the EVM will download the
48 boot image from TFTP server and boot from it. 48 boot image from TFTP server and boot from it.