diff options
-rw-r--r-- | boot_loader/examples/i2c/emac/docs/README.txt | 14 |
1 files changed, 5 insertions, 9 deletions
diff --git a/boot_loader/examples/i2c/emac/docs/README.txt b/boot_loader/examples/i2c/emac/docs/README.txt index 46f520e..380de22 100644 --- a/boot_loader/examples/i2c/emac/docs/README.txt +++ b/boot_loader/examples/i2c/emac/docs/README.txt | |||
@@ -33,17 +33,13 @@ Steps to program i2cemacboot to EMAC: | |||
33 | 2. Be sure EMAC boot parameter table is progrommed to I2C EEPROM bus address 81 (0x51), if the table is not programmed, | 33 | 2. Be sure EMAC boot parameter table is progrommed to I2C EEPROM bus address 81 (0x51), if the table is not programmed, |
34 | refer to tools\boot_loader\ibl\doc\README.txt on how to program the boot parameter table to EEPROM. | 34 | refer to tools\boot_loader\ibl\doc\README.txt on how to program the boot parameter table to EEPROM. |
35 | 35 | ||
36 | 3. Copy tools\boot_loader\examples\i2c\emac\evmc6xxxl\bin\i2cemacboot_evm6xxxl.out to tools\bin2ccs and rename | 36 | 3. Start a TFTP server (you can download a free, opensource application from http://tftpd32.jounin.net) and copy |
37 | the file to app.out. | 37 | tools\boot_loader\examples\i2c\emac\evmc6xxxl\bin\i2cemacboot_evm6xxxl.out to the TFTP base directory. Rename |
38 | i2cemacboot_evm6xxxl.out to app.out | ||
38 | 39 | ||
39 | 4. Double click bin2ccs.bat, which will convert app.out to a CCS format data file app.dat. | 40 | 4. Set the IP address of the PC that is running the TFTP server to 192.168.1.101, since by default IBL will set the EVM IP |
40 | |||
41 | 5. Start a TFTP server (you can download a free, opensource application from http://tftpd32.jounin.net) and copy | ||
42 | app.dat to the TFTP base directory. | ||
43 | |||
44 | 6. Set the IP address of the PC that is running the TFTP server to 192.168.1.101, since by default IBL will set the EVM IP | ||
45 | address to 192.168.1.100 and the TFTP server IP address to 192.168.1.101. | 41 | address to 192.168.1.100 and the TFTP server IP address to 192.168.1.101. |
46 | 42 | ||
47 | 7. Be sure the EVM and the PC are connected in the same subnet of a local network, after POR, the EVM will download the | 43 | 5. Be sure the EVM and the PC are connected in the same subnet of a local network, after POR, the EVM will download the |
48 | boot image from TFTP server and boot from it. | 44 | boot image from TFTP server and boot from it. |
49 | 45 | ||