1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
618
619
620
621
622
623
624
625
626
627
628
629
630
631
632
633
634
635
636
637
638
639
640
641
642
643
644
645
646
647
648
649
650
651
652
653
654
655
656
657
658
659
660
661
662
663
664
665
666
667
668
|
/************************************************************************************
* FILE PURPOSE: Convert a hex6x boot table file into the format required
* by the c6x chip boot loader.
************************************************************************************
* FILE NAME: bconvert.c
*
* DESCRIPTION: Converts a boot table. The boot table format is:
*
* /--------------------------------------------------------\
* | 32 bit entry point address |
* +--------------------------------------------------------+
* | 32 bit section byte count | \
* +--------------------------------------------------------+ \
* | 32 bit section byte start address | \
* +-------------+-------------+-------------+--------------+ repeat each section
* | Data byte | Data byte | Data byte | Data byte | /
* +-------------+-------------+-------------+--------------+ /
* | Data byte | Data byte | Data byte | Data byte | /
* +-------------+-------------+-------------+--------------+
* | 32 bit zero byte count (end of boot table) |
* \--------------------------------------------------------/
*
*
* The C6x boot loader expects all 32 bit values to be in big endian
* (most significant byte arrives first). Data bytes are also arranged to be 32 bit
* big endian represented.
*
* This program handles conversion of data values that are in sections that are
* not multiples of 4 bytes. For example, a program compiled in big endian format
* with a 1 byte section will have the following table entry (address 0x22222222), value
* 0x33
*
* 00 00 00 01 22 22 22 22 33 00 00 00
*
* The same file compiled with little endian mode will have the entry
*
* 00 00 00 01 22 22 22 22 00 00 00 33
*
*
* Since the boot loader has no idea what endianness the code was compiled for, this
* program performs an endian conversion on any section that does not have a length
* that is a multiple of 4 bytes, if the little endian option is specified. Nothing
* is changed for the big endian mode.
*
* Invokation:
*
* bconvert -be|-le [input_file] [output_file]
*
***************************************************************************************/
#include "stdio.h"
#include "malloc.h"
#include "string.h"
/* Global variable storing the invokation name */
char *invok;
/* Error values */
enum {
ERR_PARSE_TOO_MANY_ARGS = 1000,
ERR_PARSE_NO_ENDIAN,
ERR_PARSE_INPUT_OPEN_FAIL,
ERR_PARSE_OUTPUT_OPEN_FAIL,
ERR_READ_BFILE_INITIAL_MALLOC_FAIL,
ERR_READ_BFILE_REALLOC_FAIL,
ERR_VALUE32_SIZE_ERR,
ERR_VALUE16_SIZE_ERR,
ERR_DATA32_SIZE_ERR,
ERR_REG32_PARSE_ERROR,
ERR_DATA32_REMAIN_ERR
};
enum {
LITTLE,
BIG
};
/************************************************************************************
* FUNTION PURPOSE: Send an error string
************************************************************************************
* DESCRIPTION: Prints an error to stderr
************************************************************************************/
void showErr (int errflag)
{
char *s;
switch (errflag) {
case ERR_PARSE_TOO_MANY_ARGS:
s = "Parse error: too many args specified";
break;
case ERR_PARSE_NO_ENDIAN:
s = "Parse error: no endian mode specified";
break;
case ERR_PARSE_INPUT_OPEN_FAIL:
s = "File error: failed to open specified input file";
break;
case ERR_PARSE_OUTPUT_OPEN_FAIL:
s = "File error: Failed to open specified output file";
break;
case ERR_READ_BFILE_INITIAL_MALLOC_FAIL:
s = "Memory error: Initial malloc call failed";
break;
case ERR_READ_BFILE_REALLOC_FAIL:
s = "Memory error: Subsequent realloc call failed";
break;
case ERR_VALUE32_SIZE_ERR:
s = "Data format error: End of data on 32 bit value read";
break;
case ERR_VALUE16_SIZE_ERR:
s = "Data format error: End of data on 16 bit value read";
break;
case ERR_REG32_PARSE_ERROR:
s = "Parse error: error parsing after reg32 arg";
break;
case ERR_DATA32_REMAIN_ERR:
s = "Parse error: A remainder size greater then four was found";
break;
default:
s = "Unspecified error";
break;
}
fprintf (stderr, "%s: %s\n", invok, s);
} /* showErr */
/*************************************************************************************
* FUNCTION PURPOSE: Check if a string is prefixed with "0x".
*************************************************************************************
* DESCRIPTION: Returns non-zero if the string begins with "0x"
*************************************************************************************/
int isChex (char *s)
{
if ((s[0] == '0') && (s[1] == 'x'))
return (1);
return (0);
} /* isChex */
/*************************************************************************************
* FUNCTION PURPOSE: Parse the input parameters
*************************************************************************************
* DESCRIPTION: Checks for required args, opens source and destination streams.
*************************************************************************************/
int parseit (int argc, char *argv[], FILE **fin, FILE **fout, int *endian)
{
int inspec = 0;
int outspec = 0;
int espec = 0;
int c = 1;
char *iname;
char *oname;
*endian = -1;
/* Store the invokation name */
invok = argv[0];
while (c < argc) {
/* -be | -le */
if (!espec) {
if (!strcmp (argv[c], "-be")) {
*endian = BIG;
espec = 1;
c += 1;
continue;
} else if (!strcmp (argv[c], "-le")) {
*endian = LITTLE;
espec = 1;
c += 1;
continue;
}
}
/* input file */
if (!inspec) {
inspec = 1;
iname = argv[c];
c += 1;
continue;
}
/* output file */
if (!outspec) {
outspec = 1;
oname = argv[c];
c += 1;
continue;
}
/* Don't know what to do with the arg */
return (ERR_PARSE_TOO_MANY_ARGS);
}
/* Make sure endian is known */
if (!espec)
return (ERR_PARSE_NO_ENDIAN);
/* Open input file if not stdin */
if (inspec) {
*fin = fopen (iname, "r");
if (*fin == NULL)
return (ERR_PARSE_INPUT_OPEN_FAIL);
}
/* Open output file if not stdin */
if (outspec) {
*fout = fopen (oname, "w");
if (*fout == NULL)
return (ERR_PARSE_OUTPUT_OPEN_FAIL);
}
return (0);
} /* parseit */
/***************************************************************************************
* FUNCTION PURPOSE: Check if data is ascii
***************************************************************************************
* DESCRIPTION: Returns 1 if a byte is 0-9, a-f, 0 otherwise
***************************************************************************************/
int asciiByte (unsigned char c)
{
if ((c >= '0') && (c <= '9'))
return (1);
if ((c >= 'A') && (c <= 'F'))
return (1);
return (0);
} /* asciiByte */
/**************************************************************************************
* FUNCTION PURPOSE: Returns the binary equivalent of an ascii byte
**************************************************************************************
* DESCRIPTION: Conversion from ascii to binary
**************************************************************************************/
int toNum (unsigned char c)
{
if ((c >= '0') && (c <= '9'))
return (c - '0');
return (c - 'A' + 10);
} /* toNum */
/**********************************************************************************
* FUNCTION PURPOSE: Read a line from a file, toss it
**********************************************************************************
* DESCRIPTION: Reads a line, including the newline character, and throws it away.
**********************************************************************************/
void stripLine (FILE *s)
{
char iline[132];
fgets (iline, 131, s);
} /* stripLine */
/************************************************************************************
* FILE PURPOSE: Read the hex55 data file
************************************************************************************
* DESCRIPTION: Reads the input data file. Strips the first two lines, reads
* the byte stream.
************************************************************************************/
#define MALLOC_BLOCK_SIZE 512000
unsigned char *readBFile (FILE *fin, unsigned *n, int *errcode)
{
unsigned char *d;
unsigned allocSize;
unsigned m;
unsigned char x, y;
/* Create a block of data */
allocSize = MALLOC_BLOCK_SIZE;
d = malloc (allocSize * sizeof (unsigned char));
if (d == NULL) {
*errcode = ERR_READ_BFILE_INITIAL_MALLOC_FAIL;
if (fin != stdin)
fclose (fin);
return (NULL);
}
/* Strip the 1st two lines */
stripLine (fin);
stripLine (fin);
*errcode = 0;
m = 0;
for (;;) {
/* Read the 1st ascii char */
do {
x = fgetc (fin);
if (x == (unsigned char)EOF) {
*errcode = 0;
*n = m;
if (fin != stdin)
fclose (fin);
return (d);
}
} while (!asciiByte(x));
/* Read the next ascii char */
y = fgetc(fin);
if (y == (unsigned char)EOF) {
*errcode = 0;
*n = m;
if (fin != stdin)
fclose (fin);
return (d);
}
/* Convert the two characters into a byte */
if (asciiByte(y))
d[m++] = (toNum(x) << 4) | toNum(y);
/* Verify memory bounds */
if (m >= allocSize) {
allocSize += MALLOC_BLOCK_SIZE;
d= realloc (d, allocSize);
if (d== NULL) {
*errcode = ERR_READ_BFILE_REALLOC_FAIL;
if (fin != stdin)
fclose (fin);
return (NULL);
}
}
} /* end for */
} /* readBFile */
/**************************************************************************************
* FUNCTION PURPOSE: converts four bytes into an unsigned value
**************************************************************************************
* DESCRIPTION: Converts bytes to a value
**************************************************************************************/
unsigned value32bitAdd (int endian, unsigned char *data, unsigned n, unsigned *p, int *errflag, unsigned add)
{
unsigned v;
unsigned w;
unsigned q;
/* Verify that there are 4 values still in the character array */
if ((*p + 4) > n) {
*errflag = ERR_VALUE32_SIZE_ERR;
return (0);
}
/* Store the original pointer */
q = w = *p;
v = (unsigned)data[w+0] << 24 |
(unsigned)data[w+1] << 16 |
(unsigned)data[w+2] << 8 |
(unsigned)data[w+3] << 0 ;
*errflag = 0;
/* Add any additional value */
v = v + add;
/* Write the data back in big endian format */
data[q+0] = (v >> 24) & 0xff;
data[q+1] = (v >> 16) & 0xff;
data[q+2] = (v >> 8) & 0xff;
data[q+3] = (v >> 0) & 0xff;
*p = q+4;
return (v);
} /* value32bitAdd */
/**************************************************************************************
* FUNCTION PURPOSE: converts four bytes into an unsigned value
**************************************************************************************
* DESCRIPTION: Converts bytes to a value, depending on the endian configuration.
**************************************************************************************/
unsigned value32bit (int endian, unsigned char *data, unsigned n, unsigned *p, int *errflag)
{
return (value32bitAdd (endian, data, n, p, errflag, 0));
} /* value32bit */
/*********************************************************************************
* FUNCTION PURPOSE: Convert up to four bytes to big endian
*********************************************************************************
* DESCRIPTION: Data bytes are converted.
*********************************************************************************/
#define SWAP(x,y,z) (z)=(x);(x)=(y);(y)=(z)
void data32bit (int endian, unsigned char *data, unsigned n, unsigned *p, unsigned m, int *errflag)
{
/* Calculate the number of bytes to convert, limited to four bytes */
if (m > 4)
m = 4;
/* return an error if there are not enough values in the array */
if ((*p + m) >= n) {
*errflag = ERR_DATA32_SIZE_ERR;
return;
}
/* Clear the error flag */
*errflag = 0;
/* The data is always already in big endian, there is nothing to do but advance the pointer */
*p += m;
} /* data32bit */
void remain32bit (int endian, unsigned char *data, unsigned n, unsigned *p, unsigned m, int *errflag)
{
unsigned w;
unsigned char h;
/* return an error if the size is greater then or equal to 4 */
if (m >= 4) {
*errflag = ERR_DATA32_REMAIN_ERR;
return;
}
/* return an error if there are not enough values in the array */
if ((*p + m) >= n) {
*errflag = ERR_DATA32_SIZE_ERR;
return;
}
w = *p;
/* Only swap if endianness is little */
if (endian == LITTLE) {
/* Swap the next four bytes */
SWAP(data[w+0], data[w+3], h);
SWAP(data[w+1], data[w+2], h);
}
/* Update the full four elements */
*p = *p + 4;
} /* remain32bit */
/*********************************************************************************
* FUNCTION PURPOSE: Convert 2 bytes into an unsigned value
*********************************************************************************
* DESCRIPTION: Converts the next two bytes into an unsigned value based on
* the endian configuration.
*********************************************************************************/
unsigned value16bit (int endian, unsigned char *data, unsigned n, unsigned *p, int *errflag)
{
unsigned v;
unsigned q;
/* Verify that there are 4 values still in the character array */
if ((*p + 2) > n) {
*errflag = ERR_VALUE16_SIZE_ERR;
return (0);
}
/* Store the original pointer */
q = *p;
/* convert based on endianness. For little endain the 16 bit words are actually
* big endian, but the bytes in those words are not */
if (endian == BIG) {
v = data[(*p)++] << 8 |
data[(*p)++] << 0 ;
} else {
v = data[(*p)++] << 0 |
data[(*p)++] << 8 ;
}
*errflag = 0;
/* Write the data back in big endian format */
data[q++] = (v >> 8) & 0xff;
data[q++] = (v >> 0) & 0xff;
return (v);
} /* value16bit */
/**************************************************************************************
* FUNCTION PURPOSE: Writes a 16 bit value into the array
**************************************************************************************
* DESCRIPTION: Writes a big endian 16 bit value, increments the array pointer.
**************************************************************************************/
void write16bit (unsigned value, unsigned char *data, unsigned *p)
{
data[(*p)++] = (value >> 8) & 0xff;
data[(*p)++] = (value >> 0) & 0xff;
} /* write16bit */
/*************************************************************************************
* FUNCTION PURPOSE: Write the output file
*************************************************************************************
* DESCRIPTION: Writes the resulting output.
*************************************************************************************/
void writeBFile (FILE *fout, unsigned char *data, unsigned n)
{
unsigned i;
/* Write the two line header */
fprintf (fout, "%c\n$A000000\n", (unsigned char)2);
for (i = 0; i < n; i++) {
if ( ((i+1)%24) )
fprintf (fout, "%02X ", data[i]);
else
fprintf (fout, "%02X\n", data[i]);
}
/* Write the close character */
fprintf (fout, "\n%c", (unsigned char)3);
if (fout != stdout)
fclose (fout);
} /* writeBFile */
/**************************************************************************************
* FUNCTION PURPOSE: Main
**************************************************************************************
* DESCRIPTION: Provides the top level program flow.
**************************************************************************************/
int main (int argc, char *argv[])
{
FILE *fin; /* input stream */
FILE *fout; /* output stream */
unsigned char *data; /* The data set */
unsigned n; /* Data set size */
unsigned p; /* Data index */
unsigned v; /* Data value */
unsigned n32; /* Number of bytes that form complete 32 bit values */
unsigned r32; /* Number of bytes remaining (0-3) */
int endian; /* Endian */
int errflag; /* error indicator */
int i, j; /* loop var */
int origRegs; /* original reg count */
int shift; /* data shift amount */
/* Parse the input */
if (errflag = parseit (argc, argv, &fin, &fout, &endian)) {
showErr (errflag);
return (-1);
}
/* Read the raw data file */
data = readBFile (fin, &n, &errflag);
if (data == NULL) {
showErr (errflag);
return(-1);
}
/* Parse the sections */
p = 0;
/* The entry point */
v = value32bit (endian, data, n, &p, &errflag);
if (errflag) {
showErr (errflag);
return(-1);
}
/* The sections */
do {
/* Get the section byte count */
v = value32bit (endian, data, n, &p, &errflag);
if (errflag) {
showErr (errflag);
return(-1);
}
if (v) {
/* Convert the start address (adjusts the array index) */
value32bit (endian, data, n, &p, &errflag);
if (errflag) {
showErr (errflag);
return(-1);
}
}
/* Determine how many bytes form complete 32 bit fields, and how many are left over */
n32 = v & 0xfffffffc;
r32 = v & 0x00000003;
/* Convert the data to big endian format */
for (i = 0; i < n32; i += 4) {
data32bit (endian, data, n, &p, v-i, &errflag);
if (errflag) {
showErr (errflag);
return (-1);
}
}
/* Convert any remaining bytes. */
if (r32) {
remain32bit (endian, data, n, &p, r32, &errflag);
if (errflag) {
showErr (errflag);
return (-1);
}
}
} while (v);
/* Write out the data file */
writeBFile (fout, data, n);
/* Return resources */
free (data);
return (0);
}
|