|
|
/*
* Copyright (c) 2017-present, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/**
* \ingroup DRV_OSAL_MODULE
* \defgroup DRV_OSAL_RegisterIntr RegisterIntr
* RegisterIntr interface
*
* @{
*/
/** ============================================================================
* @file RegisterIntr.h
*
* @brief Interrupt register routines
*
*
* ============================================================================
*/
#ifndef ti_osal_RegisterIntr__include
#define ti_osal_RegisterIntr__include
#include <ti/osal/EventCombinerP.h>
#include <ti/osal/HwiP.h>
#include <ti/osal/MuxIntcP.h>
#ifdef __cplusplus
extern "C" {
#endif
#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
typedef void (*Osal_IsrRoutine)(uintptr_t arg);
/*!
* @brief Interrupt Configuration parameters for the corepac (c6x/a15/m5/a8/a9)
*/
typedef struct {
char *name; /* Name of the instance for debugging purposes, could be set to NULL */
int32_t corepacEventNum; /* Event number going in to the corepac */
int32_t intVecNum; /* Interrupt vector */
Osal_IsrRoutine isrRoutine; /* The ISR routine to hook the corepacEventNum to */
uintptr_t arg; /* Argument to the ISR routine */
uint32_t priority;
uint32_t triggerSensitivity;
} OsalRegisterIntParams_corepac_t;
/* For C6x, if intVec=16, then event combiner is to be used */
#define OSAL_REGINT_INTVEC_EVENT_COMBINER (16)
/*!
* @brief Interrupt Configuration parameters for soc mux prior to reaching the core
*/
typedef struct {
MuxIntcP_inParams *muxInParams;
MuxIntcP_outParams *muxOutParams;
} OsalRegisterIntParams_socmux_t;
/*!
* @brief Interrupt Configuration parameters for soc mux prior to reaching the core
* This is the data structure used to configure the interrupts in the system.
* coreConfig: This part configures the interrupt for corepac such as c66x, arm, m4
* socMuxConfig: This part configures the interrupt path for any SOC level mux such as CIC/GIC or cross bar,
* leading up to the corepac
*/
typedef struct {
OsalRegisterIntParams_corepac_t corepacConfig;
OsalRegisterIntParams_socmux_t socMuxConfig;
} OsalRegisterIntrParams_t;
/**
* \anchor OsalInterruptRetCode_e
* \name Osal Interrupt return Codes
* @{
*/
/*!
* @brief Return error codes for Osal Interrupt functions
*/
typedef int32_t OsalInterruptRetCode_e;
#define OSAL_INT_SUCCESS ((int32_t) 0)
/* Success return code */
#define OSAL_INT_ERR_INVALID_PARAMS ((int32_t) -1)
/* Invalid input parameters */
#define OSAL_INT_ERR_HWICREATE ((int32_t) -2)
/* Error while registering the Hwi object */
#define OSAL_INT_ERR_EVENTCOMBINER_REG ((int32_t) -3)
/* Error while registering the event combiner to the defaults */
#define OSAL_INT_ERR_DELETE ((int32_t) -4)
/* Failed to delete a Interrupt handle. */
/* @} */
void Osal_RegisterInterrupt_initParams(OsalRegisterIntrParams_t *interruptRegParams);
/*!
* @brief Function to initialize the interrupt registration configuration data structure
*
*/
OsalInterruptRetCode_e Osal_RegisterInterrupt(OsalRegisterIntrParams_t *interruptRegParams,HwiP_Handle *hwiPHandlePtr);
/*!
* @brief Function to register interrupt with parameters provided
*
*/
OsalInterruptRetCode_e Osal_DeleteInterrupt(HwiP_Handle hwiPhandle,int32_t corepacEventNum);
/*!
* @brief Function to delete interrupt corresponding to an event number
*
*/
void Osal_EnableInterrupt(int32_t corepacEvent,int32_t interruptNum);
/*!
* @brief Function to enable the interrupt corresponding to an event number
*
*/
void Osal_DisableInterrupt(int32_t corepacEvent,int32_t interruptNum);
/*!
* @brief Function to disable the interrupt corresponding to an event number
*
*/
void Osal_ClearInterrupt(int32_t corepacEvent,int32_t interruptNum);
/*!
* @brief Function to clear the interrupts corresponding to an event number
*
*/
#ifdef __cplusplus
}
#endif
#endif /* ti_osal_RegisterIntr__include */
/* @} */
|