diff options
Diffstat (limited to 'TaskP.h')
-rw-r--r-- | TaskP.h | 6 |
1 files changed, 3 insertions, 3 deletions
@@ -100,7 +100,7 @@ typedef struct TaskP_Params_s | |||
100 | * @return A TaskP_Handle on success or a NULL on an error | 100 | * @return A TaskP_Handle on success or a NULL on an error |
101 | */ | 101 | */ |
102 | extern TaskP_Handle TaskP_create(void *taskfxn, | 102 | extern TaskP_Handle TaskP_create(void *taskfxn, |
103 | TaskP_Params *params); | 103 | const TaskP_Params *params); |
104 | 104 | ||
105 | /*! | 105 | /*! |
106 | * @brief Function to delete a task. | 106 | * @brief Function to delete a task. |
@@ -147,13 +147,13 @@ extern void TaskP_setPrio(TaskP_Handle handle, uint32_t priority); | |||
147 | * @brief Function returns the Task handle of current task | 147 | * @brief Function returns the Task handle of current task |
148 | * | 148 | * |
149 | */ | 149 | */ |
150 | extern TaskP_Handle TaskP_self(); | 150 | extern TaskP_Handle TaskP_self(void); |
151 | 151 | ||
152 | /*! | 152 | /*! |
153 | * @brief Function returns the Task handle of current task.This is an inline function | 153 | * @brief Function returns the Task handle of current task.This is an inline function |
154 | * | 154 | * |
155 | */ | 155 | */ |
156 | extern TaskP_Handle TaskP_selfmacro(); | 156 | extern TaskP_Handle TaskP_selfmacro(void); |
157 | 157 | ||
158 | /*! | 158 | /*! |
159 | * @brief Function Yield processor to equal priority task | 159 | * @brief Function Yield processor to equal priority task |