/* * Copyright (c) 2018, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** * \ingroup DRV_OSAL_MODULE * \defgroup DRV_OSAL_EventP EventP * EventP interface * * @{ */ /** ============================================================================ * @file EventP.h * * @brief Event module for the RTOS Porting Interface * * * ============================================================================ */ #ifndef ti_osal_EventP__include #define ti_osal_EventP__include #ifdef __cplusplus extern "C" { #endif #include #include #include #include /* * Pre-defined Event Ids. Event_Ids are provided to simplify the specification * of andMasks and orMasks arguments to Event_pend(). * Since each Event_Id is a bitmask composed of only a single bit, * a group of Event_Ids within an andMask or orMask can be indicated by simply adding them together. */ /*! * @brief Event ID 0 */ #define EventP_ID_NONE Event_Id_NONE /*! * @brief Event ID 0 */ #define EventP_ID_00 Event_Id_00 /*! * @brief Event ID 1 */ #define EventP_ID_01 Event_Id_01 /*! * @brief Event ID 2 */ #define EventP_ID_02 Event_Id_02 /*! * @brief Event ID 3 */ #define EventP_ID_03 Event_Id_03 /*! * @brief Event ID 4 */ #define EventP_ID_04 Event_Id_04 /*! * @brief Event ID 5 */ #define EventP_ID_05 Event_Id_05 /*! * @brief Event ID 6 */ #define EventP_ID_06 Event_Id_06 /*! * @brief Event ID 7 */ #define EventP_ID_07 Event_Id_07 /*! * @brief Event ID 8 */ #define EventP_ID_08 Event_Id_08 /*! * @brief Event ID 9 */ #define EventP_ID_09 Event_Id_09 /*! * @brief Event ID 10 */ #define EventP_ID_10 Event_Id_10 /*! * @brief Status codes for EventP APIs */ typedef enum EventP_Status_e { /*! API completed successfully */ EventP_OK = 0, /*! API failed */ EventP_FAILURE = (-(int32_t)1) } EventP_Status; /*! * @brief Wait forever define */ #define EventP_WAIT_FOREVER (~((uint32_t)0U)) /*! * @brief No wait define */ #define EventP_NO_WAIT ((uint32_t)0U) /*! * @brief Opaque client reference to an instance of a EventP * * A EventP_Handle returned from the ::EventP_create represents that * instance and is used in the other instance based functions */ typedef void *EventP_Handle; /*! * @brief Basic EventP Parameters * * Structure that contains the parameters are passed into ::EventP_create * when creating a EventP instance. */ typedef struct EventP_Params_s { void *instance; /*!< Name of the task instance. */ } EventP_Params; /*! * @brief Function to create an event. * * @param params Pointer to the instance configuration parameters. * * @return A EventP_Handle on success or a NULL on an error */ extern EventP_Handle EventP_create(EventP_Params *params); /*! * @brief Function to delete an event. * * @param handle A EventP_Handle returned from EventP_create */ extern void EventP_delete(EventP_Handle *handle); /*! * @brief Initialize params structure to default values. * * @param params Pointer to the instance configuration parameters. */ extern void EventP_Params_init(EventP_Params *params); /*! * @brief Function for Event Pend * * @param handle EventP handle.created via EventP_create API * @param andMask return from pend() when ALL of these events have occurred * @param orMask return from pend() when ANY of these events have occurred * @param timeout return from pend() after this many system time units * @return All consumed events or zero if timeout */ extern uint32_t EventP_pend(EventP_Handle handle, uint32_t andMask, uint32_t orMask, uint32_t timeout); /*! * @brief Function for Event Post. * * @param handle A EventP_Handle returned from EventP_create. * @param eventMask mask of eventIds to post (must be non-zero) */ extern void EventP_post(EventP_Handle handle, uint32_t eventMask); /*! * @brief Function for Event Post. * * @param handle A EventP_Handle returned from EventP_create. * @return All un-consumed events posted to the event */ extern uint32_t EventP_getPostedEvents(EventP_Handle handle); #ifdef __cplusplus } #endif #endif /* ti_osal_EventP__include */ /* @} */