/* * Copyright (c) 2018, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /** ============================================================================ * @file TaskP.h * * @brief Task module for the RTOS Porting Interface * * * ============================================================================ */ #ifndef ti_osal_TaskP__include #define ti_osal_TaskP__include #ifdef __cplusplus extern "C" { #endif #include #include #include /*! * @brief Status codes for TaskP APIs */ typedef enum TaskP_Status_e { /*! API completed successfully */ TaskP_OK = 0, /*! API failed */ TaskP_FAILURE = (-(int32_t)1) } TaskP_Status; /*! * @brief Number Ticks by OS in 1 millisecond */ #define OS_TICKS_IN_MILLI_SEC 1 /* 1000us tick */ /*! * @brief Opaque client reference to an instance of a TaskP * * A TaskP_Handle returned from the ::TaskP_create represents that * instance and is used in the other instance based functions */ typedef void *TaskP_Handle; /*! * @brief Basic SemaphoreP Parameters * * Structure that contains the parameters are passed into ::TaskP_create * when creating a TaskP instance. */ typedef struct TaskP_Params_s { uint8_t *name; /*!< Name of the task instance. */ void *pErrBlk; /*!< Pointer to the error block for task Create */ int8_t priority; /*!< The priority of the task */ uint32_t stacksize; /*!< The stack size of the task */ void *arg0; /*!< arg0 */ void *arg1; /*!< arg1 */ void *stack; /*!< pointer to stack memory, if NULL OS will allocate internally */ } TaskP_Params; /*! * @brief Function to create a task. * * @param taskfxn Function pointer of the task. * * @param params Pointer to the instance configuration parameters. * * @return A TaskP_Handle on success or a NULL on an error */ extern TaskP_Handle TaskP_create(void *taskfxn, TaskP_Params *params); /*! * @brief Function to delete a task. * * @param handle A TaskP_Handle returned from TaskP_create * * @return Status of the functions * - TaskP__OK: Deleted the semaphore instance * - TaskP_FAILURE: Failed to delete the semaphore instance */ extern TaskP_Status TaskP_delete(TaskP_Handle *handle); /*! * @brief Initialize params structure to default values. * * @param params Pointer to the instance configuration parameters. */ extern void TaskP_Params_init(TaskP_Params *params); /*! * @brief Function for Task sleep in units of OS tick * * @param timeout sleep ticks. */ extern void TaskP_sleep(uint32_t timeout); /*! * @brief Function for Task sleep in units of msecs * * @param timeoutInMsecs sleep in units of msecs. */ extern void TaskP_sleepInMsecs(uint32_t timeoutInMsecs); /*! * @brief Function for Task sleep. * * @param handle A TaskP_Handle returned from TaskP_create. * @param priority New priority to be set. */ extern void TaskP_setPrio(TaskP_Handle handle, uint32_t priority); /*! * @brief Function returns the Task handle of current task * */ extern TaskP_Handle TaskP_self(); /*! * @brief Function returns the Task handle of current task.This is an inline function * */ extern TaskP_Handle TaskP_selfmacro(); /*! * @brief Function Yield processor to equal priority task * */ extern void TaskP_yield(void); /*! * @brief Check if task is terminated. * * Typically a task MUST be terminated before it can be deleted. * * @return 0: task is not terminated, 1: task is terminated */ extern uint32_t TaskP_isTerminated(TaskP_Handle handle); #ifdef __cplusplus } #endif #endif /* ti_osal_TaskP__include */