1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
|
/*
* Copyright (c) 2015-2018, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/** ============================================================================
* @file SemaphoreP.h
*
* @brief Semaphore module for the RTOS Porting Interface
*
* Semaphores can be counting semaphores or binary semaphores. Counting
* semaphores keep track of the number of times the semaphore has been posted
* with post functions. This is useful, for example, if you have a group of
* resources that are shared between tasks. Such tasks might call pend() to see
* if a resource is available before using one. A count of zero for a counting
* semaphore denotes that it is not available. A positive count denotes
* how many times a SemaphoreP_pend can be called before it is blocked (or
* returns SemaphoreP_TIMEOUT).
*
* Binary semaphores can have only two states: available (count = 1) and
* unavailable (count = 0). They can be used to share a single resource
* between tasks. They can also be used for a basic signalling mechanism, where
* the semaphore can be posted multiple times. Binary semaphores do not keep
* track of the count; they simply track whether the semaphore has been posted
* or not.
*
* ============================================================================
*/
#ifndef ti_osal_SemaphoreP__include
#define ti_osal_SemaphoreP__include
#ifdef __cplusplus
extern "C" {
#endif
#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
/*!
* @brief Status codes for SemaphoreP APIs
*/
typedef enum SemaphoreP_Status_e {
/*! API completed successfully */
SemaphoreP_OK = 0,
/*! API failed */
SemaphoreP_FAILURE = (-(int32_t)1),
/*! API failed because of a timeout */
SemaphoreP_TIMEOUT = (-(int32_t)2),
/*! API failed because of not supported */
SemaphoreP_UNSUPPORTED =(-(int32_t)3)
} SemaphoreP_Status;
/*!
* @brief Wait forever define
*/
#define SemaphoreP_WAIT_FOREVER (~((uint32_t)0U))
/*!
* @brief No wait define
*/
#define SemaphoreP_NO_WAIT ((uint32_t)0U)
/*!
* @brief Opaque client reference to an instance of a SemaphoreP
*
* A SemaphoreP_Handle returned from the ::SemaphoreP_create represents that
* instance and is used in the other instance based functions (e.g.
* ::SemaphoreP_post or ::SemaphoreP_pend, etc.).
*/
typedef void *SemaphoreP_Handle;
/*!
* @brief Mode of the semaphore
*/
typedef enum SemaphoreP_Mode_e {
SemaphoreP_Mode_COUNTING = 0x0,
SemaphoreP_Mode_BINARY = 0x1
} SemaphoreP_Mode;
/*!
* @brief Basic SemaphoreP Parameters
*
* Structure that contains the parameters are passed into ::SemaphoreP_create
* when creating a SemaphoreP instance. The ::SemaphoreP_Params_init function
* should be used to initialize the fields to default values before the
* application sets the fields manually. The SemaphoreP default parameters are
* noted in SemaphoreP_Params_init.
*/
typedef struct SemaphoreP_Params_s {
char *name; /*!< Name of the semaphore instance. Memory must
persist for the life of the semaphore instance */
SemaphoreP_Mode mode; /*!< Mode for the semaphore */
uint32_t maxCount; /*!< The max count allowed for counting semaphore */
} SemaphoreP_Params;
/*!
* @brief Function to create a semaphore.
*
* @param count Initial count of the semaphore. For binary semaphores,
* only values of 0 or 1 are valid.
*
* @param params Pointer to the instance configuration parameters. NULL
* denotes to use the default parameters (SemaphoreP default
* parameters as noted in ::SemaphoreP_Params_init.
*
* @return A SemaphoreP_Handle on success or a NULL on an error
*/
extern SemaphoreP_Handle SemaphoreP_create(uint32_t count,
SemaphoreP_Params *params);
/*!
* @brief Function to delete a semaphore.
*
* @param handle A SemaphoreP_Handle returned from ::SemaphoreP_create
*
* @return Status of the functions
* - SemaphoreP_OK: Deleted the semaphore instance
* - SemaphoreP_FAILED: Failed to delete the semaphore instance
*/
extern SemaphoreP_Status SemaphoreP_delete(SemaphoreP_Handle handle);
/*!
* @brief Initialize params structure to default values.
*
* The default parameters are:
* - mode: SemaphoreP_Mode_COUNTING
* - name: NULL
*
* @param params Pointer to the instance configuration parameters.
*/
extern void SemaphoreP_Params_init(SemaphoreP_Params *params);
/*!
* @brief Function to pend (wait) on a semaphore.
*
* @param handle A SemaphoreP_Handle returned from ::SemaphoreP_create
*
* @param timeout Timeout (in milliseconds) to wait for the semaphore to
* be posted (signalled).
*
* @return Status of the functions
* - SemaphoreP_OK: Obtain the semaphore
* - SemaphoreP_TIMEOUT: Timed out. Semaphore was not obtained.
* - SemaphoreP_FAILED: Non-time out failure.
*/
extern SemaphoreP_Status SemaphoreP_pend(SemaphoreP_Handle handle,
uint32_t timeout);
/*!
* @brief Function to post (signal) a semaphore.
*
* @param handle A SemaphoreP_Handle returned from ::SemaphoreP_create
*
* @return Status of the functions
* - SemaphoreP_OK: Released the semaphore
* - SemaphoreP_FAILED: Failed to post the semaphore
*/
extern SemaphoreP_Status SemaphoreP_post(SemaphoreP_Handle handle);
/*!
* @brief Function to post (signal) a semaphore from an ClockP function.
*
* @param handle A SemaphoreP_Handle returned from ::SemaphoreP_create
*
* @return Status of the functions
* - SemaphoreP_OK: Released the semaphore
* - SemaphoreP_FAILED: Failed to post the semaphore
*/
extern SemaphoreP_Status SemaphoreP_postFromClock(SemaphoreP_Handle handle);
/*!
* @brief Function to post (signal) a semaphore from an ISR.
*
* @param handle A SemaphoreP_Handle returned from ::SemaphoreP_create
*
* @return Status of the functions
* - SemaphoreP_OK: Released the semaphore
* - SemaphoreP_FAILED: Failed to post the semaphore
*/
extern SemaphoreP_Status SemaphoreP_postFromISR(SemaphoreP_Handle handle);
/*!
* @brief Function to return the count of a semaphore.
*
* @param handle A SemaphoreP_Handle returned from ::SemaphoreP_create
*
* @return The count of the semaphore
*/
extern int32_t SemaphoreP_getCount(SemaphoreP_Handle handle);
/*!
* @brief Function to clear a semaphore for resuse.
*
* @param handle A SemaphoreP_Handle returned from ::SemaphoreP_create
*/
extern SemaphoreP_Status SemaphoreP_reset(SemaphoreP_Handle handle);
#ifdef __cplusplus
}
#endif
#endif /* ti_osal_SemaphoreP__include */
|