1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
|
/*
* Copyright (c) 2018, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/** ============================================================================
* @file TaskP.h
*
* @brief Task module for the RTOS Porting Interface
*
*
* ============================================================================
*/
#ifndef ti_osal_TaskP__include
#define ti_osal_TaskP__include
#ifdef __cplusplus
extern "C" {
#endif
#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
/*!
* @brief Status codes for TaskP APIs
*/
typedef enum TaskP_Status_e
{
/*! API completed successfully */
TaskP_OK = 0,
/*! API failed */
TaskP_FAILURE = (-(int32_t)1)
} TaskP_Status;
/*!
* @brief Number Ticks by OS in 1 millisecond
*/
#define OS_TICKS_IN_MILLI_SEC 1 /* 1000us tick */
/*!
* @brief Opaque client reference to an instance of a TaskP
*
* A TaskP_Handle returned from the ::TaskP_create represents that
* instance and is used in the other instance based functions
*/
typedef void *TaskP_Handle;
/*!
* @brief Basic SemaphoreP Parameters
*
* Structure that contains the parameters are passed into ::TaskP_create
* when creating a TaskP instance.
*/
typedef struct TaskP_Params_s
{
uint8_t *name; /*!< Name of the task instance. */
void *pErrBlk; /*!< Pointer to the error block for task Create */
int8_t priority; /*!< The priority of the task */
uint32_t stacksize; /*!< The stack size of the task */
void *arg0; /*!< arg0 */
void *arg1; /*!< arg1 */
void *stack; /*!< pointer to stack memory, if NULL OS will allocate internally */
} TaskP_Params;
/*!
* @brief Function to create a task.
*
* @param taskfxn Function pointer of the task.
*
* @param params Pointer to the instance configuration parameters.
*
* @return A TaskP_Handle on success or a NULL on an error
*/
extern TaskP_Handle TaskP_create(void *taskfxn,
const TaskP_Params *params);
/*!
* @brief Function to delete a task.
*
* @param handle A TaskP_Handle returned from TaskP_create
*
* @return Status of the functions
* - TaskP__OK: Deleted the semaphore instance
* - TaskP_FAILURE: Failed to delete the semaphore instance
*/
extern TaskP_Status TaskP_delete(TaskP_Handle *handle);
/*!
* @brief Initialize params structure to default values.
*
* @param params Pointer to the instance configuration parameters.
*/
extern void TaskP_Params_init(TaskP_Params *params);
/*!
* @brief Function for Task sleep in units of OS tick
*
* @param timeout sleep ticks.
*/
extern void TaskP_sleep(uint32_t timeout);
/*!
* @brief Function for Task sleep in units of msecs
*
* @param timeoutInMsecs sleep in units of msecs.
*/
extern void TaskP_sleepInMsecs(uint32_t timeoutInMsecs);
/*!
* @brief Function for Task sleep.
*
* @param handle A TaskP_Handle returned from TaskP_create.
* @param priority New priority to be set.
*/
extern void TaskP_setPrio(TaskP_Handle handle, uint32_t priority);
/*!
* @brief Function returns the Task handle of current task
*
*/
extern TaskP_Handle TaskP_self(void);
/*!
* @brief Function returns the Task handle of current task.This is an inline function
*
*/
extern TaskP_Handle TaskP_selfmacro(void);
/*!
* @brief Function Yield processor to equal priority task
*
*/
extern void TaskP_yield(void);
/*!
* @brief Check if task is terminated.
*
* Typically a task MUST be terminated before it can be deleted.
*
* @return 0: task is not terminated, 1: task is terminated
*/
extern uint32_t TaskP_isTerminated(TaskP_Handle handle);
#ifdef __cplusplus
}
#endif
#endif /* ti_osal_TaskP__include */
|