blob: 894576e44d3c089beb63c864cd080b76b45e9558 (
plain) (
tree)
|
|
/******************************************************************************
* FILE PURPOSE: Build description for the PA LLD Package
******************************************************************************
* FILE NAME: package.bld
*
* DESCRIPTION:
* This file contains the build specification and description for the PA LLD
*
* The file takes the following parameters from the command line through the
* XDCARGS variable.
* XDCARGS[0] = PA LLD Install Type
* Valid Values are "TAR" or "SETUP"
* DEFAULT is "SETUP"
*
* Example for a valid command:
* xdc XDCARGS="SETUP" release
*
* Copyright (C) 2011, Texas Instruments, Inc.
*****************************************************************************/
/* List of all subdirectories that combine to make the PA LLD Package. */
var subDirectories = [ "src", "docs", "fw", "example", "test" , "device"];
var palldInstallType;
/* Check if we need to create the Makefiles? */
var miniBuild = java.lang.System.getenv("MINI_PACKAGE");
/* Determine if we need to create the InstallJammer Application or not?
* PA LLD Deliverables be either of the following formats:
* - TAR Ball Package
* - Setup Executable
* DEFAULT is a SETUP Executable. */
if ((arguments[0] != "TAR") && (arguments[0] != "SETUP"))
palldInstallType = "TAR";
else
palldInstallType = arguments[0];
/* Irrespective of the InstallType we always create a TAR Ball Package as a part
* of the RTSC Build. Here we determine the name of the TAR Ball Package
* Format is as follows:
* palld_<version> */
var palldRTSCFileName = "palld" + "_" + palldPartNumber + "_" +
palldReleaseVersion[0] + "_" + palldReleaseVersion[1] + "_" +
palldReleaseVersion[2] + "_" + palldReleaseVersion[3];
/******************************************************************
************************ Release Banner **************************
******************************************************************/
print ("************* PA LLD Build Information *************");
print ("PA LLD Install : " + palldInstallType);
print ("PA LLD Version : " + palldReleaseVersion);
print ("C66 Tools Directory : " + c66ToolsBaseDir);
print ("A15 Tools Directory : " + a15ToolsBaseDir);
print ("RTSC File Name : " + palldRTSCFileName);
print ("PA LLD Path : " + palldPath);
print ("Coverity Analysis : " + (coverityAnalysis == "ON" ? "ON" : "OFF"));
if(xdcTargetType == "ARM11")
{
print ("ARM LE opts : " + TIArmv6le.ccOpts.prefix);
print ("ARM BE opts : " + TIArmv6be.ccOpts.prefix);
}
else
{
print ("A15 basic opts : " + A15LE.ccOpts.prefix);
print ("C66 LE opts : " + C66LE.ccOpts.prefix);
print ("C66 BE opts : " + C66BE.ccOpts.prefix);
}
print ("***********************************************************");
/* Create the release package for the PA LLD */
Pkg.defaultRelease = Pkg.addRelease (palldRTSCFileName, {prefix: "./packages/"});
/* Moving forward we need to set the Archiver of the package to be ZIP. This is currently
* not supported in the XDC tools being used. Currenly builds need to be done with the
* following options:-
* xdc MK_FIXLISTOPTS=-t release
* ZIP is a better option as it works natively with INSTALL Jammer and we can remove the
* uncompression into a temporary directory. XDC Tools with xdc-rXX support the ZIP archiver. */
//Pkg.attrs = {archiver : "zip"};
/* Cycle through all the sub-directories and build all the files */
for (var i = 0; i < subDirectories.length; i++)
{
/* Load the capsule in the sub directory. */
var caps = xdc.loadCapsule (subDirectories[i]+"/Module.xs");
print ("Building directory " + subDirectories[i]);
/* Build the capsule. */
caps.modBuild();
/* Package the module.xs files for building via package */
Pkg.otherFiles[Pkg.otherFiles.length++] = subDirectories[i]+"/Module.xs";
}
/* Package the remaining files */
Pkg.otherFiles[Pkg.otherFiles.length++] = "config.bld";
Pkg.otherFiles[Pkg.otherFiles.length++] = "package.bld";
Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xdc";
Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xs";
Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc";
Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc.xdt";
Pkg.otherFiles[Pkg.otherFiles.length++] = "pa.h";
Pkg.otherFiles[Pkg.otherFiles.length++] = "pa_fc.h";
Pkg.otherFiles[Pkg.otherFiles.length++] = "paver.h";
Pkg.otherFiles[Pkg.otherFiles.length++] = "paver.h.xdt";
Pkg.otherFiles[Pkg.otherFiles.length++] = "pasahost.h";
Pkg.otherFiles[Pkg.otherFiles.length++] = "pa_osal.h";
Pkg.otherFiles[Pkg.otherFiles.length++] = "nss_if.h";
Pkg.otherFiles[Pkg.otherFiles.length++] = "nss_cfg.h";
Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/Doxyfile";
Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/doxyfile.xdt";
Pkg.otherFiles[Pkg.otherFiles.length++] = "build/buildlib.xs";
Pkg.otherFiles[Pkg.otherFiles.length++] = "makefile";
Pkg.otherFiles[Pkg.otherFiles.length++] = "makefile_armv7";
Pkg.otherFiles[Pkg.otherFiles.length++] = "build/armv7/libpa_aearmv7.mk";
/* Generate Users Manual Doxyfile */
var tplt = xdc.loadTemplate("./docs/doxyfile.xdt");
tplt.genFile("./docs/Doxyfile",palldReleaseVersion);
/* Generate Settings.xdc */
var tplt = xdc.loadTemplate("./Settings.xdc.xdt");
tplt.genFile("./Settings.xdc",palldReleaseVersion);
/* Generate paver.h */
var tplt = xdc.loadTemplate("./paver.h.xdt");
tplt.genFile("./paver.h",palldReleaseVersion);
/*********************************************************************
*********************** INSTALL-JAMMER Support **********************
* In order to create the InstallJammer Application; we need to UNTAR
* the package into a temporary directory. This is required because
* currently the InstallJammer does not support the TAR Files and thus
* creating an UNTAR of the file. So to work-around the problem we will
* do the following in the EPILOGUE Section:-
* (a) Create a temporary directory called 'tmp'
* (b) UNTAR the package into 'tmp'
* (c) Run the INSTALL Jammer on 'tmp'
* (d) Remove the 'tmp' directory.
*
* This can be done only after the 'release' package has been created.
* Thus all of this work is being done in the EPILOGUE.
*********************************************************************/
if (palldInstallType == "SETUP")
{
/* Create the Install Jammer Version Variable. This is used inside the
* MPI File to create the Final executable.
* The format supported is as follows:-
* - setupwin32_palld-<part_number>-<version>.exe
*/
var InstallJammerVersion = "-DVersion " + palldPartNumber + "_" +
palldReleaseVersion[0] + "_" + palldReleaseVersion[1] + "_" +
palldReleaseVersion[2] + "_" + palldReleaseVersion[3];
/* This is the location where the tmp directory is located; this is used as
* the input directory for the Install Jammer. */
var PackageBaseDir = " -DPackageBaseDir " + palldPath + "./tmp";
/* This is the location where the PA LLD will be installed by default. */
var WinInstallDir = " -DWinInstallDir C:/Program Files/Texas Instruments/palld" + "_" +
palldPartNumber + "_" +
palldReleaseVersion[0] + "_" + palldReleaseVersion[1] + "_" +
palldReleaseVersion[2] + "_" + palldReleaseVersion[3];
/* Create the actual EPILOGUE Section for the INSTALLER */
Pkg.makeEpilogue += "release: install_application\n";
Pkg.makeEpilogue += "install_application: firmware\n";
Pkg.makeEpilogue += "\t @echo -------------------------------------------------------\n";
Pkg.makeEpilogue += "\t @echo Creating the Install\n";
Pkg.makeEpilogue += "\t @echo -------------------------------------------------------\n";
Pkg.makeEpilogue += "\t -$(MKDIR) tmp\n";
Pkg.makeEpilogue += "\t -$(MKDIR) tmp/packages\n";
Pkg.makeEpilogue += "\t -$(MKDIR) tmp/eclipse\n";
Pkg.makeEpilogue += "\t -$(CP) -R eclipse tmp\n";
Pkg.makeEpilogue += "\t tar -xf ./packages/" + palldRTSCFileName + ".tar" + " -Ctmp/packages \n";
Pkg.makeEpilogue += "\t installjammer " + InstallJammerVersion + PackageBaseDir + WinInstallDir +
" --output-dir packages/ --build install/palld.mpi\n";
Pkg.makeEpilogue += "\t -$(RMDIR) /S /Q tmp\n\n";
/* We need to clean after ourselves; extend the 'clean' target to take care of this. */
Pkg.makeEpilogue += "clean::\n";
Pkg.makeEpilogue += "\t $(RM) packages/*.exe\n";
Pkg.makeEpilogue += "\t $(RM) packages/*.bin\n";
Pkg.makeEpilogue += "\t $(RMDIR) /S /Q eclipse\n";
Pkg.makeEpilogue += "\t $(RMDIR) /S /Q tmp\n";
}
if (miniBuild == "ON")
{
/***************************************************************************
********************************* MINI Package ****************************
***************************************************************************/
/* Create the MINI RTSC Package */
var additionalFiles = [];
additionalFiles[additionalFiles.length++] = "fw/classify1_bin.c";
additionalFiles[additionalFiles.length++] = "fw/classify2_bin.c";
additionalFiles[additionalFiles.length++] = "fw/pam_bin.c";
additionalFiles[additionalFiles.length++] = "fw/pafw.h";
var libUtility = xdc.loadCapsule ("build/buildlib.xs");
libUtility.createMiniPkg(palldRTSCFileName, additionalFiles);
}
|