diff options
Diffstat (limited to 'fw/v1/pa2_in4_pdsp0_bin.c')
-rw-r--r-- | fw/v1/pa2_in4_pdsp0_bin.c | 8 |
1 files changed, 4 insertions, 4 deletions
diff --git a/fw/v1/pa2_in4_pdsp0_bin.c b/fw/v1/pa2_in4_pdsp0_bin.c index d883d7b..10aba0a 100644 --- a/fw/v1/pa2_in4_pdsp0_bin.c +++ b/fw/v1/pa2_in4_pdsp0_bin.c | |||
@@ -74,9 +74,9 @@ | |||
74 | const uint32_t in4_pdsp0[] = { | 74 | const uint32_t in4_pdsp0[] = { |
75 | 0x21000300, | 75 | 0x21000300, |
76 | 0xbabe0401, | 76 | 0xbabe0401, |
77 | 0x03000109, | 77 | 0x03000110, |
78 | 0x2302b59e, | 78 | 0x2302b59e, |
79 | 0x24010982, | 79 | 0x24011082, |
80 | 0x240300c2, | 80 | 0x240300c2, |
81 | 0x81043782, | 81 | 0x81043782, |
82 | 0x2eff8582, | 82 | 0x2eff8582, |
@@ -1635,8 +1635,8 @@ const uint32_t in4_pdsp0[] = { | |||
1635 | 0x513c6002, | 1635 | 0x513c6002, |
1636 | 0x21062100, | 1636 | 0x21062100, |
1637 | 0x90800680, | 1637 | 0x90800680, |
1638 | 0x01014040, | 1638 | 0x010140c2, |
1639 | 0x090340c2, | 1639 | 0x0903c2c2, |
1640 | 0x00c28080, | 1640 | 0x00c28080, |
1641 | 0x21061400, | 1641 | 0x21061400, |
1642 | 0x90800600, | 1642 | 0x90800600, |