1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
|
/**
* @file pa_osal.h
*
* @brief
* This is the sample OS Adaptation layer which is used by the PA low level
* driver.
*
* @details The OSAL layer can be ported in either of the following manners to a native OS:
*
* <b> Approach 1: </b>
* @n Use Prebuilt Libraries
* - Ensure that the LLD users provide an implementation of all
* Osal_XXX API for their native OS.
* - Link the prebuilt libraries with their application.
* - Refer to the "test" directory for an example of this
* @n <b> Pros: </b>
* - Customers can reuse prebuilt TI provided libraries
* @n <b> Cons: </b>
* - Level of indirection in the API to get to the actual OS call
*
* <b> Approach 2: </b>
* @n Rebuilt Library
* - Create a copy of this file and modify it to directly
* inline the native OS calls
* - Rebuild the PA low level driver library; ensure that the Include
* path points to the directory where the copy of this file
* has been provided.
* - Please refer to the "test" directory for an example of this
* @n <b> Pros: </b>
* - Optimizations can be done to remove the level of indirection
* @n <b> Cons: </b>
* - PA LLD Libraries need to be rebuilt by the customer.
*
* \par
* NOTE:
* (C) Copyright 2009-2011 Texas Instruments, Inc.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
#ifndef _PA_OSAL_H
#define _PA_OSAL_H
/** @addtogroup PA_LLD_OSAL
@{ */
/**********************************************************************
************************* Extern Declarations ************************
**********************************************************************/
extern void Osal_paBeginMemAccess (void* addr, uint32_t size);
extern void Osal_paEndMemAccess (void* addr, uint32_t size);
extern void Osal_paMtCsEnter (uint32_t *key);
extern void Osal_paMtCsExit (uint32_t key);
/**
* @brief This macro is used to alert the application that the PA is
* going to access a block of memory. The application must ensure
* cache coherency for multi-core applications
*
* <b> Prototype: </b>
* The following is the C prototype for the expected OSAL API.
*
* @verbatim
void Osal_paBeginMemAccess (void* addr, uint32_t sizeWords)
@endverbatim
*
* <b> Parameters </b>
* @n The address of the table to be accessed
* @n The number of bytes in the table
*
* @note PA will make nested calls to this function for memory access
* protection of different memory tables.
*/
#define Pa_osalBeginMemAccess Osal_paBeginMemAccess
/**
* @brief This macro is used to alert the application that the PA
* has completed access to a block of memory. If the memory block is
* cached then the application would need to ensure that the contents
* of the cache are updated immediately to the actual memory.
*
* <b> Prototype: </b>
* The following is the C prototype for the expected OSAL API.
*
* @verbatim
void Osal_paEndMemAccess (void* addr, uint32_t sizeWords)
@endverbatim
*
* <b> Parameters </b>
* @n The address of the table to be accessed
* @n The number of bytes in the table
*
* @note PA will make nested calls to this function for memory access
* protection of different memory tables.
*/
#define Pa_osalEndMemAccess Osal_paEndMemAccess
/**
* @brief The macro is used by the PA LLD to provide critical section to
* protect its global and shared resources access from multiple cores.
* If the PALLD operates in single-core environment then these macros can
* be defined to be NOP.
*
* <b> Prototype: </b>
* The following is the C prototype for the expected OSAL API.
*
* @verbatim
void Osal_paMtCsEnter (uint32_t *key)
@endverbatim
*
* <b> Parameter </b>
* @n Key may be used to lock the multi-core critical section.
*
* <b> Return Value </b>
* @n Not applicable.
*
* @note The multiple-core protection area is usually pretty small. To avoid the scenario that the
* interrupt occurs after the multi-core lock is achieved, the interrupt may be disabled in
* this function and re-enabled at the function Osal_saMtCsExit.
*/
#define Pa_osalMtCsEnter Osal_paMtCsEnter
/**
* @brief The macro is used by the PA LLD to exit a critical section
* protected using the Osal_paMtCsEnter() API.
*
* <b> Prototype: </b>
* The following is the C prototype for the expected OSAL API.
*
* @verbatim
void Osal_paMtCsExit (uint32_t key)
@endverbatim
*
* <b> Parameter </b>
* @n Key may be used to lock the multi-core critical section.
*
* <b> Return Value </b>
* @n Not applicable.
*/
#define Pa_osalMtCsExit Osal_paMtCsExit
/**
@}
*/
#endif /* _PA_OSAL_H */
|