blob: 2f3f897bbfd186c12e89b55243b49b04260a8b3c (
plain) (
blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
|
/******************************************************************************
* FILE PURPOSE: Build description for the pruss Driver
******************************************************************************
* FILE NAME: package.bld
*
* DESCRIPTION:
* This file contains the build specification and description for the pruss driver
*
* The file takes the following parameters from the command line through the
* XDCARGS variable.
* XDCARGS[0] = Driver Install Type
* Valid Values are "TAR" or "SETUP"
* DEFAULT is "SETUP"
*
* Example for a valid command:
* xdc XDCARGS="SETUP" release
*
* Copyright (C) 2014-2016, Texas Instruments, Inc.
*****************************************************************************/
/* List of all subdirectories that combine to make the pruss Socket Driver Package. */
var subDirectories = [ "src", "docs", "include", "test", "example", "soc" ];
var driverInstallType;
/* Determine if we need to create the InstallJammer Application or not?
* pruss LLD Deliverables be either of the following formats:
* - TAR Ball Package
* - Setup Executable
* DEFAULT is a SETUP Executable. */
if ((arguments[0] != "TAR") && (arguments[0] != "SETUP"))
driverInstallType = "TAR";
else
driverInstallType = arguments[0];
/* Irrespective of the InstallType we always create a TAR Ball Package as a part
* of the RTSC Build. Here we determine the name of the TAR Ball Package
* Format is as follows:
* pruss_<version> */
var prussRTSCFileName = "pruss" + "_" +
driverReleaseVersion[0] + "_" + driverReleaseVersion[1] + "_" +
driverReleaseVersion[2] + "_" + driverReleaseVersion[3];
/******************************************************************
************************ Release Banner **************************
******************************************************************/
print ("************* pruss Socket Driver Build Information *************");
print ("pruss Socket Driver Install : " + driverInstallType);
print ("pruss Socket Driver LLD Version : " + driverReleaseVersion);
print ("C66 Tools Directory : " + c66ToolsBaseDir);
print ("M4 Tools Directory : " + m4ToolsBaseDir);
print ("A15 Tools Directory : " + a15ToolsBaseDir);
print ("RTSC File Name : " + prussRTSCFileName);
print ("pruss Socket Driver LLD Path : " + driverPath);
if (pOpts == 1)
{
print ("CC LE opts : " + C66LE.ccOpts.prefix);
print ("CC BE opts : " + C66BE.ccOpts.prefix);
print ("M4 LE opts : " + M4LE.ccOpts.prefix);
print ("A15 basic opts : " + A15LE.ccOpts.prefix);
}
print ("****************************************************************");
/* Create the release package for the pruss LLD */
Pkg.defaultRelease = Pkg.addRelease (prussRTSCFileName, {prefix: "./packages/"});
/* Moving forward we need to set the Archiver of the package to be ZIP. This is currently
* not supported in the XDC tools being used. Currenly builds need to be done with the
* following options:-
* xdc MK_FIXLISTOPTS=-t release
* ZIP is a better option as it works natively with INSTALL Jammer and we can remove the
* uncompression into a temporary directory. XDC Tools with xdc-rXX support the ZIP archiver. */
//Pkg.attrs = {archiver : "zip"};
/* Cycle through all the sub-directories and build all the files */
for (var i = 0; i < subDirectories.length; i++)
{
/* Load the capsule in the sub directory. */
var caps = xdc.loadCapsule (subDirectories[i]+"/Module.xs");
print ("Building directory " + subDirectories[i]);
/* Build the capsule. */
caps.modBuild();
/* Package the module.xs files for building via package */
Pkg.otherFiles[Pkg.otherFiles.length++] = subDirectories[i]+"/Module.xs";
}
/* Package the remaining files */
Pkg.otherFiles[Pkg.otherFiles.length++] = "config.bld";
Pkg.otherFiles[Pkg.otherFiles.length++] = "config_mk.bld";
Pkg.otherFiles[Pkg.otherFiles.length++] = "package.bld";
Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xdc";
Pkg.otherFiles[Pkg.otherFiles.length++] = "package.xs";
Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc";
Pkg.otherFiles[Pkg.otherFiles.length++] = "Settings.xdc.xdt";
Pkg.otherFiles[Pkg.otherFiles.length++] = "pruicss.h";
Pkg.otherFiles[Pkg.otherFiles.length++] = "pruicss_ver.h";
Pkg.otherFiles[Pkg.otherFiles.length++] = "pruicss_ver.h.xdt";
Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/Doxyfile";
Pkg.otherFiles[Pkg.otherFiles.length++] = "docs/doxyfile.xdt";
Pkg.otherFiles[Pkg.otherFiles.length++] = "build/buildlib.xs";
Pkg.otherFiles[Pkg.otherFiles.length++] = "makefile";
Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile.mk";
Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_indp.mk";
Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_profile_indp.mk";
Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_profile.mk";
Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_sorte_master.mk";
Pkg.otherFiles[Pkg.otherFiles.length++] = "build/makefile_sorte_slave.mk";
Pkg.otherFiles[Pkg.otherFiles.length++] = "src/src_files_common.mk";
Pkg.otherFiles[Pkg.otherFiles.length++] = "pruss_component.mk";
Pkg.otherFiles[Pkg.otherFiles.length++] = "./lib";
/* Generate Users Manual Doxyfile */
var tplt = xdc.loadTemplate("./docs/doxyfile.xdt");
tplt.genFile("./docs/Doxyfile",driverReleaseVersion);
/* Generate Settings.xdc */
var tplt = xdc.loadTemplate("./Settings.xdc.xdt");
tplt.genFile("./Settings.xdc",driverReleaseVersion);
/* Generate paver.h */
var tplt = xdc.loadTemplate("./pruicss_ver.h.xdt");
tplt.genFile("./pruicss_ver.h",driverReleaseVersion);
|