@REM ****************************************************************************** @REM * FILE PURPOSE: Environment Setup for building QMSS LLD @REM ****************************************************************************** @REM * FILE NAME: setupenv.bat @REM * @REM * DESCRIPTION: @REM * Configures and sets up the Build Environment @REM * @REM * Copyright (C) 2011, Texas Instruments, Inc. @REM ***************************************************************************** @echo --------------------------------------- @echo Configuring QMSS LLD Build Environment @echo off IF DEFINED PARTNO GOTO partno_defined @REM Configure the Part Number set PARTNO=keystone2 :partno_Defined IF DEFINED PDK_INSTALL_PATH GOTO pdk_defined set PDK_INSTALL_PATH=../../.. :pdk_defined @REM --------------------------------- @REM Enabling MINI PACKAGE to be Built @REM --------------------------------- set MINI_PACKAGE=OFF @echo MINI PACKAGE is set to %MINI_PACKAGE% @REM --------------------------------- @REM Enabling debug flags @REM --------------------------------- set EXTDBGFLAGS=-mn -g @REM This is the base location for the various tools. set XDCCGROOT=T:/c6xx/cgen7_3_02/c6000/cgtools set C6X_GEN_INSTALL_PATH=T:\c6xx\cgen7_3_02\c6000\cgtools REM ******************************************************************************* REM *************************** XDC PATH Configuration **************************** REM ******************************************************************************* REM QMSS LLD depends upon the following packages:- REM - CSL Package for the CSL Register Layer REM These packages should be installed before trying to build the driver else REM compilations will fail. @REM Specify the XDC Tool Path set XDC_INSTALL_PATH=T:/gen/xdc/xdctools_3_22_04_46 set XDCPATH=../../..;%XDC_INSTALL_PATH%/packages @REM Configure the XDCPATH set XDCPATH=%XDCPATH%;%PDK_INSTALL_PATH%;%C6X_GEN_INSTALL_PATH%/include @REM Eclipse Help Plugin (Not required by customers) set XDC_ECLIPSE_PLUGIN_INSTALL_PATH=T:/gen/xdc/xdc_eclipse_plugin_gen/20091203 set XDC_FILTER_INSTALL_PATH=T:/gen/xdc/xdcFilter/20100428 set XDCPATH=%XDCPATH%;%XDC_ECLIPSE_PLUGIN_INSTALL_PATH% set XDCPATH=%XDCPATH%;%XDC_FILTER_INSTALL_PATH% @REM Configure the paths to ensure that the XDC is available. set PATH=%XDC_INSTALL_PATH%;%XDC_INSTALL_PATH%\bin;T:\Doxygen\doxygen\1.5.1-p1\bin @REM Third Party Tools: Install-Jammer (Not required by customers) set PATH=%PATH%;T:\gen\InstallJammer\v1_2_05 set PATH=%PATH%;%XDCCGROOT%\bin;T:\gen\gnu\99-11-01\cygwin-b20\H-i586-cygwin32\bin set PATH=%PATH%;T:\SDOApps\cg_xml\cg_xml_v2_30_00\bin set PATH=%PATH%;T:\ti_pdsp_cgen\20111216 @REM Third Party Tools: HTML Help compiler. set PATH=%PATH%;T:\Doxygen\HTML_Help_Workshop\10-01-2007 @REM Environment Variable which control STATIC Analysis of the code set STATIC_ANALYZE_PATH=T:\gen\coverity\prevent-mingw-3.4.0 set PATH=%PATH%;%STATIC_ANALYZE_PATH%\bin @REM Set the Title Window appropriately. Title QMSS LLD Build Environment @echo QMSS LLD Build Environment Configured @echo ---------------------------------------