| Commit message (Collapse) | Author | Age | Files | Lines |
|
|
|
|
|
|
|
|
|
|
| |
Active maintenance and development of the contents of this repository
has been relocated to git.ti.com/processor-sdk/pdk.git under the path
packages/ti/drv/usb.
The use of this repository has been deprecated and will no longer
receive updates.
Signed-off-by: Jacob Stiffler <j-stiffler@ti.com>
|
|\
| |
| |
| |
| |
| |
| | |
PRSDK-7296_close_fatfs_after_unplug to master
* commit '352b6ee8a8816bf755742a47d68d62f3b0f8fcb7':
Close FATFS when device disconnect detected
|
|/
|
|
|
|
| |
After the application detects that the USB device is unplugged
it needs to close the FATFS so that when it is openned again with
new device it would have correct data
|
|\
| |
| |
| |
| | |
* commit '28248d276a5528637b86c104dac14df4828f8fc8':
Fix all Doxygen warning seen in all the .h files
|
| | |
|
|\|
| |
| |
| |
| |
| |
| | |
master
* commit '4f088e187737159f1d502af8426fc57242258a55':
Fix automotive Jenkin build after updating Cdn drv
|
|/ |
|
|\
| |
| |
| |
| |
| |
| |
| |
| | |
to master
* commit 'fe0306f1df8c1994fe7746ecdf2ef3a44bf9a2f9':
Update docs.
Update changes to match TI PDK
Update to Cadence 2.0.4 driver
|
| | |
|
| |
| |
| |
| |
| | |
Move some xhci buffers to non-cache area
Fix semaphore crash
|
|/
|
|
| |
Update to latest Cadence bare-metal USB driver (2.0.4)
|
|\
| |
| |
| |
| |
| |
| | |
master
* commit 'a69eee82ce89ea8325e203abc5798787e6110542':
Removing UART include from driver
|
| | |
|
|\|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
master
* commit '9ea86fc068ef1605968fb00c59e1415f06558b50':
Add more example src files to automotive packaging
Add example source files into packages
Packaging j721e example's linkers and BIOS cfg files
Fix error i& warning when build with CPLUSPLUS=yes
Fix type mismatch
Fix for PRSDK-7092
|
| | |
|
| | |
|
| | |
|
| | |
|
| | |
|
|/ |
|
|\
| |
| |
| |
| |
| |
| | |
to master
* commit '7d738fc060b672f967f1473f066a43e7f59ceeb0':
Disabling J7 due to Build issue
|
|/
|
|
| |
Signed-off-by: Ankur <a0132173@ti.com>
|
|\
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
* commit '1adf4face5c619d14ccf4b5f7384d971105a4903': (38 commits)
Fix Omap13x MSC USB caused by DMA_MULTIBUFFER_ALLOCATION
Fix Omap13x MSC USB caused by DMA_MULTIBUFFER_ALLOCATION
Fix USB audio issue on AM335x
remove J7 sim
Sync with latest CSL
Move noncache MSMC setting to USB
Update release notes and disable debug_printf
Synch the MSC changes to MUSB host
Add custom linker files for J7
Uinifying AM65xx and J721e builds
Restore previous version of xhci to non-j7
Merge Master branch to j721_usb
USB dev bulk application is now working
MCU J7 USB dev MSC is now working
USB3.0 host MSC working
Clear g_sUSBHCD to fix some enumeration issues
Move error codes to error.h
Fix perf measurement
Fix USB host for release build profile
Fix connection/disconnection problem
...
|
| |\
| | |
| | |
| | | |
ssh://bitbucket.itg.ti.com/processor-sdk/usb into j721_to_master
|
| | |
| | |
| | |
| | |
| | |
| | | |
New USB stack uses fixed EpReq. The multiallocation options replaced
the RxBuffer in the EpReq while the MSC stack still expects the
received data coming from the buffer it passes to the driver.
|
| |/
| |
| |
| |
| |
| | |
New USB stack uses fixed EpReq. The multiallocation options replaced
the RxBuffer in the EpReq while the MSC stack still expects the
received data coming from the buffer it passes to the driver.
|
| |
| |
| |
| |
| | |
Fix USB audio issue on AM335x
Restore inEpReq and outEpReq in usbMusbDcdDevice_t so that interrupt routing in Omap13x does not break
|
| | |
|
| | |
|
| |
| |
| |
| |
| |
| |
| | |
Move non-cache section setting from OSAL to USB so that
other non-cache section settings are in one place inside USB.
Update the GPIO interrupt number with latest CSL
|
| |\
| |/
|/| |
|
|\ \
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
PRSDK-6167_enable_compliance_mode to master
* commit '63d5bb75e4017f0c7304228d7bf77dedd19ec725':
Fix make release error
Enable compliance state early during USB host init
|
| | | |
|
|/ /
| |
| |
| |
| |
| |
| |
| | |
Currently USB host doesn't get to compliance mode if USB probe is connected
to USB port before the controller is starting up.
Move the code that enable compliance mode to right after the controller is
set to host mode and after we poll for the PR bit to go low
|
|\ \
| | |
| | |
| | |
| | |
| | |
| | | |
PRSDK-5873_PRSDK-5867_move_DMSC_reserve to master
* commit '8c3bdae6bdb94f3a2b742492bdbfc5bcfb23a0d1':
Change the USB LLD examples linker files
|
| |\ \
| |/ /
|/| |
| | | |
PRSDK-5873_PRSDK-5867_move_DMSC_reserve
|
|\ \ \
| | | |
| | | |
| | | |
| | | | |
* commit '7545dca27fc4701b569665b87c20a773c68a6598':
Docs update
|
| | | | |
|
|\| | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
PRSDK-5873_PRSDK-5867_move_DMSC_reserve to master
* commit '458bc4ba27ae61bbf5debb5a297bdeaa26ce23ce':
Move linker files with no-cache sections to USB example
Update USB examples with new linker files
|
|\ \ \ \
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
PRSDK-5653_usb_config_declaration_mismatch to master
* commit '0a4f1d2492209a7da6add67c4f8323c6a39f7fdd':
Change USB_Config from const to non-const
Moving away from const USB_Config
|
| | | | | |
|
| |\ \ \ \
| |/ / / /
|/| | | | |
|
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
USB_Config can be set dynamically during run time so need to change
it to non-const.
Also fix linking error due to mismatch declarations of
consts variables
|
| | |/ /
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Change all USB CCS examples on AM65xx to use local linker files
instead of from the ti/build infrastructure. These local linker files
move the DMSC reserved localtion to end of MSMC to match with
actual DMSC firewalls.
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
CSL does not init an non-cache section in MSMC.
So moving build infrastructure linker files with non-cache sections to internal USB examples
The ti/build linker files no longer have these non-cache sections
|
| |/ /
|/| |
| | |
| | |
| | |
| | |
| | | |
DMSC changes its firewalled memory. Update the examples to use these
new linker files in ti/build infrastructure.
Update the non-cache section addresses based on the new linker file
|
|\ \ \
| | | |
| | | |
| | | |
| | | | |
* commit 'a1cff62fcf7b5798f2a7661d17e1ad15c17b59df':
PRSDK-4453 Rename SMP example name in align with other LLD examples
|
|/ / / |
|
|\ \ \
| | | |
| | | |
| | | |
| | | |
| | | | |
* commit 'c5fdcce7422d2e013e2727caa7d142f56031cab4':
PRSDK-4453 Add SMP enable examples for A15 and A53
PRSDK-4453 Update makefile for SMP mode
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Add USB example with SMP enabled for AM65xx and AM572x EVM
Update component makefile to add entry for SMP enabled test.
Add RTSC project text file and config file for AM572x EVM to create SMP
enabled project.
|