aboutsummaryrefslogblamecommitdiffstats
blob: f76196d0740976001e964c444fe2fb13c9dcc3a4 (plain) (tree)
1
2
3
4
5
6
7




                                                                     

                                                                       

















                                                                            
                         


                            

   



                                                        

                                              
   
                                                                               

                                             
                                 
 


                                                                   
 
                      




















                                                                      
                            
                  



                                    


                                                               
         



                                   




                                                       
                                                               















                                                               
/*
 * Lock-less NULL terminated single linked list
 *
 * The basic atomic operation of this list is cmpxchg on long.  On
 * architectures that don't have NMI-safe cmpxchg implementation, the
 * list can NOT be used in NMI handlers.  So code that uses the list in
 * an NMI handler should depend on CONFIG_ARCH_HAVE_NMI_SAFE_CMPXCHG.
 *
 * Copyright 2010,2011 Intel Corp.
 *   Author: Huang Ying <ying.huang@intel.com>
 *
 * This program is free software; you can redistribute it and/or
 * modify it under the terms of the GNU General Public License version
 * 2 as published by the Free Software Foundation;
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
 */
#include <linux/kernel.h>
#include <linux/export.h>
#include <linux/interrupt.h>
#include <linux/llist.h>


/**
 * llist_add_batch - add several linked entries in batch
 * @new_first:	first entry in batch to be added
 * @new_last:	last entry in batch to be added
 * @head:	the head for your lock-less list
 *
 * Return whether list is empty before adding.
 */
bool llist_add_batch(struct llist_node *new_first, struct llist_node *new_last,
		     struct llist_head *head)
{
	struct llist_node *first;

	do {
		new_last->next = first = ACCESS_ONCE(head->first);
	} while (cmpxchg(&head->first, first, new_first) != first);

	return !first;
}
EXPORT_SYMBOL_GPL(llist_add_batch);

/**
 * llist_del_first - delete the first entry of lock-less list
 * @head:	the head for your lock-less list
 *
 * If list is empty, return NULL, otherwise, return the first entry
 * deleted, this is the newest added one.
 *
 * Only one llist_del_first user can be used simultaneously with
 * multiple llist_add users without lock.  Because otherwise
 * llist_del_first, llist_add, llist_add (or llist_del_all, llist_add,
 * llist_add) sequence in another user may change @head->first->next,
 * but keep @head->first.  If multiple consumers are needed, please
 * use llist_del_all or use lock between consumers.
 */
struct llist_node *llist_del_first(struct llist_head *head)
{
	struct llist_node *entry, *old_entry, *next;

	entry = head->first;
	for (;;) {
		if (entry == NULL)
			return NULL;
		old_entry = entry;
		next = entry->next;
		entry = cmpxchg(&head->first, old_entry, next);
		if (entry == old_entry)
			break;
	}

	return entry;
}
EXPORT_SYMBOL_GPL(llist_del_first);

/**
 * llist_reverse_order - reverse order of a llist chain
 * @head:	first item of the list to be reversed
 *
 * Reverse the order of a chain of llist entries and return the
 * new first entry.
 */
struct llist_node *llist_reverse_order(struct llist_node *head)
{
	struct llist_node *new_head = NULL;

	while (head) {
		struct llist_node *tmp = head;
		head = head->next;
		tmp->next = new_head;
		new_head = tmp;
	}

	return new_head;
}
EXPORT_SYMBOL_GPL(llist_reverse_order);