aboutsummaryrefslogblamecommitdiffstats
blob: 1ac414fd50300384663248c0ac651c9887bfe45d (plain) (tree)
1
2
3
4
5
6
7
8




                                                                            
                                                                               
 
                                                                      
















                                                                       

                                                                          
                                         
                                                                       


                                                                  
                                                    
 



























                                                                         
                                        
                                                                        












                                                                          







                                                        


                                                       



                                                                        



                                                        

















                                                       

                                                             
                                           







                                                                  
                                                            





                                                              
                                           








                                                                       
                                                                              




                                                                 
                                              





                                                                    
                                             







                                                                   
                                               




                                                                           
# ==========================================================================
# Building binaries on the host system
# Binaries are used during the compilation of the kernel, for example
# to preprocess a data file.
#
# Both C and C++ are supported, but preferred language is C for such utilities.
#
# Sample syntax (see Documentation/kbuild/makefiles.txt for reference)
# hostprogs-y := bin2hex
# Will compile bin2hex.c and create an executable named bin2hex
#
# hostprogs-y    := lxdialog
# lxdialog-objs := checklist.o lxdialog.o
# Will compile lxdialog.c and checklist.c, and then link the executable
# lxdialog, based on checklist.o and lxdialog.o
#
# hostprogs-y      := qconf
# qconf-cxxobjs   := qconf.o
# qconf-objs      := menu.o
# Will compile qconf as a C++ program, and menu as a C program.
# They are linked as C++ code to the executable qconf

# hostprogs-y := conf
# conf-objs  := conf.o libkconfig.so
# libkconfig-objs := expr.o type.o
# Will create a shared library named libkconfig.so that consists of
# expr.o and type.o (they are both compiled as C code and the object files
# are made as position independent code).
# conf.c is compiled as a C program, and conf.o is linked together with
# libkconfig.so as the executable conf.
# Note: Shared libraries consisting of C++ files are not supported

__hostprogs := $(sort $(hostprogs-y) $(hostprogs-m))

# C code
# Executables compiled from a single .c file
host-csingle	:= $(foreach m,$(__hostprogs),$(if $($(m)-objs),,$(m)))

# C executables linked based on several .o files
host-cmulti	:= $(foreach m,$(__hostprogs),\
		   $(if $($(m)-cxxobjs),,$(if $($(m)-objs),$(m))))

# Object (.o) files compiled from .c files
host-cobjs	:= $(sort $(foreach m,$(__hostprogs),$($(m)-objs)))

# C++ code
# C++ executables compiled from at least on .cc file
# and zero or more .c files
host-cxxmulti	:= $(foreach m,$(__hostprogs),$(if $($(m)-cxxobjs),$(m)))

# C++ Object (.o) files compiled from .cc files
host-cxxobjs	:= $(sort $(foreach m,$(host-cxxmulti),$($(m)-cxxobjs)))

# Shared libaries (only .c supported)
# Shared libraries (.so) - all .so files referenced in "xxx-objs"
host-cshlib	:= $(sort $(filter %.so, $(host-cobjs)))
# Remove .so files from "xxx-objs"
host-cobjs	:= $(filter-out %.so,$(host-cobjs))

#Object (.o) files used by the shared libaries
host-cshobjs	:= $(sort $(foreach m,$(host-cshlib),$($(m:.so=-objs))))

# output directory for programs/.o files
# hostprogs-y := tools/build may have been specified. Retrieve directory
host-objdirs := $(foreach f,$(__hostprogs), $(if $(dir $(f)),$(dir $(f))))
# directory of .o files from prog-objs notation
host-objdirs += $(foreach f,$(host-cmulti),                  \
                    $(foreach m,$($(f)-objs),                \
                        $(if $(dir $(m)),$(dir $(m)))))
# directory of .o files from prog-cxxobjs notation
host-objdirs += $(foreach f,$(host-cxxmulti),                  \
                    $(foreach m,$($(f)-cxxobjs),                \
                        $(if $(dir $(m)),$(dir $(m)))))

host-objdirs := $(strip $(sort $(filter-out ./,$(host-objdirs))))


__hostprogs     := $(addprefix $(obj)/,$(__hostprogs))
host-csingle	:= $(addprefix $(obj)/,$(host-csingle))
host-cmulti	:= $(addprefix $(obj)/,$(host-cmulti))
host-cobjs	:= $(addprefix $(obj)/,$(host-cobjs))
host-cxxmulti	:= $(addprefix $(obj)/,$(host-cxxmulti))
host-cxxobjs	:= $(addprefix $(obj)/,$(host-cxxobjs))
host-cshlib	:= $(addprefix $(obj)/,$(host-cshlib))
host-cshobjs	:= $(addprefix $(obj)/,$(host-cshobjs))
host-objdirs    := $(addprefix $(obj)/,$(host-objdirs))

obj-dirs += $(host-objdirs)

#####
# Handle options to gcc. Support building with separate output directory

_hostc_flags   = $(HOSTCFLAGS)   $(HOST_EXTRACFLAGS)   \
                 $(HOSTCFLAGS_$(basetarget).o)
_hostcxx_flags = $(HOSTCXXFLAGS) $(HOST_EXTRACXXFLAGS) \
                 $(HOSTCXXFLAGS_$(basetarget).o)

ifeq ($(KBUILD_SRC),)
__hostc_flags	= $(_hostc_flags)
__hostcxx_flags	= $(_hostcxx_flags)
else
__hostc_flags	= -I$(obj) $(call flags,_hostc_flags)
__hostcxx_flags	= -I$(obj) $(call flags,_hostcxx_flags)
endif

hostc_flags    = -Wp,-MD,$(depfile) $(__hostc_flags)
hostcxx_flags  = -Wp,-MD,$(depfile) $(__hostcxx_flags)

#####
# Compile programs on the host

# Create executable from a single .c file
# host-csingle -> Executable
quiet_cmd_host-csingle 	= HOSTCC  $@
      cmd_host-csingle	= $(HOSTCC) $(hostc_flags) -o $@ $< \
	  	$(HOST_LOADLIBES) $(HOSTLOADLIBES_$(@F))
$(host-csingle): $(obj)/%: $(src)/%.c FORCE
	$(call if_changed_dep,host-csingle)

# Link an executable based on list of .o files, all plain c
# host-cmulti -> executable
quiet_cmd_host-cmulti	= HOSTLD  $@
      cmd_host-cmulti	= $(HOSTCC) $(HOSTLDFLAGS) -o $@ \
			  $(addprefix $(obj)/,$($(@F)-objs)) \
			  $(HOST_LOADLIBES) $(HOSTLOADLIBES_$(@F))
$(host-cmulti): $(obj)/%: $(host-cobjs) $(host-cshlib) FORCE
	$(call if_changed,host-cmulti)

# Create .o file from a single .c file
# host-cobjs -> .o
quiet_cmd_host-cobjs	= HOSTCC  $@
      cmd_host-cobjs	= $(HOSTCC) $(hostc_flags) -c -o $@ $<
$(host-cobjs): $(obj)/%.o: $(src)/%.c FORCE
	$(call if_changed_dep,host-cobjs)

# Link an executable based on list of .o files, a mixture of .c and .cc
# host-cxxmulti -> executable
quiet_cmd_host-cxxmulti	= HOSTLD  $@
      cmd_host-cxxmulti	= $(HOSTCXX) $(HOSTLDFLAGS) -o $@ \
			  $(foreach o,objs cxxobjs,\
			  $(addprefix $(obj)/,$($(@F)-$(o)))) \
			  $(HOST_LOADLIBES) $(HOSTLOADLIBES_$(@F))
$(host-cxxmulti): $(obj)/%: $(host-cobjs) $(host-cxxobjs) $(host-cshlib) FORCE
	$(call if_changed,host-cxxmulti)

# Create .o file from a single .cc (C++) file
quiet_cmd_host-cxxobjs	= HOSTCXX $@
      cmd_host-cxxobjs	= $(HOSTCXX) $(hostcxx_flags) -c -o $@ $<
$(host-cxxobjs): $(obj)/%.o: $(src)/%.cc FORCE
	$(call if_changed_dep,host-cxxobjs)

# Compile .c file, create position independent .o file
# host-cshobjs -> .o
quiet_cmd_host-cshobjs	= HOSTCC  -fPIC $@
      cmd_host-cshobjs	= $(HOSTCC) $(hostc_flags) -fPIC -c -o $@ $<
$(host-cshobjs): $(obj)/%.o: $(src)/%.c FORCE
	$(call if_changed_dep,host-cshobjs)

# Link a shared library, based on position independent .o files
# *.o -> .so shared library (host-cshlib)
quiet_cmd_host-cshlib	= HOSTLLD -shared $@
      cmd_host-cshlib	= $(HOSTCC) $(HOSTLDFLAGS) -shared -o $@ \
			  $(addprefix $(obj)/,$($(@F:.so=-objs))) \
			  $(HOST_LOADLIBES) $(HOSTLOADLIBES_$(@F))
$(host-cshlib): $(obj)/%: $(host-cshobjs) FORCE
	$(call if_changed,host-cshlib)

targets += $(host-csingle)  $(host-cmulti) $(host-cobjs)\
	   $(host-cxxmulti) $(host-cxxobjs) $(host-cshlib) $(host-cshobjs)