diff options
author | Linus Torvalds | 2013-12-02 12:09:07 -0600 |
---|---|---|
committer | Linus Torvalds | 2013-12-02 12:09:07 -0600 |
commit | 5fc92de3c7106d17f85c245383ba072d810d6bb0 (patch) | |
tree | 1e27a49e82ca9736144cc73ad5544a7ddf906644 /crypto | |
parent | b0d8d2292160bb63de1972361ebed100c64b5b37 (diff) | |
parent | 833846e8fa0c51fb3e47bca8adfdd7b10643b737 (diff) | |
download | linux-phy-5fc92de3c7106d17f85c245383ba072d810d6bb0.tar.gz linux-phy-5fc92de3c7106d17f85c245383ba072d810d6bb0.tar.xz linux-phy-5fc92de3c7106d17f85c245383ba072d810d6bb0.zip |
Merge git://git.kernel.org/pub/scm/linux/kernel/git/davem/net
Pull networking updates from David Miller:
"Here is a pile of bug fixes that accumulated while I was in Europe"
1) In fixing kernel leaks to userspace during copying of socket
addresses, we broke a case that used to work, namely the user
providing a buffer larger than the in-kernel generic socket address
structure. This broke Ruby amongst other things. Fix from Dan
Carpenter.
2) Fix regression added by byte queue limit support in 8139cp driver,
from Yang Yingliang.
3) The addition of MSG_SENDPAGE_NOTLAST buggered up a few sendpage
implementations, they should just treat it the same as MSG_MORE.
Fix from Richard Weinberger and Shawn Landden.
4) Handle icmpv4 errors received on ipv6 SIT tunnels correctly, from
Oussama Ghorbel. In particular we should send an ICMPv6 unreachable
in such situations.
5) Fix some regressions in the recent genetlink fixes, in particular
get the pmcraid driver to use the new safer interfaces correctly.
From Johannes Berg.
6) macvtap was converted to use a per-cpu set of statistics, but some
code was still bumping tx_dropped elsewhere. From Jason Wang.
7) Fix build failure of xen-netback due to missing include on some
architectures, from Andy Whitecroft.
8) macvtap double counts received packets in statistics, fix from Vlad
Yasevich.
9) Fix various cases of using *_STATS_BH() when *_STATS() is more
appropriate. From Eric Dumazet and Hannes Frederic Sowa.
10) Pktgen ipsec mode doesn't update the ipv4 header length and checksum
properly after encapsulation. Fix from Fan Du.
* git://git.kernel.org/pub/scm/linux/kernel/git/davem/net: (61 commits)
net/mlx4_en: Remove selftest TX queues empty condition
{pktgen, xfrm} Update IPv4 header total len and checksum after tranformation
virtio_net: make all RX paths handle erors consistently
virtio_net: fix error handling for mergeable buffers
virtio_net: Fixed a trivial typo (fitler --> filter)
netem: fix gemodel loss generator
netem: fix loss 4 state model
netem: missing break in ge loss generator
net/hsr: Support iproute print_opt ('ip -details ...')
net/hsr: Very small fix of comment style.
MAINTAINERS: Added net/hsr/ maintainer
ipv6: fix possible seqlock deadlock in ip6_finish_output2
ixgbe: Make ixgbe_identify_qsfp_module_generic static
ixgbe: turn NETIF_F_HW_L2FW_DOFFLOAD off by default
ixgbe: ixgbe_fwd_ring_down needs to be static
e1000: fix possible reset_task running after adapter down
e1000: fix lockdep warning in e1000_reset_task
e1000: prevent oops when adapter is being closed and reset simultaneously
igb: Fixed Wake On LAN support
inet: fix possible seqlock deadlocks
...
Diffstat (limited to 'crypto')
-rw-r--r-- | crypto/algif_hash.c | 3 | ||||
-rw-r--r-- | crypto/algif_skcipher.c | 3 |
2 files changed, 6 insertions, 0 deletions
diff --git a/crypto/algif_hash.c b/crypto/algif_hash.c index ef5356cd280a..850246206b12 100644 --- a/crypto/algif_hash.c +++ b/crypto/algif_hash.c | |||
@@ -114,6 +114,9 @@ static ssize_t hash_sendpage(struct socket *sock, struct page *page, | |||
114 | struct hash_ctx *ctx = ask->private; | 114 | struct hash_ctx *ctx = ask->private; |
115 | int err; | 115 | int err; |
116 | 116 | ||
117 | if (flags & MSG_SENDPAGE_NOTLAST) | ||
118 | flags |= MSG_MORE; | ||
119 | |||
117 | lock_sock(sk); | 120 | lock_sock(sk); |
118 | sg_init_table(ctx->sgl.sg, 1); | 121 | sg_init_table(ctx->sgl.sg, 1); |
119 | sg_set_page(ctx->sgl.sg, page, size, offset); | 122 | sg_set_page(ctx->sgl.sg, page, size, offset); |
diff --git a/crypto/algif_skcipher.c b/crypto/algif_skcipher.c index 6a6dfc062d2a..a19c027b29bd 100644 --- a/crypto/algif_skcipher.c +++ b/crypto/algif_skcipher.c | |||
@@ -378,6 +378,9 @@ static ssize_t skcipher_sendpage(struct socket *sock, struct page *page, | |||
378 | struct skcipher_sg_list *sgl; | 378 | struct skcipher_sg_list *sgl; |
379 | int err = -EINVAL; | 379 | int err = -EINVAL; |
380 | 380 | ||
381 | if (flags & MSG_SENDPAGE_NOTLAST) | ||
382 | flags |= MSG_MORE; | ||
383 | |||
381 | lock_sock(sk); | 384 | lock_sock(sk); |
382 | if (!ctx->more && ctx->used) | 385 | if (!ctx->more && ctx->used) |
383 | goto unlock; | 386 | goto unlock; |