diff options
author | Linus Torvalds | 2014-01-21 19:51:34 -0600 |
---|---|---|
committer | Linus Torvalds | 2014-01-21 19:51:34 -0600 |
commit | f075e0f6993f41c72dbb1d3e7a2d7740f14e89e2 (patch) | |
tree | a25b464a67fffc6f43940e0e85e2735a48bb1ad7 /init | |
parent | 5cb7398caf69e3943df78435a19a8a77fe8b9463 (diff) | |
parent | dd4b0a4676907481256d16d5de0851b315a6f22c (diff) | |
download | linux-phy-f075e0f6993f41c72dbb1d3e7a2d7740f14e89e2.tar.gz linux-phy-f075e0f6993f41c72dbb1d3e7a2d7740f14e89e2.tar.xz linux-phy-f075e0f6993f41c72dbb1d3e7a2d7740f14e89e2.zip |
Merge branch 'for-3.14' of git://git.kernel.org/pub/scm/linux/kernel/git/tj/cgroup
Pull cgroup updates from Tejun Heo:
"The bulk of changes are cleanups and preparations for the upcoming
kernfs conversion.
- cgroup_event mechanism which is and will be used only by memcg is
moved to memcg.
- pidlist handling is updated so that it can be served by seq_file.
Also, the list is not sorted if sane_behavior. cgroup
documentation explicitly states that the file is not sorted but it
has been for quite some time.
- All cgroup file handling now happens on top of seq_file. This is
to prepare for kernfs conversion. In addition, all operations are
restructured so that they map 1-1 to kernfs operations.
- Other cleanups and low-pri fixes"
* 'for-3.14' of git://git.kernel.org/pub/scm/linux/kernel/git/tj/cgroup: (40 commits)
cgroup: trivial style updates
cgroup: remove stray references to css_id
doc: cgroups: Fix typo in doc/cgroups
cgroup: fix fail path in cgroup_load_subsys()
cgroup: fix missing unlock on error in cgroup_load_subsys()
cgroup: remove for_each_root_subsys()
cgroup: implement for_each_css()
cgroup: factor out cgroup_subsys_state creation into create_css()
cgroup: combine css handling loops in cgroup_create()
cgroup: reorder operations in cgroup_create()
cgroup: make for_each_subsys() useable under cgroup_root_mutex
cgroup: css iterations and css_from_dir() are safe under cgroup_mutex
cgroup: unify pidlist and other file handling
cgroup: replace cftype->read_seq_string() with cftype->seq_show()
cgroup: attach cgroup_open_file to all cgroup files
cgroup: generalize cgroup_pidlist_open_file
cgroup: unify read path so that seq_file is always used
cgroup: unify cgroup_write_X64() and cgroup_write_string()
cgroup: remove cftype->read(), ->read_map() and ->write()
hugetlb_cgroup: convert away from cftype->read()
...
Diffstat (limited to 'init')
-rw-r--r-- | init/Kconfig | 3 |
1 files changed, 1 insertions, 2 deletions
diff --git a/init/Kconfig b/init/Kconfig index 5236dc562a36..8d402e33b7fc 100644 --- a/init/Kconfig +++ b/init/Kconfig | |||
@@ -854,7 +854,6 @@ config NUMA_BALANCING | |||
854 | 854 | ||
855 | menuconfig CGROUPS | 855 | menuconfig CGROUPS |
856 | boolean "Control Group support" | 856 | boolean "Control Group support" |
857 | depends on EVENTFD | ||
858 | help | 857 | help |
859 | This option adds support for grouping sets of processes together, for | 858 | This option adds support for grouping sets of processes together, for |
860 | use with process control subsystems such as Cpusets, CFS, memory | 859 | use with process control subsystems such as Cpusets, CFS, memory |
@@ -921,6 +920,7 @@ config MEMCG | |||
921 | bool "Memory Resource Controller for Control Groups" | 920 | bool "Memory Resource Controller for Control Groups" |
922 | depends on RESOURCE_COUNTERS | 921 | depends on RESOURCE_COUNTERS |
923 | select MM_OWNER | 922 | select MM_OWNER |
923 | select EVENTFD | ||
924 | help | 924 | help |
925 | Provides a memory resource controller that manages both anonymous | 925 | Provides a memory resource controller that manages both anonymous |
926 | memory and page cache. (See Documentation/cgroups/memory.txt) | 926 | memory and page cache. (See Documentation/cgroups/memory.txt) |
@@ -1160,7 +1160,6 @@ config UIDGID_STRICT_TYPE_CHECKS | |||
1160 | 1160 | ||
1161 | config SCHED_AUTOGROUP | 1161 | config SCHED_AUTOGROUP |
1162 | bool "Automatic process group scheduling" | 1162 | bool "Automatic process group scheduling" |
1163 | select EVENTFD | ||
1164 | select CGROUPS | 1163 | select CGROUPS |
1165 | select CGROUP_SCHED | 1164 | select CGROUP_SCHED |
1166 | select FAIR_GROUP_SCHED | 1165 | select FAIR_GROUP_SCHED |