aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorArnd Bergmann2010-08-15 11:52:59 -0500
committerArnd Bergmann2010-10-15 08:53:27 -0500
commit6038f373a3dc1f1c26496e60b6c40b164716f07e (patch)
treea0d3bbd026eea41b9fc36b8c722cbaf56cd9f825 /samples
parent1ec5584e3edf9c4bf2c88c846534d19cf986ba11 (diff)
downloadlinux-phy-6038f373a3dc1f1c26496e60b6c40b164716f07e.tar.gz
linux-phy-6038f373a3dc1f1c26496e60b6c40b164716f07e.tar.xz
linux-phy-6038f373a3dc1f1c26496e60b6c40b164716f07e.zip
llseek: automatically add .llseek fop
All file_operations should get a .llseek operation so we can make nonseekable_open the default for future file operations without a .llseek pointer. The three cases that we can automatically detect are no_llseek, seq_lseek and default_llseek. For cases where we can we can automatically prove that the file offset is always ignored, we use noop_llseek, which maintains the current behavior of not returning an error from a seek. New drivers should normally not use noop_llseek but instead use no_llseek and call nonseekable_open at open time. Existing drivers can be converted to do the same when the maintainer knows for certain that no user code relies on calling seek on the device file. The generated code is often incorrectly indented and right now contains comments that clarify for each added line why a specific variant was chosen. In the version that gets submitted upstream, the comments will be gone and I will manually fix the indentation, because there does not seem to be a way to do that using coccinelle. Some amount of new code is currently sitting in linux-next that should get the same modifications, which I will do at the end of the merge window. Many thanks to Julia Lawall for helping me learn to write a semantic patch that does all this. ===== begin semantic patch ===== // This adds an llseek= method to all file operations, // as a preparation for making no_llseek the default. // // The rules are // - use no_llseek explicitly if we do nonseekable_open // - use seq_lseek for sequential files // - use default_llseek if we know we access f_pos // - use noop_llseek if we know we don't access f_pos, // but we still want to allow users to call lseek // @ open1 exists @ identifier nested_open; @@ nested_open(...) { <+... nonseekable_open(...) ...+> } @ open exists@ identifier open_f; identifier i, f; identifier open1.nested_open; @@ int open_f(struct inode *i, struct file *f) { <+... ( nonseekable_open(...) | nested_open(...) ) ...+> } @ read disable optional_qualifier exists @ identifier read_f; identifier f, p, s, off; type ssize_t, size_t, loff_t; expression E; identifier func; @@ ssize_t read_f(struct file *f, char *p, size_t s, loff_t *off) { <+... ( *off = E | *off += E | func(..., off, ...) | E = *off ) ...+> } @ read_no_fpos disable optional_qualifier exists @ identifier read_f; identifier f, p, s, off; type ssize_t, size_t, loff_t; @@ ssize_t read_f(struct file *f, char *p, size_t s, loff_t *off) { ... when != off } @ write @ identifier write_f; identifier f, p, s, off; type ssize_t, size_t, loff_t; expression E; identifier func; @@ ssize_t write_f(struct file *f, const char *p, size_t s, loff_t *off) { <+... ( *off = E | *off += E | func(..., off, ...) | E = *off ) ...+> } @ write_no_fpos @ identifier write_f; identifier f, p, s, off; type ssize_t, size_t, loff_t; @@ ssize_t write_f(struct file *f, const char *p, size_t s, loff_t *off) { ... when != off } @ fops0 @ identifier fops; @@ struct file_operations fops = { ... }; @ has_llseek depends on fops0 @ identifier fops0.fops; identifier llseek_f; @@ struct file_operations fops = { ... .llseek = llseek_f, ... }; @ has_read depends on fops0 @ identifier fops0.fops; identifier read_f; @@ struct file_operations fops = { ... .read = read_f, ... }; @ has_write depends on fops0 @ identifier fops0.fops; identifier write_f; @@ struct file_operations fops = { ... .write = write_f, ... }; @ has_open depends on fops0 @ identifier fops0.fops; identifier open_f; @@ struct file_operations fops = { ... .open = open_f, ... }; // use no_llseek if we call nonseekable_open //////////////////////////////////////////// @ nonseekable1 depends on !has_llseek && has_open @ identifier fops0.fops; identifier nso ~= "nonseekable_open"; @@ struct file_operations fops = { ... .open = nso, ... +.llseek = no_llseek, /* nonseekable */ }; @ nonseekable2 depends on !has_llseek @ identifier fops0.fops; identifier open.open_f; @@ struct file_operations fops = { ... .open = open_f, ... +.llseek = no_llseek, /* open uses nonseekable */ }; // use seq_lseek for sequential files ///////////////////////////////////// @ seq depends on !has_llseek @ identifier fops0.fops; identifier sr ~= "seq_read"; @@ struct file_operations fops = { ... .read = sr, ... +.llseek = seq_lseek, /* we have seq_read */ }; // use default_llseek if there is a readdir /////////////////////////////////////////// @ fops1 depends on !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier readdir_e; @@ // any other fop is used that changes pos struct file_operations fops = { ... .readdir = readdir_e, ... +.llseek = default_llseek, /* readdir is present */ }; // use default_llseek if at least one of read/write touches f_pos ///////////////////////////////////////////////////////////////// @ fops2 depends on !fops1 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier read.read_f; @@ // read fops use offset struct file_operations fops = { ... .read = read_f, ... +.llseek = default_llseek, /* read accesses f_pos */ }; @ fops3 depends on !fops1 && !fops2 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier write.write_f; @@ // write fops use offset struct file_operations fops = { ... .write = write_f, ... + .llseek = default_llseek, /* write accesses f_pos */ }; // Use noop_llseek if neither read nor write accesses f_pos /////////////////////////////////////////////////////////// @ fops4 depends on !fops1 && !fops2 && !fops3 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier read_no_fpos.read_f; identifier write_no_fpos.write_f; @@ // write fops use offset struct file_operations fops = { ... .write = write_f, .read = read_f, ... +.llseek = noop_llseek, /* read and write both use no f_pos */ }; @ depends on has_write && !has_read && !fops1 && !fops2 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier write_no_fpos.write_f; @@ struct file_operations fops = { ... .write = write_f, ... +.llseek = noop_llseek, /* write uses no f_pos */ }; @ depends on has_read && !has_write && !fops1 && !fops2 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier read_no_fpos.read_f; @@ struct file_operations fops = { ... .read = read_f, ... +.llseek = noop_llseek, /* read uses no f_pos */ }; @ depends on !has_read && !has_write && !fops1 && !fops2 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; @@ struct file_operations fops = { ... +.llseek = noop_llseek, /* no read or write fn */ }; ===== End semantic patch ===== Signed-off-by: Arnd Bergmann <arnd@arndb.de> Cc: Julia Lawall <julia@diku.dk> Cc: Christoph Hellwig <hch@infradead.org>
Diffstat (limited to 'samples')
-rw-r--r--samples/kfifo/bytestream-example.c1
-rw-r--r--samples/kfifo/inttype-example.c1
-rw-r--r--samples/kfifo/record-example.c1
-rw-r--r--samples/tracepoints/tracepoint-sample.c1
4 files changed, 4 insertions, 0 deletions
diff --git a/samples/kfifo/bytestream-example.c b/samples/kfifo/bytestream-example.c
index 178061e87ffe..cfe40addda76 100644
--- a/samples/kfifo/bytestream-example.c
+++ b/samples/kfifo/bytestream-example.c
@@ -148,6 +148,7 @@ static const struct file_operations fifo_fops = {
148 .owner = THIS_MODULE, 148 .owner = THIS_MODULE,
149 .read = fifo_read, 149 .read = fifo_read,
150 .write = fifo_write, 150 .write = fifo_write,
151 .llseek = noop_llseek,
151}; 152};
152 153
153static int __init example_init(void) 154static int __init example_init(void)
diff --git a/samples/kfifo/inttype-example.c b/samples/kfifo/inttype-example.c
index 71b2aabca96a..6f8e79e76c9e 100644
--- a/samples/kfifo/inttype-example.c
+++ b/samples/kfifo/inttype-example.c
@@ -141,6 +141,7 @@ static const struct file_operations fifo_fops = {
141 .owner = THIS_MODULE, 141 .owner = THIS_MODULE,
142 .read = fifo_read, 142 .read = fifo_read,
143 .write = fifo_write, 143 .write = fifo_write,
144 .llseek = noop_llseek,
144}; 145};
145 146
146static int __init example_init(void) 147static int __init example_init(void)
diff --git a/samples/kfifo/record-example.c b/samples/kfifo/record-example.c
index e68bd16a5da4..2d7529eeb294 100644
--- a/samples/kfifo/record-example.c
+++ b/samples/kfifo/record-example.c
@@ -155,6 +155,7 @@ static const struct file_operations fifo_fops = {
155 .owner = THIS_MODULE, 155 .owner = THIS_MODULE,
156 .read = fifo_read, 156 .read = fifo_read,
157 .write = fifo_write, 157 .write = fifo_write,
158 .llseek = noop_llseek,
158}; 159};
159 160
160static int __init example_init(void) 161static int __init example_init(void)
diff --git a/samples/tracepoints/tracepoint-sample.c b/samples/tracepoints/tracepoint-sample.c
index 26fab33ffa8c..f4d89e008c32 100644
--- a/samples/tracepoints/tracepoint-sample.c
+++ b/samples/tracepoints/tracepoint-sample.c
@@ -30,6 +30,7 @@ static int my_open(struct inode *inode, struct file *file)
30 30
31static const struct file_operations mark_ops = { 31static const struct file_operations mark_ops = {
32 .open = my_open, 32 .open = my_open,
33 .llseek = noop_llseek,
33}; 34};
34 35
35static int __init sample_init(void) 36static int __init sample_init(void)