summaryrefslogtreecommitdiffstats
Commit message (Expand)AuthorAgeFilesLines
* execute_command.sh: update the check for /etc/profile.d filesHEADmasterHongmei Gou2017-06-281-3/+4
* execute_command.sh: execute /etc/profile.d/*.sh only when they existHongmei Gou2017-06-261-4/+7
* execute_command.sh: Remove refresh_screen.Jacob Stiffler2015-09-241-2/+0
* execute_command.sh: Set up default environment for matrix apps.Jacob Stiffler2015-03-201-0/+8
* Remove border from HTML 5 appsFranklin S. Cooper Jr2014-08-211-0/+5
* index.php: Generate json.txt if file is emptyFranklin S Cooper Jr2014-02-071-1/+1
* Update makefile to include install errorFranklin S Cooper Jr2014-02-051-0/+5
* Add support for application icons for various resolutionsFranklin S. Cooper Jr2013-06-053-3/+3
* Add php page to allow commands to be executedFranklin S. Cooper Jr2013-06-051-0/+9
* Add support for HTML 5 applicationsFranklin S. Cooper Jr2013-06-052-4/+41
* matrix-gui-v2: Enhance to all allow double quotes on executable argumentsJeff Lance2012-05-012-2/+2
* Makefile: Add a simple makefile for build clean installChase Maupin2012-04-041-0/+13
* matrix-gui-v2: Auto Resolution DetectionFranklin S Cooper Jr2012-01-309-59/+66
* matrix-gui-v2: Fix bug with .desktop and Json.txt filesFranklin S Cooper Jr2012-01-262-10/+8
* matrix-gui-v2: Bug fixesgeneration-fixFranklin S Cooper Jr2012-01-266-5/+46
* LICENSE: clarify licensingChase Maupin2012-01-231-0/+5
* matrix-gui-v2: Generate json.txt file when neededFranklin S Cooper Jr2011-12-231-0/+12
* matrix-gui-v2: Matrix v2 restructuringFranklin S Cooper Jr2011-12-2214-766/+536
* matrix-gui: Set icon image for Remote Matrix to 96x96Franklin Cooper Jr2011-11-301-0/+5
* matrix-gui: Added support for tab characterFranklin Cooper Jr2011-11-301-2/+4
* matrix_gui: Updated to use the new refresh screen applicationFranklin Cooper Jr2011-11-221-1/+1
* matrix-gui: Added License information and Modified some filesFranklin Cooper Jr2011-11-2114-71/+312
* matrix-gui: Updated some various visual aspects of MatrixFranklin Cooper Jr2011-11-215-27/+106
* matrix-gui-v2: Updated support for 640x480 screensFranklin Cooper Jr2011-11-184-4/+64
* Added support for am335x and am180x. Console application's output now use a f...Franklin Cooper Jr2011-11-1712-121/+201
* Fixed issue in IE. Single bracket was missing and prevented the app_descripti...Franklin Cooper Jr2011-10-271-1/+1
* Prevent apps/scripts that doesn't have a lock from creating a -1 lock fileFranklin Cooper Jr2011-10-271-2/+3
* Added check for lock incase the -1 to indicate there is nothing in the menu o...Franklin Cooper Jr2011-10-271-1/+2
* Moved around the div tags for app_description, title and all the possible err...Franklin Cooper Jr2011-10-272-10/+10
* Deleting am37x-evm.css file from repo. Was deleted by the previous commit but...Franklin Cooper Jr2011-10-271-71/+0
* Moved the console output files to a new directory called tmp. Moved the lock ...Franklin Cooper Jr2011-10-276-13/+106
* This commit changes which pages worry about passing lock information. Previou...Franklin Cooper Jr2011-10-253-66/+87
* Updated the generate script to be case insensitive when searching for .deskto...Franklin Cooper Jr2011-10-241-4/+6
* Changed the fetching of the output txt from using a php script to read the fi...scroll-disableFranklin Cooper Jr2011-10-232-4/+5
* Fixed issue in IE 7 that prevented links from being clicked onFranklin Cooper Jr2011-10-231-3/+3
* Added HTML Document Type for IE so that the javascript code will work properl...Franklin Cooper Jr2011-10-224-52/+66
* Remove final references to YUI. Updated the jquery javascript library to use ...Franklin Cooper Jr2011-10-223-9528/+14
* Alot of javascript cleanup was done. Also added ProgramType support to the ge...Franklin Cooper Jr2011-10-226-88/+120
* Added Up Directory/Aka Back featureFranklin Cooper Jr2011-10-214-12/+36
* Included the change that the div's output will automatically display the late...Franklin Cooper Jr2011-10-211-0/+2
* Removed swiping gestureFranklin Cooper Jr2011-10-214-188/+24
* Updated to correct TI logo. Disable the Main Menu button when a script is ru...Franklin Cooper Jr2011-10-215-4/+5
* Added fix to also redirect error output to the txt file which is read into th...Franklin Cooper Jr2011-10-201-1/+1
* Made the fix for dragging images on the subarctic evmFranklin Cooper Jr2011-10-201-0/+9
* Increased the swipe distance needed to swipe to next page if there are more a...Franklin Cooper Jr2011-10-204-8/+8
* Merge branch 'franklin' of git://gitorious.org/matrix-gui-v2/matrix-gui-v2 in...Franklin Cooper Jr2011-10-200-0/+0
|\
| * Fixed the coming soon feature to take the user to a seperate page and letting...Franklin Cooper Jr2011-10-201-0/+51
* | Amending commit. Fixed the coming soon feature to take the user to a seperate...Franklin Cooper Jr2011-10-202-7/+53
|/
* Fix issued where gui applications werent runningFranklin Cooper Jr2011-10-201-1/+5
* Fix issues with IE 8 that resulted in running scripts not properly working an...Franklin Cooper Jr2011-10-204-77/+48