summaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* matrix_browser: update for QWebEngine from QWebKitHEADmastere-ruei1@ti.com2017-08-284-9/+4
| | | | | | | Replace QWebkit with QWebEngine because QWebkit is obslete. Signed-off-by: Eric Ruei <e-ruei1@ti.com> Signed-off-by: Jacob Stiffler <j-stiffler@ti.com>
* MatrixWebView.h MatrixWebView.cpp main.cpp: Replace QWebView with ↵Eric Ruei2016-06-123-10/+16
| | | | | | | | QMainWindow as top-layer display window This change is made to resolve the issue that QWebView.showFullScreen() does not work in QPA Linuxfb Signed-off-by: Eric Ruei <e-ruei1@ti.com>
* main.cpp: print error if signal handler setup failsJacob Stiffler2015-09-301-0/+5
| | | | Signed-off-by: Jacob Stiffler <j-stiffler@ti.com>
* Add handler for SigTerm to gracefully exit QT applicationEric Ruei2015-09-244-6/+163
| | | | | | | Add MatrixWebView Class inherted from QWebView to support additional functionalities such as signal (SigTerm)handler Signed-off-by: Vivek Chengalvala <vchengalvala@ti.com>
* Makefile.build: with Qt5 use qmake available in PATHDenys Dmytriyenko2015-09-241-2/+2
| | | | Signed-off-by: Denys Dmytriyenko <denys@ti.com>
* matrix_browser: Update for QT5Jacob Stiffler2015-09-242-2/+2
| | | | Signed-off-by: Jacob Stiffler <j-stiffler@ti.com>
* Add "--windowed" option to disable full screen.Jacob Stiffler2015-06-121-4/+13
| | | | Signed-off-by: Jacob Stiffler <j-stiffler@ti.com>
* main: add "using std::endl;" to fix compilation warningHongmei Gou2015-04-091-0/+2
|
* Use dos2unix to convert from dos encoding to unixFranklin S Cooper Jr2015-04-091-61/+61
|
* Rename SDK Makefile back to Makefile.buildFranklin S. Cooper Jr2014-03-192-5/+3
| | | | | | | * This insures that Qt users will have qmake generate "Makefile" instead of App-Makefile which is the expected/default behavior. Signed-off-by: Franklin S. Cooper Jr <fcooper@ti.com>
* Fix make cleanFranklin S Cooper Jr2014-02-071-2/+1
| | | | | | | * Make sure the clean target runs qmake to insure that App-Makefile always exist. Signed-off-by: Franklin S Cooper Jr <fcooper@ti.com>
* Remove obsolete make targetsFranklin S Cooper Jr2014-02-051-2/+2
| | | | Signed-off-by: Franklin S Cooper Jr <fcooper@ti.com>
* Update MakefileFranklin S Cooper Jr2014-02-053-37/+51
| | | | | | | | | * Update Makefile to throw an error if destinatoin directory doesn't exist. * By default only build release version * Rename Makefile.build to Makefile * Have qmake generate App-Makefile as the makefile name Signed-off-by: Franklin S Cooper Jr <fcooper@ti.com>
* main: added licensing informationChase Maupin2012-01-251-0/+38
| | | | Signed-off-by: Chase Maupin <Chase.Maupin@ti.com>
* matrix_browser: Accept commandline argumentFranklin S Cooper Jr2011-12-221-4/+10
| | | | | | *Use the first parameter as the url to view instead of the hardcoded value Signed-off-by: Franklin S Cooper Jr <fcooper@ti.com>
* Adding CCS project files and removing unneeded MakefileFranklin Cooper Jr2011-10-273-221/+129
|
* Merge branch 'qwebview'Franklin Cooper Jr2011-10-261-21/+8
|\
| * Removed the reference to test.h since it is no longer being usedqwebviewFranklin Cooper Jr2011-10-261-1/+0
| |
| * Changed from WebView to QWebView which is the valid QT classFranklin Cooper Jr2011-10-211-1/+1
| |
| * Using the stripped down version using just regular QWebViewFranklin Cooper Jr2011-10-211-21/+8
| |
* | Removed the reference to test.h since it is no longer being usedFranklin Cooper Jr2011-10-261-1/+0
|/
* Initial commit of the Matrix BrowserFranklin Cooper Jr2011-10-213-0/+267