#===-- Makefile.config - Local configuration for LLVM ------*- Makefile -*--===#
#
# The LLVM Compiler Infrastructure
#
# This file is distributed under the University of Illinois Open Source
# License. See LICENSE.TXT for details.
#
#===------------------------------------------------------------------------===#
#
# This file is included by Makefile.common. It defines paths and other
# values specific to a particular installation of LLVM.
#
#===------------------------------------------------------------------------===#
# Define LLVM specific info and directories based on the autoconf variables
LLVMPackageName := @PACKAGE_TARNAME@
LLVMVersion := @PACKAGE_VERSION@
LLVM_CONFIGTIME := @LLVM_CONFIGTIME@
###########################################################################
# Directory Configuration
# This section of the Makefile determines what is where. To be
# specific, there are several locations that need to be defined:
#
# o LLVM_SRC_ROOT : The root directory of the LLVM source code.
# o LLVM_OBJ_ROOT : The root directory containing the built LLVM code.
#
# o PROJ_SRC_DIR : The directory containing the code to build.
# o PROJ_SRC_ROOT : The root directory of the code to build.
#
# o PROJ_OBJ_DIR : The directory in which compiled code will be placed.
# o PROJ_OBJ_ROOT : The root directory in which compiled code is placed.
#
###########################################################################
PWD := @BINPWD@
# Set the project name to LLVM if its not defined
ifndef PROJECT_NAME
PROJECT_NAME := $(LLVMPackageName)
endif
# The macro below is expanded when 'realpath' is not built-in.
# Built-in 'realpath' is available on GNU Make 3.81.
realpath = $(shell cd $(1); $(PWD))
PROJ_OBJ_DIR := $(call realpath, .)
PROJ_OBJ_ROOT := $(call realpath, $(PROJ_OBJ_DIR)/$(LEVEL))
CLANG_SRC_ROOT := @CLANG_SRC_ROOT@
ifeq ($(PROJECT_NAME),$(LLVMPackageName))
LLVM_SRC_ROOT := $(call realpath, @abs_top_srcdir@)
LLVM_OBJ_ROOT := $(call realpath, @abs_top_builddir@)
PROJ_SRC_ROOT := $(LLVM_SRC_ROOT)
PROJ_SRC_DIR := $(LLVM_SRC_ROOT)$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR))
ifneq ($(CLANG_SRC_ROOT),)
CLANG_SRC_ROOT:= $(call realpath, $(CLANG_SRC_ROOT))
PROJ_SRC_DIR := $(patsubst $(LLVM_SRC_ROOT)/tools/clang%,$(CLANG_SRC_ROOT)%,$(PROJ_SRC_DIR))
endif
prefix := @prefix@
PROJ_prefix := $(prefix)
program_prefix := @program_prefix@
PROJ_VERSION := $(LLVMVersion)
else
ifndef PROJ_SRC_ROOT
$(error Projects must define PROJ_SRC_ROOT)
endif
ifndef PROJ_OBJ_ROOT
$(error Projects must define PROJ_OBJ_ROOT)
endif
ifndef PROJ_INSTALL_ROOT
$(error Projects must define PROJ_INSTALL_ROOT)
endif
ifndef LLVM_SRC_ROOT
$(error Projects must define LLVM_SRC_ROOT)
endif
ifndef LLVM_OBJ_ROOT
$(error Projects must define LLVM_OBJ_ROOT)
endif
PROJ_SRC_DIR := $(call realpath, $(PROJ_SRC_ROOT)/$(patsubst $(PROJ_OBJ_ROOT)%,%,$(PROJ_OBJ_DIR)))
prefix := $(PROJ_INSTALL_ROOT)
PROJ_prefix := $(prefix)
ifndef PROJ_VERSION
PROJ_VERSION := 1.0
endif
endif
INTERNAL_PREFIX := @INTERNAL_PREFIX@
ifneq ($(INTERNAL_PREFIX),)
PROJ_internal_prefix := $(INTERNAL_PREFIX)
else
PROJ_internal_prefix := $(prefix)
endif
PROJ_bindir := $(PROJ_prefix)/bin
PROJ_libdir := $(PROJ_prefix)/lib
PROJ_datadir := $(PROJ_prefix)/share
PROJ_docsdir := $(PROJ_prefix)/docs/llvm
PROJ_etcdir := $(PROJ_prefix)/etc/llvm
PROJ_includedir := $(PROJ_prefix)/include
PROJ_infodir := $(PROJ_prefix)/info
PROJ_mandir := $(PROJ_prefix)/share/man
# Determine if we're on a unix type operating system
LLVM_ON_UNIX:=@LLVM_ON_UNIX@
LLVM_ON_WIN32:=@LLVM_ON_WIN32@
# Host operating system for which LLVM will be run.
OS=@OS@
HOST_OS=@HOST_OS@
# Target operating system for which LLVM will compile for.
TARGET_OS=@TARGET_OS@
# Host hardware architecture
HOST_ARCH=@HOST_ARCH@
# Target hardware architecture
ARCH=@ARCH@
TARGET_NATIVE_ARCH := $(ARCH)
# Indicates, whether we're cross-compiling LLVM or not
LLVM_CROSS_COMPILING=@LLVM_CROSS_COMPILING@
# Executable file extension for build platform (mainly for
# tablegen call if we're cross-compiling).
BUILD_EXEEXT=@BUILD_EXEEXT@
# Compilers for the build platflorm (mainly for tablegen
# call if we're cross-compiling).
BUILD_CC=@BUILD_CC@
BUILD_CXX=@BUILD_CXX@
# Triple for configuring build tools when cross-compiling
BUILD_TRIPLE=@build@
# Target triple (cpu-vendor-os) which LLVM is compiled for
HOST_TRIPLE=@host@
# Target triple (cpu-vendor-os) for which we should generate code
TARGET_TRIPLE=@target@
# Extra options to compile LLVM with
EXTRA_OPTIONS=@EXTRA_OPTIONS@
# Extra options to link LLVM with
EXTRA_LD_OPTIONS=@EXTRA_LD_OPTIONS@
# Endian-ness of the target
ENDIAN=@ENDIAN@
# Path to the C++ compiler to use. This is an optional setting, which defaults
# to whatever your gmake defaults to.
CXX = @CXX@
# Path to the CC binary, which use used by testcases for native builds.
CC := @CC@
# C/C++ preprocessor flags.
CPPFLAGS += @CPPFLAGS@
# C compiler flags.
CFLAGS += @CFLAGS@
# C++ compiler flags.
CXXFLAGS += @CXXFLAGS@
# Linker flags.
LDFLAGS += @LDFLAGS@
# Path to the library archiver program.
AR_PATH = @AR@
AR = @AR@
# Path to the nm program
NM_PATH = @NM@
# The pathnames of the programs we require to build
CMP := @CMP@
CP := @CP@
DATE := @DATE@
FIND := @FIND@
GREP := @GREP@
INSTALL := @INSTALL@
MKDIR := $(LLVM_SRC_ROOT)/autoconf/mkinstalldirs
MV := @MV@
RANLIB := @RANLIB@
RM := @RM@
SED := @SED@
TAR := @TAR@
PYTHON := @PYTHON@
# Paths to miscellaneous programs we hope are present but might not be
BZIP2 := @BZIP2@
CAT := @CAT@
DOT := @DOT@
DOXYGEN := @DOXYGEN@
GROFF := @GROFF@
GZIPBIN := @GZIPBIN@
OCAMLC := @OCAMLC@
OCAMLOPT := @OCAMLOPT@
OCAMLDEP := @OCAMLDEP@
OCAMLDOC := @OCAMLDOC@
GAS := @GAS@
POD2HTML := @POD2HTML@
POD2MAN := @POD2MAN@
PDFROFF := @PDFROFF@
ZIP := @ZIP@
HAVE_PTHREAD := @HAVE_PTHREAD@
LIBS := @LIBS@
# Targets that we should build
TARGETS_TO_BUILD=@TARGETS_TO_BUILD@
# Path to directory where object files should be stored during a build.
# Set OBJ_ROOT to "." if you do not want to use a separate place for
# object files.
OBJ_ROOT := .
# What to pass as rpath flag to g++
RPATH := @RPATH@
# What to pass as -rdynamic flag to g++
RDYNAMIC := @RDYNAMIC@
# These are options that can either be enabled here, or can be enabled on the
# make command line (ie, make ENABLE_PROFILING=1):
# When ENABLE_LIBCPP is enabled, LLVM uses libc++ by default to build.
#ENABLE_LIBCPP = 0
ENABLE_LIBCPP = @ENABLE_LIBCPP@
# When ENABLE_CXX11 is enabled, LLVM uses c++11 mode by default to build.
ENABLE_CXX11 = @ENABLE_CXX11@
# When ENABLE_CLANG_ARCMT is enabled, clang will have ARCMigrationTool.
ENABLE_CLANG_ARCMT = @ENABLE_CLANG_ARCMT@
# When ENABLE_CLANG_REWRITER is enabled, clang will have Rewriter.
ENABLE_CLANG_REWRITER = @ENABLE_CLANG_REWRITER@
# When ENABLE_CLANG_STATIC_ANALYZER is enabled, clang will have StaticAnalyzer.
ENABLE_CLANG_STATIC_ANALYZER = @ENABLE_CLANG_STATIC_ANALYZER@
# When ENABLE_WERROR is enabled, we'll pass -Werror on the command line
ENABLE_WERROR = @ENABLE_WERROR@
# When ENABLE_OPTIMIZED is enabled, LLVM code is optimized and output is put
# into the "Release" directories. Otherwise, LLVM code is not optimized and
# output is put in the "Debug" directories.
#ENABLE_OPTIMIZED = 1
@ENABLE_OPTIMIZED@
# When ENABLE_PROFILING is enabled, profile instrumentation is done
# and output is put into the "<Flavor>+Profile" directories, where
# <Flavor> is either Debug or Release depending on how other build
# flags are set. Otherwise, output is put in the <Flavor>
# directories.
#ENABLE_PROFILING = 1
@ENABLE_PROFILING@
# When DISABLE_ASSERTIONS is enabled, builds of all of the LLVM code will
# exclude assertion checks, otherwise they are included.
#DISABLE_ASSERTIONS = 1
@DISABLE_ASSERTIONS@
# When ENABLE_EXPENSIVE_CHECKS is enabled, builds of all of the LLVM
# code will include expensive checks, otherwise they are excluded.
#ENABLE_EXPENSIVE_CHECKS = 0
@ENABLE_EXPENSIVE_CHECKS@
# When DEBUG_RUNTIME is enabled, the runtime libraries will retain debug
# symbols.
#DEBUG_RUNTIME = 1
@DEBUG_RUNTIME@
# When DEBUG_SYMBOLS is enabled, the compiler libraries will retain debug
# symbols.
#DEBUG_SYMBOLS = 1
@DEBUG_SYMBOLS@
# When KEEP_SYMBOLS is enabled, installed executables will never have their
# symbols stripped.
#KEEP_SYMBOLS = 1
@KEEP_SYMBOLS@
# The compiler flags to use for optimized builds.
OPTIMIZE_OPTION := @OPTIMIZE_OPTION@
# When ENABLE_PROFILING is enabled, the llvm source base is built with profile
# information to allow gprof to be used to get execution frequencies.
#ENABLE_PROFILING = 1
# When ENABLE_DOCS is disabled, docs/ will not be built.
ENABLE_DOCS = @ENABLE_DOCS@
# When ENABLE_DOXYGEN is enabled, the doxygen documentation will be built
ENABLE_DOXYGEN = @ENABLE_DOXYGEN@
# Do we want to enable threads?
ENABLE_THREADS := @LLVM_ENABLE_THREADS@
# Do we want to enable zlib?
ENABLE_ZLIB := @LLVM_ENABLE_ZLIB@
# Do we want to build with position independent code?
ENABLE_PIC := @ENABLE_PIC@
# Do we want to build a shared library and link the tools with it?
ENABLE_SHARED := @ENABLE_SHARED@
# Do we want to link the stdc++ into a shared library? (Cygming)
ENABLE_EMBED_STDCXX := @ENABLE_EMBED_STDCXX@
# Use -fvisibility-inlines-hidden?
ENABLE_VISIBILITY_INLINES_HIDDEN := @ENABLE_VISIBILITY_INLINES_HIDDEN@
# Do we want to allow timestamping information into builds?
ENABLE_TIMESTAMPS := @ENABLE_TIMESTAMPS@
# This option tells the Makefiles to produce verbose output.
# It essentially prints the commands that make is executing
#VERBOSE = 1
# Enable JIT for this platform
TARGET_HAS_JIT = @TARGET_HAS_JIT@
# Environment variable to set to change the runtime shared library search path.
SHLIBPATH_VAR = @SHLIBPATH_VAR@
# Shared library extension for host platform.
SHLIBEXT = @SHLIBEXT@
# Executable file extension for host platform.
EXEEXT = @EXEEXT@
# Things we just assume are "there"
ECHO := echo
# Get the options for causing archives to link all their content instead of
# just missing symbols, and the inverse of that. This is used for certain LLVM
# tools that permit loadable modules. It ensures that the LLVM symbols will be
# available to those loadable modules.
LINKALL := @LINKALL@
NOLINKALL := @NOLINKALL@
# Get the value of HUGE_VAL_SANITY which will be either "yes" or "no" depending
# on the check.
HUGE_VAL_SANITY = @HUGE_VAL_SANITY@
# Bindings that we should build
BINDINGS_TO_BUILD := @BINDINGS_TO_BUILD@
ALL_BINDINGS := @ALL_BINDINGS@
OCAML_LIBDIR := @OCAML_LIBDIR@
# When compiling under Mingw/Cygwin, executables such as tblgen
# expect Windows paths, whereas the build system uses Unix paths.
# The function SYSPATH transforms Unix paths into Windows paths.
ifneq (,$(findstring -mno-cygwin, $(CXX)))
SYSPATH = $(shell echo $(1) | cygpath -m -f -)
else
SYSPATH = $(1)
endif
# Location of the plugin header file for gold.
BINUTILS_INCDIR := @BINUTILS_INCDIR@
# Optional flags supported by the compiler
# -Wno-missing-field-initializers
NO_MISSING_FIELD_INITIALIZERS = @NO_MISSING_FIELD_INITIALIZERS@
# -Wno-variadic-macros
NO_VARIADIC_MACROS = @NO_VARIADIC_MACROS@
# -Wcovered-switch-default
COVERED_SWITCH_DEFAULT = @COVERED_SWITCH_DEFAULT@
# -Wno-uninitialized
NO_UNINITIALIZED = @NO_UNINITIALIZED@
# -Wno-maybe-uninitialized
NO_MAYBE_UNINITIALIZED = @NO_MAYBE_UNINITIALIZED@
# Was polly found in tools/polly?
LLVM_HAS_POLLY = @LLVM_HAS_POLLY@
# Flags supported by the linker.
# bfd ld / gold --version-script=file
HAVE_LINK_VERSION_SCRIPT = @HAVE_LINK_VERSION_SCRIPT@
# Flags to control using libxml2
LIBXML2_LIBS := @LIBXML2_LIBS@
LIBXML2_INC := @LIBXML2_INC@
# Flags to control building support for Intel JIT Events API
USE_INTEL_JITEVENTS := @USE_INTEL_JITEVENTS@
INTEL_JITEVENTS_INCDIR := @INTEL_JITEVENTS_INCDIR@
INTEL_JITEVENTS_LIBDIR := @INTEL_JITEVENTS_LIBDIR@
# Flags to control building support for OProfile JIT API
USE_OPROFILE := @USE_OPROFILE@
ifeq ($(USE_INTEL_JITEVENTS), 1)
OPTIONAL_COMPONENTS += IntelJITEvents
endif
ifeq ($(USE_OPROFILE), 1)
OPTIONAL_COMPONENTS += OProfileJIT
endif