1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
|
ZED Stereo Camera ROS Node
==========================
ZED stereo camera ROS node based on OpenCV VideoCapture API for publishing left and right raw images and their camera_info.
## Usage:
1. Obtain the stereo camera calibration data file for your ZED camera (for a particular serial number) with one of two ways described below (already done for `SN29788442` and `SN5867575`):
Find the calibration file in
```
cd /usr/local/zed/settings
```
or, download from:
http://calib.stereolabs.com/?SN=xxxx
where xxxx is the serial number (SN) of your ZED camera.
Place the `SNxxxx.conf` file into `<zed_capture>/config` folder
Update the ZED camera SN string, `zed_sn_str`, in `<zed_capture>/launch/zed_capture.launch`
2. Generate `camera_info` YAML files and undistortion & rectification LUT files (already done for `SN29788442` and `SN5867575`)
Run the following script:
```
python2 <zed_capture>/script/generate_undist_rect_map.py -i SNxxxx.conf -m <camera_mode>
```
where
- `<zed_capture>` is the folder where the ZED camera node is installed (try `roscd zed_capture` to change directory after `catkin_make`),
- `SNxxxx.conf` is the factory calibration data file obtained from Step 1, and
- `<camera_mode>` is camera mode. Valid `<camera_mode>`: `2K`, `FHD`, `HD`, `HD2`, `VGA` (see ``Launch File Parameters`` section for description). If the `-m` argument is not provided, by default the tool will iterate for the following three camera modes: `HD`, `HD2`, and `FHD`.
This script parses the calibration data and generates the following files:
* `<zed_capture>/config/<SN_string>_<camera_mode>_camera_info_{left,right}.yaml`: `camera_info` for left and right raw image
* `<zed_capture>/config/<SN_string>_<camera_mode>_remap_LUT_{left,right}.{txt,bin}`: undist/rect remap LUT for left and right raw images, which are required by J7 VPAC/LDC hardware accelerator.
3. Build the ZED camera ROS node
```
cd $CATKIN_WS
catkin_make -j1
```
4. Launch the ZED camera node
```
roslaunch zed_capture zed_capture.launch
```
## Launch File Parameters
Parameter | Description | Value
------------------------------|-------------------------------------------------------------|-------------------------
zed_sn_str | ZED camera SN string | string
device_name | camera device_name. Typically `/dev/video0` on the target | string
camera_mode | ZED camera mode | '2K' (2208x1242)
_ | _ | 'FHD' (1920x1080)
_ | _ | 'HD' (1280x720)
_ | _ | 'HD2' (1280x720)*
_ | _ | 'VGA' (672x376)
frame_rate | rate at which images are published | int
encoding | image encoding | 'yuv422' (default) or 'bgr8'
**'HD2'** is a newly added mode that provides 720p resolution for experiments that need a longer focal length than the native 'HD'. The images are obtained by center-cropping the original 1080p images captured from the 'FHD' mode.
## Data Collection Steps
1. Connect the ZED camera to **UBS 3** Type-C port and check it with `ls /dev/video*`. In my Ubuntu PC setup, ZED camera is recognized as `/dev/video2`; while J7 host Linux, recognized as `/dev/video0`.
2. If necessary, update `launch/zed_capture.launch` to change video device, camera mode, frame rate, and etc.
3. On the first terminal, launch the ZED capture node with following, and **keep it running**:
```
$ roslaunch zed_capture zed_capture.launch
```
4. On the second terminal, to capture into ROS bag files, run one of two examples below
```
$ roslaunch zed_capture recordbag.launch # collect 15 seconds of data and stop itself
$ roslaunch zed_capture recordbag_split.launch # save into a series of bag files, each keeping 15 seconds of data, until terminated with Ctrl+C
```
5. (Optional to check the ROS topics) On 3rd terminal,
```
$ rostopic list
$ rqt_image_view /camera/left/image_raw
```
By default, ROS bag files are stored under `${HOME}/.ros` folder.
**Note**: It is not recommended combining the `zed_capture` node and ROSBAG capture into a single launch file, since it takes some several seconds for the ZED camera to settle down its ISP tuning after the ZED camera node starts.
|