blob: db24b84726479e4432c60eadb1a628e0ee125b9a (
plain) (
tree)
|
|
/**
* @file foreign.h
* @brief Defines a foreign clock record.
* @note Copyright (C) 2011 Richard Cochran <richardcochran@gmail.com>
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License as published by
* the Free Software Foundation; either version 2 of the License, or
* (at your option) any later version.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*
* You should have received a copy of the GNU General Public License along
* with this program; if not, write to the Free Software Foundation, Inc.,
* 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
*/
#ifndef HAVE_FOREIGN_H
#define HAVE_FOREIGN_H
#include <sys/queue.h>
#include "ds.h"
#include "port.h"
#define FOREIGN_MASTER_THRESHOLD 2
struct foreign_clock {
/**
* Pointer to next foreign_clock in list.
*/
LIST_ENTRY(foreign_clock) list;
/**
* A list of received announce messages.
*
* The data set field, foreignMasterPortIdentity, is the
* sourcePortIdentity of the first message.
*/
TAILQ_HEAD(messages, ptp_message) messages;
/**
* Number of elements in the message list,
* aka foreignMasterAnnounceMessages.
*/
unsigned int n_messages;
/**
* Pointer to the associated port.
*/
struct port *port;
/**
* Contains the information from the latest announce message
* in a form suitable for comparision in the BMCA.
*/
struct dataset dataset;
};
#endif
|