/** * @file filter.h * @brief Implements a generic filter interface. * @note Copyright (C) 2013 Miroslav Lichvar * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License, or * (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License along * with this program; if not, write to the Free Software Foundation, Inc., * 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA. */ #ifndef HAVE_FILTER_H #define HAVE_FILTER_H #include "tmv.h" /** Opaque type */ struct filter; /** * Defines the available filters. */ enum filter_type { FILTER_MOVING_AVERAGE, FILTER_MOVING_MEDIAN, }; /** * Create a new instance of a filter. * @param type The type of the filter to create. * @param length The filter's length. * @return A pointer to a new filter on success, NULL otherwise. */ struct filter *filter_create(enum filter_type type, int length); /** * Destroy an instance of a filter. * @param filter Pointer to a filter obtained via @ref filter_create(). */ void filter_destroy(struct filter *filter); /** * Feed a sample into a filter. * @param filter Pointer to a filter obtained via @ref filter_create(). * @param sample The input sample. * @return The output value. */ tmv_t filter_sample(struct filter *filter, tmv_t sample); /** * Reset a filter. * @param filter Pointer to a filter obtained via @ref filter_create(). */ void filter_reset(struct filter *filter); #endif