1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
|
/**
* @file ntpshm.c
* @brief Implements a servo providing the NTP SHM reference clock to
* send the samples to another process.
* @note Copyright (C) 2014 Miroslav Lichvar <mlichvar@redhat.com>
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License as published by
* the Free Software Foundation; either version 2 of the License, or
* (at your option) any later version.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*
* You should have received a copy of the GNU General Public License along
* with this program; if not, write to the Free Software Foundation, Inc.,
* 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
*/
#include <stdlib.h>
#include <sys/types.h>
#include <sys/shm.h>
#include "config.h"
#include "print.h"
#include "ntpshm.h"
#include "servo_private.h"
/* NTP leap values */
#define LEAP_NORMAL 0x0
#define LEAP_INSERT 0x1
#define LEAP_DELETE 0x2
/* Key of the first SHM segment */
#define SHMKEY 0x4e545030
/* Declaration of the SHM segment from ntp (ntpd/refclock_shm.c) */
struct shmTime {
int mode; /* 0 - if valid set
* use values,
* clear valid
* 1 - if valid set
* if count before and after read of values is equal,
* use values
* clear valid
*/
volatile int count;
time_t clockTimeStampSec;
int clockTimeStampUSec;
time_t receiveTimeStampSec;
int receiveTimeStampUSec;
int leap;
int precision;
int nsamples;
volatile int valid;
int clockTimeStampNSec;
int receiveTimeStampNSec;
int dummy[8];
};
struct ntpshm_servo {
struct servo servo;
struct shmTime *shm;
int leap;
};
static void ntpshm_destroy(struct servo *servo)
{
struct ntpshm_servo *s = container_of(servo, struct ntpshm_servo, servo);
shmdt(s->shm);
free(s);
}
static double ntpshm_sample(struct servo *servo,
int64_t offset,
uint64_t local_ts,
double weight,
enum servo_state *state)
{
struct ntpshm_servo *s = container_of(servo, struct ntpshm_servo, servo);
uint64_t clock_ts = local_ts - offset;
s->shm->mode = 1;
s->shm->count++;
s->shm->valid = 0;
/* TODO: write memory barrier */
s->shm->clockTimeStampSec = clock_ts / NS_PER_SEC;
s->shm->clockTimeStampNSec = clock_ts % NS_PER_SEC;
s->shm->clockTimeStampUSec = s->shm->clockTimeStampNSec / 1000;
s->shm->receiveTimeStampSec = local_ts / NS_PER_SEC;
s->shm->receiveTimeStampNSec = local_ts % NS_PER_SEC;
s->shm->receiveTimeStampUSec = s->shm->receiveTimeStampNSec / 1000;
s->shm->precision = -30; /* 1 nanosecond */
switch (s->leap) {
case -1:
s->shm->leap = LEAP_DELETE;
break;
case 1:
s->shm->leap = LEAP_INSERT;
break;
default:
s->shm->leap = LEAP_NORMAL;
}
/* TODO: write memory barrier */
s->shm->count++;
s->shm->valid = 1;
*state = SERVO_UNLOCKED;
return 0.0;
}
static void ntpshm_sync_interval(struct servo *servo, double interval)
{
}
static void ntpshm_reset(struct servo *servo)
{
}
static void ntpshm_leap(struct servo *servo, int leap)
{
struct ntpshm_servo *s = container_of(servo, struct ntpshm_servo, servo);
s->leap = leap;
}
struct servo *ntpshm_servo_create(struct config *cfg)
{
struct ntpshm_servo *s;
int ntpshm_segment = config_get_int(cfg, NULL, "ntpshm_segment");
int shmid;
s = calloc(1, sizeof(*s));
if (!s)
return NULL;
s->servo.destroy = ntpshm_destroy;
s->servo.sample = ntpshm_sample;
s->servo.sync_interval = ntpshm_sync_interval;
s->servo.reset = ntpshm_reset;
s->servo.leap = ntpshm_leap;
shmid = shmget(SHMKEY + ntpshm_segment, sizeof (struct shmTime),
IPC_CREAT | 0600);
if (shmid == -1) {
pr_err("ntpshm: shmget failed: %m");
free(s);
return NULL;
}
s->shm = (struct shmTime *)shmat(shmid, 0, 0);
if (s->shm == (void *)-1) {
pr_err("ntpshm: shmat failed: %m");
free(s);
return NULL;
}
return &s->servo;
}
|